Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Evaluate GNU Radio application performance on Pi4(2G)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 674 subscribers
  • Views 8242 views
  • Users 0 members are here
  • raspberry_pi
Related

Evaluate GNU Radio application performance on Pi4(2G)

colporteur
colporteur over 6 years ago

The results after using a Raspberry Pi 3B+ to run a GNU Radio flow graph were unacceptable. The audio outputed from the Pi was distorted. I speculate the SBC doesn't have the performance specification to support GNU Radio.

 

I am trying to determine if the Raspberry Pi (version ?) is capable of supporting a GNU Radio flow graph. My current assessment is no. The hardware performance is not sufficient to handle the digital signal processing requirements.

 

It was suggested I make a forum post while some testing was done, so other interested could follow.

 

My objective was to write a tutorial for the GNU Radio application using a Raspberry Pi. After successfully building two GNU Radio flow graphs on my Ubuntu 18.04 i7 processor desktop, I ported the flow graphs to a Pi3B+ connected to an HDMI with audio monitor. One flow graph is an audio signal generator outputed to a speaker. The second is an FM receiver. Both flow graphs work in the sense they produce audio but with distortion and in the case of FM broadcast, unreadable.

 

The audio flow graph requires a GNU Radio software installation. The FM flow graph requires an SDR dongle to gather a broadcasted signal to feed the GNU Radio FM radio receiver flow graph. The test will be using the audio flow graph since no additional hardware is required.

 

image

cstanton  has agreed to use his Pi4(2G) to run the test. Before starting the exercise, I will ask Christopher to review review the procedures and provide feedback. I'm keeping the the verbiage terse, assuming a higher level of understanding. If more details are required or feel something is more appropriate or missing please let me know.

 

A zip file of two flow graphs is attached. The file with basic is minimal as it gets. The second file provides a test module. I experienced a problem with both.

 

 

Test Procedure:

Fresh install of Raspbian Buster Full, current release.

Apply O/S updates/upgrades & Install GNU Radio

 

///CODE START///

sudo apt-get update -y;sudo apt-get upgrade -y

sudo reboot

sudo apt-get install gnuradio

///CODE END///

 

Take screen shots of htop screen at the following milestones.

1. O/S idle, no application running on the GUI desktop other than what is defaulted.

2. GNU Radio started, no flow graph

3. GNU Radio flow graph loaded.

4. GNU Radio flow graph started.

5. Evaluate audio coming from speaker and advise.

 

Depending on results, i would like to expand the test Ginny pig agreed.

 

Sean

 

Message was edited by: sean conway I have uploaded the two audio flow graphs for GNU Radio. The current version of GNU Radio encourages development in QT widgets verses the WX widgets. Three is discussion in the community support for WX will disappear. The flow graphs provided are QT. Sean

Attachments:
gnuradio.zip
gnuradio_FM.zip
  • Sign in to reply
  • Cancel
Parents
  • cstanton
    cstanton over 6 years ago

    Running Pi 4, 4GB in a cooled case

    - downloaded latest raspbian

    - installed latest updates

    - installed latest firmware

    - installed latest bootloader

    - ran sudo apt-get install rtl-sdr gnuradio gr-osmosdr

     

    image

     

    - opened gnuradio

     

    image

     

    - opened file audio_QTv1.grc

    - clicked to 'generate'

    - clicked to 'run'

    - received error 'xterm executable is missing, you can change this setting in your gnuradio.conf in section [grc] xterm_executable

    fix- https://steemit.com/raspberrypi/@chirimenjako/gnuradio-tips-terminal-error

     

    - Ran again

     

    execute:

    Warning: failed to XInitThreads()

    qt5ct: using qt5ct plugin

     

    (process:2326): Gtk-WARNING **: 21:36:30.684: Locale not supported by C library.

    Using the fallback 'C' locale.

    gr::log :INFO: audio source - Audio sink arch: alsa

    gr::log :ERROR: audio_alsa_sink0 - [default]: set_channels failed: Invalid argument

    Traceback (most recent call last):

      File "/home/pi/gnu/gnur/top_block.py", line 172, in <module>

        main()

      File "/home/pi/gnu/gnur/top_block.py", line 161, in main

        tb.start()

      File "/usr/lib/python2.7/dist-packages/gnuradio/gr/top_block.py", line 109, in start

        top_block_start_unlocked(self._impl, max_noutput_items)

      File "/usr/lib/python2.7/dist-packages/gnuradio/gr/runtime_swig.py", line 5656, in top_block_start_unlocked

        return _runtime_swig.top_block_start_unlocked(r, max_noutput_items)

    RuntimeError: check topology failed on audio_alsa_sink(2) using ninputs=1, noutputs=0

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to cstanton

    Hopefully I haven't lost your interest.

     

    I queried to the gnuradio group on their slack service and one member provided some insight. It is an ALSA configuration issue. The default configuration of a Pi isn't compatible with GNR. The bluetooth speaker install changes the defaults in .asoundrc that resolve the run time error. Another way to get the flow graph to work without installing a bluetooth speaker is to change the device parameter in the audio sink block to null. The flow graph works but no audio output.

     

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 6 years ago in reply to colporteur

    RPi distros always seem to be one step behind the other Linux/Unix distros.  That is a pity but reality.  I will keep following because I am still curious to know if the RPi4 (faster, more modern RAM, 4MB) can replace my x64 desktop without having to run that RPi4 in the refrigerator to keep cool enough.  You need to push on the gnuradio github folks that RPi4 is now a real general purpose desktop unlike its predecessors.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to Former Member

      just got a aluminum case with dual fans for my RPi 4 and it seems to stay cool. If only the Beaglebone AI would do the same. Today, it reached 85 degrees and was going to shutdown with out a fan. Ugh...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 6 years ago in reply to clem57

    clem57  The enclosure + fans:  which product? Got a link?  This one looked cool: https://www.amazon.com/Pastall-Raspberry-Armor-Cooling-Enclosure/dp/B07X59H4RR/ref=sr_1_1_sspa?keywords=Raspberry+Pi+4+Armor+Case&qid=1573483528&s=electronics&sr=1-1-spons&psc=1&spLa=ZW5jcnlwdGVkUXVhbGlmaWVyPUExWDUyRDNSWEYxTExLJmVuY3J5cHRlZElkPUEwMzExOTg5M0NVMkZVT1hNWjBFOSZlbmNyeXB0ZWRBZElkPUEwNzYxNTEwM1FYMk9FSjdLSjM2MCZ3aWRnZXROYW1lPXNwX2F0ZiZhY3Rpb249Y2xpY2tSZWRpcmVjdCZkb05vdExvZ0NsaWNrPXRydWU=

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 6 years ago in reply to Former Member

    Had you tried the CanaKit with fan and found it insufficient?

    https://www.amazon.com/CanaKit-Raspberry-4GB-Basic-Starter/dp/B07VYC6S56/ref=sr_1_3?keywords=Raspberry+Pi+4+canakit&qid=…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 6 years ago in reply to Former Member

    Are the dual fans noisy?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 6 years ago in reply to Former Member

    Are the dual fans noisy?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 6 years ago in reply to Former Member

    This was an interesting blog about MicroSD performance on pi 3 & 4: https://www.jeffgeerling.com/blog/2019/raspberry-pi-microsd-card-performance-comparison-2019

    Also, good notes about USB access.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to Former Member

    Not at all. They are small ones hooked up to 5 V.

    Clem