Hi
i don't really know much about this device ,but i would like to use it in a regulated vacuum tube filament supply , output voltage should be able to move from min voltage to about 10vdc ,6.3v @ 3A max load.
I have played with the lm317 and the 5A version to that device and i could never get them to regulated properly and they very easy to damage ,
My luck with SS parts , are a joke maybe it is ,the lack of knowledge in this area , which is stopping me from understanding how these reg work and @ £ 7 a pop i need to be pretty sure
about what resistors and capacitors are needed for the project before i buy a single Ldo
cheers