PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Forum KiCAD 8: alternative pin functions
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 129 subscribers
  • Views 3502 views
  • Users 0 members are here
  • kicad 8
  • kicad
Related

KiCAD 8: alternative pin functions

Jan Cumps
Jan Cumps over 1 year ago

I tried KiCAD's (not so) new alternative pin functions option in  the library editor.

I'm designing a project with a Renesas controller. There wasn't a symbol yet, so I started to create one. The majority of the mcu's pins have more than 5 functions. I figured this would be a good candidate to test the new option.

image

Here's the definition in the editor:

image

And a schematic with 3 symbols placed, with a few pins showing different functions.

image

I've attached the symbols: MCU_RENESAS_R_20240323_3.zip

It's a bit of work to get this set up, but it works well. Thoughts?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 1 year ago +4
    Very interesting! For sure it will simplify many circuit layouts. I'm looking forward to using it. I have not used that so far, but I think I would be super-tempted during symbol creation, to add one…
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz +2
    I was tempted to do that for a few pins. The same that have multiple functions in the datasheet (43, 44, 47, 48) But what choice do you make as a symbol designer. It 'll always be the wrong one.…
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz +2
    ... and I've also been playing with alternatives. Below a functionally-split-up one, and two with all in one symbol the U1 has a separate block for analogue, digital and power.
Parents
  • baldengineer
    baldengineer over 1 year ago
    Jan Cumps said:
    I tried KiCAD's new alternative pin functions option in  the library editor.

    So, I don't want to be *that guy*... buuuuuut, Alternative Pin functions are not new to KiCad 8.

    They've been available as far back as early as KiCad 5, maybe even before.

    However, what is new in version 8 is how you assign them. The "Alternative Pin Function" table in the Schematic Editor now better shows which pins have alternative functions. And you can now change the pin assignment on the symbol in the schematic editor. (If clicking on a pin selects the entire symbol, there is an option in preferences named something like "Clicking on pin selects symbol," which needs to be unchecked.)

    By the way, there's an open feature request to graphically indicate on the symbol which pins have alt functions available. The issue could probably use some feedback on what such a feedback symbol would look like.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 1 year ago
    Jan Cumps said:
    I tried KiCAD's new alternative pin functions option in  the library editor.

    So, I don't want to be *that guy*... buuuuuut, Alternative Pin functions are not new to KiCad 8.

    They've been available as far back as early as KiCad 5, maybe even before.

    However, what is new in version 8 is how you assign them. The "Alternative Pin Function" table in the Schematic Editor now better shows which pins have alternative functions. And you can now change the pin assignment on the symbol in the schematic editor. (If clicking on a pin selects the entire symbol, there is an option in preferences named something like "Clicking on pin selects symbol," which needs to be unchecked.)

    By the way, there's an open feature request to graphically indicate on the symbol which pins have alt functions available. The issue could probably use some feedback on what such a feedback symbol would look like.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 1 year ago in reply to baldengineer

    Your real photo suits you better than avatar! : ) 

    • Cancel
    • Vote Up +2 Vote Down