Arduino Forum Pololu USB AVR Programmer
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
  • State Verified Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 404 subscribers
  • Views 639 views
  • Users 0 members are here
Related

Pololu USB AVR Programmer

gtrplyer16
gtrplyer16 over 10 years ago

Does anyone know if the above programmer is compatible with windows 8?? I bought some ATMega chips and they weren't the right ones so I was going to buy a programmer to mess around with an program it using AVR studio 6 instead of finding an arduino to use them in.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago in reply to clem57 +3 suggested
    Note: This programmer supports standard in-system programming (ISP), which is also sometimes called in-circuit serial programming (ICSP). It does not support JTAG, DebugWire, or High-Voltage programming…
  • clem57
    clem57 over 10 years ago +2 suggested
    Supported Operating Systems The programmer has been tested under Windows XP, Windows Vista, Windows 7, Windows 8, and Linux from https://www.pololu.com/product/1300 Clem
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    I poersonally have the PGM03A and it works across the board (Its a POLOLU Board also)
Parents
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    I have used one of these and it works. Tested few time ago to see how W8 was working, because as a matter of fact I have almost all the C++ development environment working on a Windows7 machine so I have only put a try. But if you have one Arduino at-home (Arduino duemilanove and UNO R2/3 works fine) you can do a very minimal circuit to program from the IDE your AVR with the Arduino. It is one of the options of the IDE.

     

    To speedup the development from the AVR Studio I have bought and I am using a standard AVR MKII programmer from Atmel but it is almost expensive (+/- 30$) and it is the worth only with the AVR Studio because it is the most compatible ISP programmer for fast developing. You can see it here: Connecting Atmel AVRISP mkII - - AVRISP MkII

     

    Instead to program multiple units and save time and money, you can do one for yourself for about the half of the cost of the Pololu with a simple - minimal - circuit I show in the image below. It has the advantage that with a zero-force connector it is fast and secure to put the microcontroller chip inside, program and remove. I had in past to write the same program for every test cycle on about 10 different units. If you need the circuit - very simple - for this silly programmer let me know.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    I have used one of these and it works. Tested few time ago to see how W8 was working, because as a matter of fact I have almost all the C++ development environment working on a Windows7 machine so I have only put a try. But if you have one Arduino at-home (Arduino duemilanove and UNO R2/3 works fine) you can do a very minimal circuit to program from the IDE your AVR with the Arduino. It is one of the options of the IDE.

     

    To speedup the development from the AVR Studio I have bought and I am using a standard AVR MKII programmer from Atmel but it is almost expensive (+/- 30$) and it is the worth only with the AVR Studio because it is the most compatible ISP programmer for fast developing. You can see it here: Connecting Atmel AVRISP mkII - - AVRISP MkII

     

    Instead to program multiple units and save time and money, you can do one for yourself for about the half of the cost of the Pololu with a simple - minimal - circuit I show in the image below. It has the advantage that with a zero-force connector it is fast and secure to put the microcontroller chip inside, program and remove. I had in past to write the same program for every test cycle on about 10 different units. If you need the circuit - very simple - for this silly programmer let me know.

     

    image

    • Cancel
    • Vote Up +2 Vote Down