Arduino Forum Pololu USB AVR Programmer
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
  • State Verified Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 404 subscribers
  • Views 625 views
  • Users 0 members are here
Related

Pololu USB AVR Programmer

gtrplyer16
gtrplyer16 over 10 years ago

Does anyone know if the above programmer is compatible with windows 8?? I bought some ATMega chips and they weren't the right ones so I was going to buy a programmer to mess around with an program it using AVR studio 6 instead of finding an arduino to use them in.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago in reply to clem57 +3 suggested
    Note: This programmer supports standard in-system programming (ISP), which is also sometimes called in-circuit serial programming (ICSP). It does not support JTAG, DebugWire, or High-Voltage programming…
  • clem57
    clem57 over 10 years ago +2 suggested
    Supported Operating Systems The programmer has been tested under Windows XP, Windows Vista, Windows 7, Windows 8, and Linux from https://www.pololu.com/product/1300 Clem
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    I poersonally have the PGM03A and it works across the board (Its a POLOLU Board also)
Parents
  • clem57
    0 clem57 over 10 years ago

    Supported Operating Systems

    The programmer has been tested under Windows XP, Windows Vista, Windows 7, Windows 8, and Linux

    from https://www.pololu.com/product/1300

    Clem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    Supported Operating Systems

    The programmer has been tested under Windows XP, Windows Vista, Windows 7, Windows 8, and Linux

    from https://www.pololu.com/product/1300

    Clem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to clem57

    Note:

    This programmer supports standard in-system programming (ISP), which is also sometimes called in-circuit serial programming (ICSP). It does not support JTAG, DebugWire, or High-Voltage programming.


    Very nice features for this programmer...

     

    Please see for many things to help you ==> https://www.pololu.com/product/1300/resources

    Clem

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer