1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog 1 METRE OF PI – EIGHTH POST – CONSTRUCTION - MAIN ELEMENTS – POWER
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
  • Author Author: stevotech
  • Date Created: 14 Dec 2020 11:29 AM Date Created
  • Views 552 views
  • Likes 4 likes
  • Comments 1 comment
  • design challenge
  • raspberry pi
  • 1meterofpi raspberry_pi
Related
Recommended

1 METRE OF PI – EIGHTH POST – CONSTRUCTION - MAIN ELEMENTS – POWER

stevotech
stevotech
14 Dec 2020

Completing the last stages of scale-model construction to form a Power Module that sits at a foundations/ground level:

The special pump/base/tank assembly is affixed in the centre of the bottom housing

image

A-MVF-GIZZMOTO & BASE MTG.jpg

 

An Air Compressor is positioned on one side and an Air Receiver on the opposite side.

image

B-MVF POWER MODULE ISO VIEW 1.jpg

 
  image

C-MVF POWER MODULE ISO VIEW 2.jpg

In this instance the piece of equipment has a 12-volts DC motor (*)

 

An additional element is the ‘WIZZROTO’ (to the right on the plan layout) a hydro-energy device with a water collecting chamber that will take its source of supply from the mains water connection feeding into the top, No. 4, level and convert it into electrical energy for battery storage and as a supplementary supply. (**)

  image

D-MVF POWER MODULE PLAN LAYOUT.jpg

  

The next section fits on top to complete the ‘ceiling’ for the Power Module.

  image

E-MVF-GIZZMOTO BASE MTG & FIRST LEVEL BASE 1.jpg

 

Followed by the upper set of 4 levels framework

image

F-MVF-GIZZMOTO & BASE MTG & 4 LEVELS.jpg

 

This enables the loading and stacking of ‘food-growing’ containers on each level (the ‘supermarket-shelves’ syndrome)

image

G-MVF-LEVELS 1-4 CONTAINERS.jpg

 

*In a full-size installation the Compressed Air Supply could be separate to the Modular Vertical Farm, with the Air Compressor mounted onto the Air Receiver as a self-contained Power Pack, sited adjacent to the Farm or remotely in a Compressor House. To give you an idea of scale, I have shown the Power Pack as a stand-alone item; the size of the model is 22 cm long x 9 cm wide x 15 cm high; also, alongside the Power Module.

  image

H-MVF AIR COMPRESSOR.jpg

 
image
 

I-MVF POWER MODULE EXTERNAL AIR SUPPLY 1.jpg

 
image

J-MVF POWER MODULE EXTERNAL AIR SUPPLY 2.jpg

 
**The ‘WIZZROTO’ is conceptual but I have consulted with a university professor who is an expert in hydro-energy, and he agrees that in principle it could work.

K-WIZZROTO CONCEPT SCHEMATIC.pdf

**The concept is not an essential part of this project but so that I can follow the idea through I have started to assemble a small-scale 3D unit to test early 2021.

image

L-MVF-WIZZROTO 1.jpg

  1meterofpi raspberry_pi, design challenge, raspberry pi 4 2gb, 1 meter of pi, 1_meter_of_pi, 1 meter of pi - design challenge

Attachments:
imageK-WIZZROTO CONCEPT SCHEMATIC.pdf
  • Sign in to reply

Top Comments

  • skruglewicz
    skruglewicz over 5 years ago +1
    nice mechanical design
Parents
  • skruglewicz
    skruglewicz over 5 years ago

    nice mechanical design

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • skruglewicz
    skruglewicz over 5 years ago

    nice mechanical design