1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog 2Pi Microgravity Garden Blog 8 | AI Image Recognition Improvements with Google Coral and Heat Mat
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
  • Author Author: kurama007
  • Date Created: 23 Dec 2020 11:28 PM Date Created
  • Views 678 views
  • Likes 4 likes
  • Comments 0 comments
  • google coral
  • 1meterofpi
  • 1 meter of pi
Related
Recommended

2Pi Microgravity Garden Blog 8 | AI Image Recognition Improvements with Google Coral and Heat Mat

kurama007
kurama007
23 Dec 2020

We are already in the second half of the project and we want to see how we can help astronauts with this 1 meter of Pi project. So far, during this project, we realized that there are a couple of challenges in microgravity garden.

 

Let's recap a couple of challenges that we want to solve with this project!

 

1. Non self-pollinating plants need pollination --> how to monitor them and help pollination mechanically, bugs, or wind

2. We want to avoid bugs in space  --> Bug catcher plants! But, this doesn't help pollination

3. Water monitor for hydroponics system --> Hydroponics system requires water and nutrition constantly

4. Environment change in space --> temperature, humidity, and light which are required for photosynthsis

 

image

 

Let's do our best to tackle those challenges with the time left in this project.

 

Interestingly, NASA is researching a microgravity garden.

https://twitter.com/ISS_Research/status/1342510163249438720?s=20

 

image

 

Blog 8 Task List

 

Previously, we tried an image recognition with a Raspberry Pi and webcam. For improvements, I researched a bit and tried a couple of things.

 

1. Add Google Coral to increase frame rate per second

2. Try different web cameras

     2.1 1080p

     2.2 2K 30 FPS with winder viewing angle for capturing 1 cubic meter range

 

image

 

For plants, now is winter season and temperature is low, so I added a new item to warm up plants image

 

3. Added a gardening heat mat

image

 

Content

1. Improve frame per second by Google Coral: AI Accelerator

 

In the previous blog (2Pi Microgravity Garden Blog 7 | AI Image Recognition with Raspberry Pi and Tensor Flow

), we tried the image recognition just by the raspberry Pi and webcam. The frame per second is about 7.

 

This time, Google Coral is a nice and reasonable AI accelerator which is Raspberry Pi ready by a USB connection.

https://coral.ai/products/accelerator/

 

Without Google Coral, the Frame Per Second (FPS) was about 4.5 and all objects stay still now.

image

With Google Coral, the Frame Per Second (FPS) improved to 22 - 24. But, the object detection is not properly working anymore. This is the area of improvements.

image

 

To switch with and without Google Coral, just created an automation script.

 

The automation bash script is available on github.

https://github.com/kurama007/1MeterOfPi/blob/main/run_tfl.sh

 

2. Try different webcams

 

The original webcam used in this project was 1080p and regular angle. Then, I've switched to 2K (2560x1440) 90 degree wide viewing angle

https://www.amazon.com/gp/product/B08CMV4GF6/ref=ppx_yo_dt_b_asin_title_o01_s01?ie=UTF8&psc=1

 

This camera has wider viewing angle and I mounted it on a tripod. This turned out to be a good setup to capture 1 cubic meter area.

 

3. Add a heat mat

 

The outer space is very cold! The temperature is 2.7K which is -455 F or -270 C. So, we want to measure water temperature and outside temperature for environmental control.

image

Project Information

Project Description: https://green-scientist.com/projects/1-meter-of-pi-2pi-microgravity-garden/

1 Meter of Pi Project Blog: 1 Meter of Pi

Github repo: https://github.com/kurama007/1MeterOfPi