1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog 3. Spirulina Farming Blueprint
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
  • Author Author: surbhika
  • Date Created: 27 Dec 2020 5:25 PM Date Created
  • Views 2153 views
  • Likes 4 likes
  • Comments 4 comments
  • algae
  • spirulina
Related
Recommended

3. Spirulina Farming Blueprint

surbhika
surbhika
27 Dec 2020

image

Design Features:

  1. This is a modular and scalable design. More water tanks can be added at any time and a single or more water tank can be removed easily from the system for harvesting the required amount of algae at a time.

  2. Valves at the end of each water tank for the maintenance and scalability of the system

  3. Each water container is to be half-filled with water and half with used capsules of air. As the algae grow and photosynthesis occurs, it will replenish the oxygen level in the air.

image

 

Following sensors are installed to monitor and ensure healthy growth of algae:

 

  1. pH Sensor: to ensure alkalinity of water. It indicates that it is time to add alkaline substances.
  2. Temperature sensor: to ensure a suitable temperature for algae growth. Turns On and Off Heater as required.
  3. Light Sensor: to ensure proper supply of light required for photosynthesis (growth of algae). If natural light hours per day are less, then turns on Lamp
  • Sign in to reply
Parents
  • DAB
    DAB over 5 years ago

    Nice simple solution.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • surbhika
    surbhika over 5 years ago in reply to DAB

    I hope it's spaceproof  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • surbhika
    surbhika over 5 years ago in reply to DAB

    I hope it's spaceproof