1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog Space Vegetables - #25 | biweekly update
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
  • Author Author: feiticeir0
  • Date Created: 2 Feb 2021 2:55 PM Date Created
  • Views 1641 views
  • Likes 5 likes
  • Comments 5 comments
  • 1meterofpi
  • 1 meter of pi
  • 1 meter of pi - design challenge
  • space vegetables
  • 1meter of pi
Related
Recommended

Space Vegetables - #25 | biweekly update

feiticeir0
feiticeir0
2 Feb 2021

image

 

Hello everyone. Hope all are well and safe. This be hard times.

 

Welcome to another update of keeping the Astronauts feed and alive ! image

 

This week I've noted that there was some condensation inside the greenhouse. I was not expecting that for several reasons, but the main one is this is not a tight seal. There's an opening above, where all the Electronics are. The temperature inside is always higher than outside, but this wasn't there the day before yesterday... Don't know what could it be.

image

 

Vegetables

 

The beans are growing a lot and I had to trim them or else they don't get light (and there's just not enough space)..They look like ghosts:

image

Sadly, some beans are getting sick, but not all. The following photo shows some things that are appearing on the stems of the beans. I don't know what they are, but this doesn't seem natural.

 

EDIT: This is a disease called "Bean rust - Uromyces appendiculatus" . It is caused by a fungus that was spread by air.. WT*... ? How did it came here ? In space this wouldn't happen - I think.

image

I removed them from the hydroponics. The roots were brown and sick.. Hope it doesn't spread to other plants..

 

All the others are doing just fine, but growing slowly.. Since November, 2 months have passed (uau, already..). I'm in the Northern Hemisphere, and now it's winter. I have the "1 meter of PI" in my garage, away from the sun and the cold outside. The temperature inside the greenhouse never drops below 10 degrees, but still...

The lettuce is really developing well and soon I think I can harvest some ! image Can't wait.

The bell peppers are slowly growing, but I knew it would be so. The other vegetables are also growing slowly.

 

Since I'm keeping the project going, when the weather outside presents itself more pleasing and warm, I'm moving this outside - at least will save the lights electricity bill  - and there's no better light source than the sun! image

imageimage

I wish you could smell the earthy scent that comes from the hydroponics. It's really really awesome (for those who like it).

 

Space Vegetables Client : Program

I'm still experiencing some glitches, but not in the code. The code works and does everything it is supposed to do. This time, I think that's the Python executable that is crashing (or the schedule function of Python), but without any warnings whatsoever... Every once in a while, it just stops executing the commands to turn on the pumps (air and water) and updating the values. Need to investigate the scheduler of Python.

 

Time lapse.

Here's the time lapse from the very beginning until now showing the Vegetables growing.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • skruglewicz
    skruglewicz over 5 years ago +1
    nice progress. Hope we hear about the winners soon!
  • feiticeir0
    feiticeir0 over 5 years ago in reply to skruglewicz +1
    Thank you ! Yeah, they really are late, but with all this of COVID-19, I understand !
  • skruglewicz
    skruglewicz over 5 years ago in reply to feiticeir0 +1
    Yes, but it would be nice off the organizer to communicate with the participants that have spent time on the challenge. It's almost like it's gone dark.
Parents
  • skruglewicz
    skruglewicz over 5 years ago

    nice progress. Hope we hear about the winners soon!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • feiticeir0
    feiticeir0 over 5 years ago in reply to skruglewicz

    Thank you !

    Yeah, they really are late, but with all this of COVID-19, I understand !

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skruglewicz
    skruglewicz over 5 years ago in reply to feiticeir0

    Yes, but it would be nice off the organizer to communicate with the participants that have spent time on the challenge. It's almost like it's gone dark.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 5 years ago in reply to skruglewicz

    Hello! we are just putting together the winners announcement right now!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14phil
    e14phil over 5 years ago in reply to skruglewicz

    Hello! we are just putting together the winners announcement right now!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • skruglewicz
    skruglewicz over 5 years ago in reply to e14phil

    Thanks so much for the updatee14phil

    I understand you have a Ton of blogs to go over..

    no problem.. I was just wondering

    I Appreciate your efforts.

    Steve K