1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog Space Vegetables #7 : Hydroponics kit and greenhouse
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
  • Author Author: feiticeir0
  • Date Created: 12 Nov 2020 2:11 PM Date Created
  • Views 791 views
  • Likes 4 likes
  • Comments 3 comments
  • 1meterofpi
  • 1 meter of pi
  • 1 meter of pi - design challenge
  • space vegetables
  • 1meter of pi
Related
Recommended

Space Vegetables #7 : Hydroponics kit and greenhouse

feiticeir0
feiticeir0
12 Nov 2020

image

 

Hello everybody ! Hope everyone is safe.

This past two weekends was finally the time to finish the greenhouse where the magic will happen. The wiring and connections to the Raspberry PI's is finished and will be explained further down.

The beginnings of the greenhouse are started in the third post of this series.

 

Greenhouse

 

This is the finished "contraption" to house the hydroponics and all the electronics that goes into controlling it.

image

imageimage

The housing is just some aluminum profiles with wood to make it sturdy and be able to fix all the electronics.

Because this is not able to withstand the rain - and I'm in the northern hemisphere, its fall/winter time, it has lights to help the plants grow.

imageimage

 

The first set of lights are fixed to the greenhouse and the second set of lights are fixed to the top layer of the hydroponics kit.

I have white lights and red/blue lights, in the ratio 5:1 .

It has been shown that plants not also need red/blue, but also white lights - the full spectrum. It's certain that when growing they need more of one than the other, but when in the vegetative state or fruiting, the need more of the other

Further reading here and here

 

It has a tick plastic all around it and the "doors" - front and back - have velcro to allow to "open" and "close" when needed.

 

The kit already has been tested with water to search for leaks. Everything is fine and no leak was found. There was some problems with the water tube connection, but a bit of plumber tape solved the problem.

 

Assembly of the hydroponics kit

 

Here are some pictures of the assembly

imageimage

 

imageimage

 

 

Electronics

 

The electronics are housed above, in a shelf just for them.

We have (from left to right):

  • Raspberry PI4b with the Enviro HAT
  • Raspberry PI 3B+ with the Automation HAT mini
  • 4 channel relay controlled by the Automation HAT mini

Fullscreen contentimage_146440.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Because the terminals in the Automation HAT mini are so small, some wires would touch each other and strange things would happen, like, after turning the lights on, the air pump would also turn on, etc.., I decided to use the outputs to turn on/off an external relay.

The Automation HAT mini controls everything, but using an external relay and not the outputs directly. The relay of the automation HAT is controlling the Water Pump.

So, here's what each one does:

  • RPI 4B 2GB with Enviro HAT
    • Temperature
    • Pressure
    • Humidity
    • Luminosity
    • SQLITE3 database
    • Flask Webservices
  • RPI 3B+ with Automation Hat MINI
    • Water Pump
    • 4 channel relay
      • Air Pump
      • Red/Blue lights
      • White Lights
  • RPI Zero W (not in the picture)
    • Takes a picture every 10 minutes for a posterior time lapse.
    • Uses Webservices from RPI4 to gather environmental data
      • Post to twitter 4 times a day with the environmental data and a picture of the hydroponics grow status

 

Why two lights ? Well, they should have been together, but the 12v power source I was going to use for both does not have enough amps.So, I've split them into two.

image

 

The next weekend it's play time. Everything is going to start working - for another post.

  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 5 years ago +2
    Hello Bruno Gretat work! However some pictures in the post are not visible (broken link). I am very curious to see the details!
  • feiticeir0
    feiticeir0 over 5 years ago in reply to amgalbu +1
    Hi amgalbu ! Thank you for the warning. They are now corrected ! Cheers
  • genebren
    genebren over 5 years ago +1
    This is really looking good! It will be interesting to see some actual plant growth. Keep up the good work!
Parents
  • genebren
    genebren over 5 years ago

    This is really looking good!  It will be interesting to see some actual plant growth.  Keep up the good work!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 5 years ago

    This is really looking good!  It will be interesting to see some actual plant growth.  Keep up the good work!