1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Forum Official Email?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 3 answers
  • Subscribers 7 subscribers
  • Views 2764 views
  • Users 0 members are here
Related

Official Email?

hugohu
hugohu over 6 years ago

I am indeed, impatient... so I was chosen as a challenger, I believe there should be an email but I haven't received one.... (I've checked junk and main).

 

I was tagged, but no email, so I was wondering if it's safe to begin buying parts for my project? Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +4 suggested
    Hi Hugo, Sometimes it helps to tag the administrator by inserting his ID in your question so you are sure your question is noticed. I believe e14phil is the one who originally posted the project. It will…
  • e14phil
    e14phil over 6 years ago +4 verified
    John is right! I am now summoned! Hey Hugo, ill be sending an email shortly. I had to keep it under wraps but I was just launching the New micro:bit . Now that has gone live I am back on Design Challenges…
  • hugohu
    hugohu over 6 years ago in reply to e14phil +2
    Hopefully the new Micro:Bit is more of a competitor to the Adafruit Clue! At least, I'm not too sure why you need 512K of flash on a MicroBit to say, since it's block coding... But the extra the merrier…
Parents
  • e14phil
    0 e14phil over 6 years ago

    John is right! I am now summoned! image Hey Hugo, ill be sending an email shortly. 

    I had to keep it under wraps but I was just launching the New micro:bit. Now that has gone live I am back on Design Challenges

     

    Phil

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hugohu
    0 hugohu over 6 years ago in reply to e14phil

    Hopefully the new Micro:Bit is more of a competitor to the Adafruit Clue! image

     

    At least, I'm not too sure why you need 512K of flash on a MicroBit to say, since it's block coding...

     

    But the extra the merrier! I have 2MB Flash, 512K SRAM, on a feather I got as part as a roadtest. I will not use that Feather very much, and lastly, I won't even need half that much Flash/RAM. I could say my code is extremely optimized... but the truth is, I just don't write advanced code image

     

    Back to topic... thanks for the reply, as soon as I get the email I'm going to buy stuff!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hugohu
    0 hugohu over 6 years ago in reply to e14phil

    Hopefully the new Micro:Bit is more of a competitor to the Adafruit Clue! image

     

    At least, I'm not too sure why you need 512K of flash on a MicroBit to say, since it's block coding...

     

    But the extra the merrier! I have 2MB Flash, 512K SRAM, on a feather I got as part as a roadtest. I will not use that Feather very much, and lastly, I won't even need half that much Flash/RAM. I could say my code is extremely optimized... but the truth is, I just don't write advanced code image

     

    Back to topic... thanks for the reply, as soon as I get the email I'm going to buy stuff!