1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Forum Some advice please?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 5 answers
  • Subscribers 7 subscribers
  • Views 2486 views
  • Users 0 members are here
Related

Some advice please?

hugohu
hugohu over 6 years ago

I’m a challenger for 1 Meter of Pi, I’ve been designing a lightning system for the plants, however, I realize that the LEDs would require 5A total of current, so I split them into 5 parts, for 1A per section. This still is too much for an arduino pin to handle- at most they can handle one or two, while each had 5.

I’ve considered using multiple pins and boards but my friend says that would likely overload the regulators and fry the chip, or damage.

He said using buck converters, and MOSFETs, would be an ideal solution.

can someone please eleaborate on this part, like a bit of conceptual explanation, and/or other ideas? Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • gam3t3ch
    gam3t3ch over 6 years ago +2 suggested
    I would need to know more about the lights setup to give you my opinion but off the top of my head using a simple relay would allow you to do that then you can use the appropriate power output and use…
  • milosrasic98
    milosrasic98 over 6 years ago +2 suggested
    Hi! You can either use a relay to turn on/off the lights, which will work good, or you can go the route of using MOSFETs where you can also control how bright the LEDs are using PWM. Here is a project…
  • colporteur
    colporteur over 6 years ago +2 suggested
    A buck (reduce)/boost (increase) board enables you to move the output voltage up or down in relation to the input. I use them extensively in my personal projects. I have base 12VDC power supply that is…
Parents
  • colporteur
    0 colporteur over 6 years ago

    A buck (reduce)/boost (increase) board enables you to move the output voltage up or down in relation to the input. I use them extensively in my personal projects. I have base 12VDC power supply that is used to power strings of LED's. I then use a buck/boost board to produce 5VDC and 3VDC for the digital electronics.

     

    image

     

    I have had good success with LM2596 DC-DC Adjustable Step Down Power Supply Module from banggood.com. They are inexpensive if bought in quantity and have yet to replace any from burning them out. Trust me I have done some not to smart stuff!

     

    I tend to not use relays if I need to control a load. Solid state devices vs mechanical devices are less problematic. I switch 12 VDC LED strings with an IRFZ44 FET.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 6 years ago

    A buck (reduce)/boost (increase) board enables you to move the output voltage up or down in relation to the input. I use them extensively in my personal projects. I have base 12VDC power supply that is used to power strings of LED's. I then use a buck/boost board to produce 5VDC and 3VDC for the digital electronics.

     

    image

     

    I have had good success with LM2596 DC-DC Adjustable Step Down Power Supply Module from banggood.com. They are inexpensive if bought in quantity and have yet to replace any from burning them out. Trust me I have done some not to smart stuff!

     

    I tend to not use relays if I need to control a load. Solid state devices vs mechanical devices are less problematic. I switch 12 VDC LED strings with an IRFZ44 FET.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer