1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Forum Some advice please?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 5 answers
  • Subscribers 7 subscribers
  • Views 2483 views
  • Users 0 members are here
Related

Some advice please?

hugohu
hugohu over 6 years ago

I’m a challenger for 1 Meter of Pi, I’ve been designing a lightning system for the plants, however, I realize that the LEDs would require 5A total of current, so I split them into 5 parts, for 1A per section. This still is too much for an arduino pin to handle- at most they can handle one or two, while each had 5.

I’ve considered using multiple pins and boards but my friend says that would likely overload the regulators and fry the chip, or damage.

He said using buck converters, and MOSFETs, would be an ideal solution.

can someone please eleaborate on this part, like a bit of conceptual explanation, and/or other ideas? Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • gam3t3ch
    gam3t3ch over 6 years ago +2 suggested
    I would need to know more about the lights setup to give you my opinion but off the top of my head using a simple relay would allow you to do that then you can use the appropriate power output and use…
  • milosrasic98
    milosrasic98 over 6 years ago +2 suggested
    Hi! You can either use a relay to turn on/off the lights, which will work good, or you can go the route of using MOSFETs where you can also control how bright the LEDs are using PWM. Here is a project…
  • colporteur
    colporteur over 6 years ago +2 suggested
    A buck (reduce)/boost (increase) board enables you to move the output voltage up or down in relation to the input. I use them extensively in my personal projects. I have base 12VDC power supply that is…
Parents
  • milosrasic98
    0 milosrasic98 over 6 years ago

    Hi!

     

    You can either use a relay to turn on/off the lights, which will work good, or you can go the route of using MOSFETs where you can also control how bright the LEDs are using PWM. Here is a project I did where I've done that using MOSFETS Ski Lamp . I've used 3 MOSFETs because the LED strip was RGB, so I was controlling each of the channels, one would be sufficient if you're using a single color LED. If you plan on doing that just make sure in the datasheet what are the voltages that can turn on the MOSFET so you don't need a comparator before it like me, as well as the max current, though, the second one shouldn't be an issue. Hope this helps!

     

    Milos

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • milosrasic98
    0 milosrasic98 over 6 years ago

    Hi!

     

    You can either use a relay to turn on/off the lights, which will work good, or you can go the route of using MOSFETs where you can also control how bright the LEDs are using PWM. Here is a project I did where I've done that using MOSFETS Ski Lamp . I've used 3 MOSFETs because the LED strip was RGB, so I was controlling each of the channels, one would be sufficient if you're using a single color LED. If you plan on doing that just make sure in the datasheet what are the voltages that can turn on the MOSFET so you don't need a comparator before it like me, as well as the max current, though, the second one shouldn't be an issue. Hope this helps!

     

    Milos

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer