At The Core Design Challenge
  • Challenges & Projects
  • Design Challenges
  • At The Core Design Challenge
  • More
  • Cancel
At The Core Design Challenge
Forum CY8C62 DMA from buffer to GPIO P10_0..2
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join At The Core Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 51 subscribers
  • Views 2511 views
  • Users 0 members are here
  • design challenge
  • dmac
  • gpio
  • psoc6
  • at the core
Related

CY8C62 DMA from buffer to GPIO P10_0..2

Digimorf
Digimorf over 3 years ago

Hello,

I am working on the configuration of a DMAC channel for streaming data bytes from a buffer to the GPIO port 10, using only GPIOs from 0 to 2. I think I am missing something but I really can't make it work.

Since I am learning for now I am triggering the DMA by simply enabling the block, next I will trigger it with a CC0 of a counter. But, let's see what I got so far.

I have started an "Empty Project" from the getting started section. Then in the "Device Configurator" I simply set the DMAC channel 0 for a transfer of 1 byte.

/* NOTE: This is a preview only. It combines elements of the
 * cycfg_dmas.c and cycfg_dmas.h files located in the folder
 * C:/Users/Francesco/mtw/Empty_App_1/bsps/TARGET_APP_CY8CKIT-062S4/config/GeneratedSource.
 */

#include "cy_dmac.h"
#if defined (CY_USING_HAL)
    #include "cyhal_hwmgr.h"
#endif //defined (CY_USING_HAL)

#define cpuss_0_dmac_0_chan_0_HW DMAC
#define cpuss_0_dmac_0_chan_0_CHANNEL 0U
#define cpuss_0_dmac_0_chan_0_IRQ cpuss_interrupts_dmac_0_IRQn

cy_stc_dmac_descriptor_config_t cpuss_0_dmac_0_chan_0_Descriptor_0_config = 
{
    .retrigger = CY_DMAC_RETRIG_IM,
    .interruptType = CY_DMAC_1ELEMENT,
    .triggerOutType = CY_DMAC_1ELEMENT,
    .channelState = CY_DMAC_CHANNEL_ENABLED,
    .triggerInType = CY_DMAC_1ELEMENT,
    .dataPrefetch = false,
    .dataSize = CY_DMAC_WORD,
    .srcTransferSize = CY_DMAC_TRANSFER_SIZE_WORD,
    .dstTransferSize = CY_DMAC_TRANSFER_SIZE_WORD,
    .descriptorType = CY_DMAC_SINGLE_TRANSFER,
    .srcAddress = NULL,
    .dstAddress = NULL,
    .srcXincrement = 0,
    .dstXincrement = 0,
    .xCount = 1,
    .srcYincrement = 1,
    .dstYincrement = 1,
    .yCount = 1,
    .nextDescriptor = NULL,
};
cy_stc_dmac_descriptor_t cpuss_0_dmac_0_chan_0_Descriptor_0 = 
{
    .ctl = 0UL,
    .src = 0UL,
    .dst = 0UL,
    .xSize = 0UL,
    .xIncr = 0UL,
    .ySize = 0UL,
    .yIncr = 0UL,
    .nextPtr = 0UL,
};
cy_stc_dmac_channel_config_t cpuss_0_dmac_0_chan_0_channelConfig = 
{
    .descriptor = &cpuss_0_dmac_0_chan_0_Descriptor_0,
    .priority = 3,
    .enable = false,
    .bufferable = false,
};
#if defined (CY_USING_HAL)
    const cyhal_resource_inst_t cpuss_0_dmac_0_chan_0_obj = 
    {
        .type = CYHAL_RSC_DMA,
        .block_num = 2U,
        .channel_num = cpuss_0_dmac_0_chan_0_CHANNEL,
    };
#endif //defined (CY_USING_HAL)


void reserve_cycfg_dmas(void)
{
#if defined (CY_USING_HAL)
    cyhal_hwmgr_reserve(&cpuss_0_dmac_0_chan_0_obj);
#endif //defined (CY_USING_HAL)
}

The three GPIOs P10_0..2 are configured as:

const cy_stc_gpio_pin_config_t CYBSP_A0_config = 
{
    .outVal = 0,
    .driveMode = CY_GPIO_DM_STRONG_IN_OFF,
    .hsiom = CYBSP_A0_HSIOM,
    .intEdge = CY_GPIO_INTR_DISABLE,
    .intMask = 0UL,
    .vtrip = CY_GPIO_VTRIP_CMOS,
    .slewRate = CY_GPIO_SLEW_FAST,
    .driveSel = CY_GPIO_DRIVE_1_2,
    .vregEn = 0UL,
    .ibufMode = 0UL,
    .vtripSel = 0UL,
    .vrefSel = 0UL,
    .vohSel = 0UL,
};

Then in the main.c I set the destination and source:

#include "cyhal.h"
#include "cybsp.h"

#define scanline_dma_HW             cpuss_0_dmac_0_chan_0_HW
#define scanline_dma_descriptor     cpuss_0_dmac_0_chan_0_Descriptor_0
#define scanline_dma_descriptor_cfg cpuss_0_dmac_0_chan_0_Descriptor_0_config
#define scanline_dma_CH             cpuss_0_dmac_0_chan_0_CHANNEL
#define scanline_dma_CH_cfg         cpuss_0_dmac_0_chan_0_channelConfig

uint32_t pix = 0x5;
GPIO_PRT_Type* scanline_rgb_port = GPIO_PRT10;


int main(void)
{
    cy_rslt_t result;

#if defined (CY_DEVICE_SECURE)
    cyhal_wdt_t wdt_obj;

    /* Clear watchdog timer so that it doesn't trigger a reset */
    result = cyhal_wdt_init(&wdt_obj, cyhal_wdt_get_max_timeout_ms());
    CY_ASSERT(CY_RSLT_SUCCESS == result);
    cyhal_wdt_free(&wdt_obj);
#endif

    /* Initialize the device and board peripherals */
    result = cybsp_init();

    /* Board init failed. Stop program execution */
    if (result != CY_RSLT_SUCCESS)
    {
        CY_ASSERT(0);
    }

    /* Enable global interrupts */
    __enable_irq();

    Cy_DMAC_Descriptor_Init(&scanline_dma_descriptor,
                            &scanline_dma_descriptor_cfg);

    Cy_DMAC_Descriptor_SetSrcAddress(&scanline_dma_descriptor,
                                     (void*)&pix);

    Cy_DMAC_Descriptor_SetDstAddress(&scanline_dma_descriptor,
                                     (void*)(scanline_rgb_port->OUT));

    Cy_DMAC_Channel_Init(scanline_dma_HW,
                         scanline_dma_CH,
                         &scanline_dma_CH_cfg);

    Cy_DMAC_Channel_SetDescriptor(scanline_dma_HW,
                                  scanline_dma_CH,
                                  &scanline_dma_descriptor);

    Cy_DMAC_Channel_Enable(scanline_dma_HW,
                          scanline_dma_CH);

    Cy_DMAC_Enable(scanline_dma_HW);

    for (;;)
    {

    }
}

My Logic Analyzer should show signals 0 and 2 pulsing from low to high but nothing happens, I can't understand if the transfer doesn't start, or if the GPIO port is not correct for output.

I haven't been lucky in finding an example of the use of DMA on GPIOs, so I am asking here Slight smile

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • Digimorf
    Digimorf over 3 years ago +2
    Digimorf said: In the Trigger multiplexer diagram, I saw that the CPUSS.Zero should be a software trigger connected to the DMAC block, but I wasn't able to find what this "Zero" means in the CPU SubSystem…
  • misaz
    misaz over 3 years ago in reply to Digimorf +1
    In my app I use DW instead of DMAC and DW works. I will write several blogs about it. How do you trigger DMA(C) transfer?
  • misaz
    misaz over 3 years ago in reply to Digimorf +1
    Your DMA transfer most probably failed because of ilegal bus access. I have faced similar problem. Issue is that GPIO OUT register prohibits byte (8-bit) and word (16-bit) AXI access and allows only…
Parents
  • Digimorf
    0 Digimorf over 3 years ago

    Definitely, there is something wrong with DMA. Currently, I did a simple test with a memory-to-memory transfer, like the one shown in the online PDL documentation, but it doesn't start at all. So there's something I am missing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • misaz
    0 misaz over 3 years ago in reply to Digimorf

    In my app I use DW instead of DMAC and DW works. I will write several blogs about it. How do you trigger DMA(C) transfer?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Digimorf
    0 Digimorf over 3 years ago in reply to misaz

    I am working on a Dual-core project, in the CM0+ part.

        Cy_DMAC_Descriptor_Init(&scanline_dma_descriptor,
                                &scanline_dma_descriptor_cfg);
    
        Cy_DMAC_Descriptor_SetSrcAddress(&scanline_dma_descriptor,
                                         (void*)(&src[0]));
    
        Cy_DMAC_Descriptor_SetDstAddress(&scanline_dma_descriptor,
                                         (void*)(&dst[0]));
    
        Cy_DMAC_Channel_Init(scanline_dma_HW,
                             scanline_dma_CH,
                             &scanline_dma_CH_cfg);
    
        Cy_DMAC_Channel_SetDescriptor(scanline_dma_HW,
                                      scanline_dma_CH,
                                      &scanline_dma_descriptor);
    
        Cy_DMAC_Channel_Enable(scanline_dma_HW,
                              scanline_dma_CH);
    
        Cy_DMAC_Enable(scanline_dma_HW);

    #define scanline_dma_HW             cpuss_0_dmac_0_chan_0_HW
    #define scanline_dma_descriptor     cpuss_0_dmac_0_chan_0_Descriptor_0
    #define scanline_dma_descriptor_cfg cpuss_0_dmac_0_chan_0_Descriptor_0_config
    #define scanline_dma_CH             cpuss_0_dmac_0_chan_0_CHANNEL
    #define scanline_dma_CH_cfg         cpuss_0_dmac_0_chan_0_channelConfig
    

    Basically here, for test purposes, I am trying to perform a memory-to-memory copy. So I only need a simple software trigger.

    The two buffers are simple arrays of chars:

    char src[32];
    char dst[32];

    While the descriptor has been defined in Device Configurator:

    #define cpuss_0_dmac_0_chan_0_HW DMAC
    #define cpuss_0_dmac_0_chan_0_CHANNEL 0U
    #define cpuss_0_dmac_0_chan_0_IRQ cpuss_interrupts_dmac_0_IRQn
    
    cy_stc_dmac_descriptor_config_t cpuss_0_dmac_0_chan_0_Descriptor_0_config = 
    {
        .retrigger = CY_DMAC_RETRIG_IM,
        .interruptType = CY_DMAC_DESCR,
        .triggerOutType = CY_DMAC_DESCR,
        .channelState = CY_DMAC_CHANNEL_ENABLED,
        .triggerInType = CY_DMAC_DESCR,
        .dataPrefetch = false,
        .dataSize = CY_DMAC_BYTE,
        .srcTransferSize = CY_DMAC_TRANSFER_SIZE_DATA,
        .dstTransferSize = CY_DMAC_TRANSFER_SIZE_DATA,
        .descriptorType = CY_DMAC_MEMORY_COPY,
        .srcAddress = NULL,
        .dstAddress = NULL,
        .srcXincrement = 1,
        .dstXincrement = 1,
        .xCount = 16,
        .srcYincrement = 1,
        .dstYincrement = 1,
        .yCount = 1,
        .nextDescriptor = NULL,
    };
    cy_stc_dmac_descriptor_t cpuss_0_dmac_0_chan_0_Descriptor_0 = 
    {
        .ctl = 0UL,
        .src = 0UL,
        .dst = 0UL,
        .xSize = 0UL,
        .xIncr = 0UL,
        .ySize = 0UL,
        .yIncr = 0UL,
        .nextPtr = 0UL,
    };
    cy_stc_dmac_channel_config_t cpuss_0_dmac_0_chan_0_channelConfig = 
    {
        .descriptor = &cpuss_0_dmac_0_chan_0_Descriptor_0,
        .priority = 3,
        .enable = false,
        .bufferable = false,
    };
         

    In the few examples I have found in Application Notes, and PDL documentation, the DMA transfer should start as soon as a "Cy_DMAC_Enable" it's invoked. Maybe I am wrong...

    In the Trigger multiplexer diagram, I saw that the CPUSS.Zero should be a software trigger connected to the DMAC block, but I wasn't able to find what this "Zero" means in the CPU SubSystem. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Digimorf
    0 Digimorf over 3 years ago in reply to misaz

    I am working on a Dual-core project, in the CM0+ part.

        Cy_DMAC_Descriptor_Init(&scanline_dma_descriptor,
                                &scanline_dma_descriptor_cfg);
    
        Cy_DMAC_Descriptor_SetSrcAddress(&scanline_dma_descriptor,
                                         (void*)(&src[0]));
    
        Cy_DMAC_Descriptor_SetDstAddress(&scanline_dma_descriptor,
                                         (void*)(&dst[0]));
    
        Cy_DMAC_Channel_Init(scanline_dma_HW,
                             scanline_dma_CH,
                             &scanline_dma_CH_cfg);
    
        Cy_DMAC_Channel_SetDescriptor(scanline_dma_HW,
                                      scanline_dma_CH,
                                      &scanline_dma_descriptor);
    
        Cy_DMAC_Channel_Enable(scanline_dma_HW,
                              scanline_dma_CH);
    
        Cy_DMAC_Enable(scanline_dma_HW);

    #define scanline_dma_HW             cpuss_0_dmac_0_chan_0_HW
    #define scanline_dma_descriptor     cpuss_0_dmac_0_chan_0_Descriptor_0
    #define scanline_dma_descriptor_cfg cpuss_0_dmac_0_chan_0_Descriptor_0_config
    #define scanline_dma_CH             cpuss_0_dmac_0_chan_0_CHANNEL
    #define scanline_dma_CH_cfg         cpuss_0_dmac_0_chan_0_channelConfig
    

    Basically here, for test purposes, I am trying to perform a memory-to-memory copy. So I only need a simple software trigger.

    The two buffers are simple arrays of chars:

    char src[32];
    char dst[32];

    While the descriptor has been defined in Device Configurator:

    #define cpuss_0_dmac_0_chan_0_HW DMAC
    #define cpuss_0_dmac_0_chan_0_CHANNEL 0U
    #define cpuss_0_dmac_0_chan_0_IRQ cpuss_interrupts_dmac_0_IRQn
    
    cy_stc_dmac_descriptor_config_t cpuss_0_dmac_0_chan_0_Descriptor_0_config = 
    {
        .retrigger = CY_DMAC_RETRIG_IM,
        .interruptType = CY_DMAC_DESCR,
        .triggerOutType = CY_DMAC_DESCR,
        .channelState = CY_DMAC_CHANNEL_ENABLED,
        .triggerInType = CY_DMAC_DESCR,
        .dataPrefetch = false,
        .dataSize = CY_DMAC_BYTE,
        .srcTransferSize = CY_DMAC_TRANSFER_SIZE_DATA,
        .dstTransferSize = CY_DMAC_TRANSFER_SIZE_DATA,
        .descriptorType = CY_DMAC_MEMORY_COPY,
        .srcAddress = NULL,
        .dstAddress = NULL,
        .srcXincrement = 1,
        .dstXincrement = 1,
        .xCount = 16,
        .srcYincrement = 1,
        .dstYincrement = 1,
        .yCount = 1,
        .nextDescriptor = NULL,
    };
    cy_stc_dmac_descriptor_t cpuss_0_dmac_0_chan_0_Descriptor_0 = 
    {
        .ctl = 0UL,
        .src = 0UL,
        .dst = 0UL,
        .xSize = 0UL,
        .xIncr = 0UL,
        .ySize = 0UL,
        .yIncr = 0UL,
        .nextPtr = 0UL,
    };
    cy_stc_dmac_channel_config_t cpuss_0_dmac_0_chan_0_channelConfig = 
    {
        .descriptor = &cpuss_0_dmac_0_chan_0_Descriptor_0,
        .priority = 3,
        .enable = false,
        .bufferable = false,
    };
         

    In the few examples I have found in Application Notes, and PDL documentation, the DMA transfer should start as soon as a "Cy_DMAC_Enable" it's invoked. Maybe I am wrong...

    In the Trigger multiplexer diagram, I saw that the CPUSS.Zero should be a software trigger connected to the DMAC block, but I wasn't able to find what this "Zero" means in the CPU SubSystem.