Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog BTU - Project LOKI.11 - Mobile use
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
  • Author Author: jkutzsch
  • Date Created: 21 Jul 2018 1:01 AM Date Created
  • Views 1064 views
  • Likes 6 likes
  • Comments 1 comment
  • raspberry pi 3 b+
  • kali
  • bluetooth unleashed design challenge
Related
Recommended

BTU - Project LOKI.11 - Mobile use

jkutzsch
jkutzsch
21 Jul 2018

Time for a short and quick update.

 

I took Project LOKI out for a little trip to the grocery store and wanted to show the results.

 

image

 

As you can see it was able to find 3 mac addresses while I was out.

 

image

Here is our Blue Book ready to carry out the clandestine adventures with Project LOKI.

 

image

 

Here you can see Project LOKI powered up and portable inside the Blue Book.

 

For further adventures I think I will have to look at better venting though since the wood and paper of the book box just traps the heat of Project LOKI.

 

image

 

Here I have pulled the 5000mAh battery out from under the Project.

 

If you look carefully at the first open book picture you can see the battery poking up on the left hand side.

 

By placing it there it keeps the weight all at the bottom if you flip the book up like a normal book and the battery actually helps everything fit pretty snug inside the book box.

 

image

 

I had picked up this battery a year or so ago since it was one of the few I could find that claims have pass through charging and was inexpensive.

 

Under $10 from Amazon minus shipping. 

 

This definitely show promise for using the Raspberry Pi 3b+ with builtin bluetooth as a security device.  Portability is a huge benefit with the screen and battery being the main limiting factors for size weight. 

 

Reviewing Re4son's work shows he used a much smaller setup and attached it to a drone to create a mobile platform that could be remotely controlled. 

 

image

 

While I would love to try out that as a future endeavor I do not have a drone that would be capable of carrying the setup so it will have to wait for now.  I do have a smaller screen but my eyes prefers the larger screen if I am not limited by weight and size.  :-)

 

Please feel free to message me if you come across any linux bluetooth tools you think could be promising and I will give it a go on see if Project LOKI can utilize it!

 

Thank you!

 

 

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +1
    Nice update on your design challenge project. It is pretty cool that you were able to sniff out a couple of MAC addresses out in a real world environment. Cool! Gene
Parents
  • genebren
    genebren over 8 years ago

    Nice update on your design challenge project.  It is pretty cool that you were able to sniff out a couple of MAC addresses out in a real world environment.

    Cool!

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Nice update on your design challenge project.  It is pretty cool that you were able to sniff out a couple of MAC addresses out in a real world environment.

    Cool!

    Gene