Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog Smart Doorbell System - Part 10 - Complete Project Video
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
  • Author Author: shabaz
  • Date Created: 20 Jul 2018 10:58 PM Date Created
  • Views 7939 views
  • Likes 17 likes
  • Comments 28 comments
  • bluetooth
  • cc2640r2
  • ti launchpad
  • bluetooth le
  • bluetooth_unleashed
  • winners
  • bt_smart_doorbell
  • design_challenges
  • bluetooth 5.0
  • raspberry_pi
  • rpi 3b+
  • bbb
  • texas_instruments
  • cc2640r2f
  • rpi 3b
  • bluetooth_le
Related
Recommended

Smart Doorbell System - Part 10 - Complete Project Video

shabaz
shabaz
20 Jul 2018

For all the parts to this project, click here! Smart Doorbell System

 

Introduction

The Smart Doorbell System is a Bluetooth Low Energy (BLE) project to build a better doorbell! However, it could also have other uses - to open and close gates, to act as an emergency attendant button or to control or monitor all sorts of things. It can also be connected up to a Pi or BeagleBone, for extending reach and capabilities even further. For example, the Pi could log and timestamp activity, or activate a camera, or tunnel the information to another Pi or BeagleBone, and then pass the information onward over BLE to the far end, providing all the benefits of BLE combined with the compute horsepower and cloud connecting capability of the Pi.

 

All software and schematics and PCB files and bill-of-materials (BoM) are available.

 

For more information, click on the link above to explore all the blog posts, or (easier) watch the twenty-minute video below.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

What Was Built?

Two modules were constructed; the bell push module, and the chime module. The can communicate directly to each other, or they can connect to a Linux system for extra features such as tunnelling alerts over the Internet, or for logging events or taking photos of who is at the door. With some effort the same system could be used for patient care, or for alerting people in a warehouse / shop floor.

image

 

The Bell Push Module runs from an AA sized battery and should run for four years (I intend to make code changes to improve that further - currently it consumes 45uA but around 20uA should be feasible). It uses a Texas Instruments chip, the CC2640R2FCC2640R2F. When connecting to the wireless Chime Module, it consumes around 12-13mA average, briefly until the communication is complete. More accurate tests still need to be done, but these values were promising.

image

 

The Chime Module was constructed from a custom PCB plugged on top of a ready-made Texas Instruments microcontroller board called the CC2640R2 LaunchPadCC2640R2 LaunchPad. The custom PCB contains digital audio capability and dual supply capability (external DC, or the attached rechargeable battery which gets charged up automatically). The Chime Module can be used plugged-in to the DC supply, or it can be detached and taken outdoors (e.g. into the garden). When used on battery power, the current consumption is about 8mA, which allows for several days of outdoor use with the 600mA battery that was used. The battery will charge itself so there should be no maintenance required.

image

 

Next Steps

Although the system functions, the code is very proof-of-concept and I'd like to take the time to improve it and add more features. I've already tested communications with the Pi (so that the Bell Push module connects to the Pi, and another Pi connects to the Chime Module) and the code functions nicely (see blog post 9 for the source code). So, with little effort, it should be possible to use this system over any distance.

Thanks for following the project!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +5
    Well done. It's a lot of work, and I'm betting your're glad it over. A simple suggestion is to look at wireless charging. I used something very similar in the Beyond_the_phone challenge Wireless Challenge…
  • shabaz
    shabaz over 8 years ago in reply to Problemchild +4
    I think we need to develop an app, let's call it ChimeOS say, that allows users to configure on their Pi the doorbell strategy for the home, and let it accept the commands from the bell push, and then…
  • Problemchild
    Problemchild over 8 years ago in reply to mcb1 +3
    Hey Mark wouldn't the wireless charging require the charge pad to be behind the button unit which would becool but you would need to make sure the distance between the unit and the bell was very small…
Parents
  • aspork42
    aspork42 over 8 years ago

    What would you estimate the BOM cost for 10 units? I was thinking of using the pushbutton type setup as a home security monitoring device - i.e. window sensor. Instead of a pushbutton, it would be a reed switch & magnet and look for any transition to report. I would need to build up about 20 units; and would possibly use a single sensor and dual sensor unit (for two windows right next to each other). I've seen other units that cost like $40 each, so that is pretty cost prohibitive. If these are in the area of $10/unit it becomes much more feasible.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to aspork42

    Hi James,

     

    I think BoM could be reduced to $10 ballpark, especially if using (say) lower cost AAA cells, and eliminating the microswitch of course.

    One thing I'd suggest is examining the antenna closely - I thought I had got all measurements spot-on, but I've made a small error, there is a portion of the PCB antenna that looks like it has the incorrect dimension, I must have mistyped when I copied co-ordinates from the gerber file. So, although the system works, the range is just adequate until I get that sorted. Quite annoying that I missed it, but it is like a millimetre difference that was near-impossible to visually spot until I had the revision 1 board in my hand. I hope to have newer CAD files in the next few weeks. Also, it would be worth spending time seeking cost-efficient parts, because some of the inductors and capacitors are expensive, but cheaper alternatives will exist. There seems to be an industry-wide capacitor shortage recently which isn't helping : (

    There are also a few other tweaks I'd like to make to the board, although it functions today. One is that I really shouldn't have ground plane directly under the positive battery contact terminal! in case the solder resist ever accidentally scratches off : ( This was an oversight (or maybe I'm being over-paranoid about the likelihood), but ok for a rev 1 prototype where I can be extra careful with handling it all.

    Also, the tiny ceramic caps have a tendency to short when damaged, so I'd want to re-examine their positions, or perhaps specify flexible-termination caps, because an outdoor unit may end up with a flexed board when installing or over time with impacts. So it's an important thing to consider. A small resistor in series with the supply, or a polyswitch will also help to protect things in that circumstance.. there is space for such a resistor, currently a zero-ohm resistor is specified for that position. So in summary a few things are needed to improve long-term reliability.

    It would also be cool to see if there is a convenient sized enclosure out there (or 3D print something) so that the board is a good fit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 8 years ago in reply to aspork42

    Hi James,

     

    I think BoM could be reduced to $10 ballpark, especially if using (say) lower cost AAA cells, and eliminating the microswitch of course.

    One thing I'd suggest is examining the antenna closely - I thought I had got all measurements spot-on, but I've made a small error, there is a portion of the PCB antenna that looks like it has the incorrect dimension, I must have mistyped when I copied co-ordinates from the gerber file. So, although the system works, the range is just adequate until I get that sorted. Quite annoying that I missed it, but it is like a millimetre difference that was near-impossible to visually spot until I had the revision 1 board in my hand. I hope to have newer CAD files in the next few weeks. Also, it would be worth spending time seeking cost-efficient parts, because some of the inductors and capacitors are expensive, but cheaper alternatives will exist. There seems to be an industry-wide capacitor shortage recently which isn't helping : (

    There are also a few other tweaks I'd like to make to the board, although it functions today. One is that I really shouldn't have ground plane directly under the positive battery contact terminal! in case the solder resist ever accidentally scratches off : ( This was an oversight (or maybe I'm being over-paranoid about the likelihood), but ok for a rev 1 prototype where I can be extra careful with handling it all.

    Also, the tiny ceramic caps have a tendency to short when damaged, so I'd want to re-examine their positions, or perhaps specify flexible-termination caps, because an outdoor unit may end up with a flexed board when installing or over time with impacts. So it's an important thing to consider. A small resistor in series with the supply, or a polyswitch will also help to protect things in that circumstance.. there is space for such a resistor, currently a zero-ohm resistor is specified for that position. So in summary a few things are needed to improve long-term reliability.

    It would also be cool to see if there is a convenient sized enclosure out there (or 3D print something) so that the board is a good fit.