Connected Cloud Challenge
  • Challenges & Projects
  • Design Challenges
  • Connected Cloud Challenge
  • More
  • Cancel
Connected Cloud Challenge
Blog Begin the journey : Hello the World by PSoC6 Kits
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
  • Author Author: saicheong
  • Date Created: 27 Mar 2020 2:16 PM Date Created
  • Views 1168 views
  • Likes 6 likes
  • Comments 5 comments
  • amazon web services
  • dog bites
  • mailbox
  • cypress
Related
Recommended

Begin the journey : Hello the World by PSoC6 Kits

saicheong
saicheong
27 Mar 2020

An Intellectual Mailbox

Briefing of Project

Our project is build a mailbox which can detect the mail arrived and inform owner which the mail coming though cloud services, the prototype based on PSoC 6 WiFI-BT Pioneer Kit and try to minimum the BOM, the target is the final solution is simple for build and easy for use which not just amateur and consider for commerce such as power consumption, cost and the reliability.

 

The kit installed inside back side for a typical vertical mailbox which open on top.

 

Our Project based on two phases:

 

1. send notification to owner when the mail coming

2. use AI (such as Tensor Lite for embedded https://www.tensorflow.org/lite/microcontrollers ) for embedded to detect heavy dog barking, trigger the buzzer and inform owner by AWS

 

The first target is essential and second is experimenting, which the CPU of pioneer kit may not powerful enough for target or the embedded tensor engine not good enough for sound recognition.

 

We may also added the environment sensor to detect the air quality and weather and send though AWS.

 

 

First Look of the  PSoC 6 WiFI-BT Pioneer Kit

 

Thanks for the element14 community term, Cypress and Amazon AWS. We received the pioneer kit and AWS credit moment ago.

 

The Cypress Pioneer Kit, which included some jumpers, a USB-C to A cable, the Quick start guides, the kits and the TFT which is pre-housed top of main kits.

 

image

We follow the quick guides and sucess connect the device to our local Wifi network.

image

After that, I download the ModusToolbox 2.0 under cypress web-site, start the ModusToolbox 2.0 IDE, choose new application,

select kit CY8CKIT-062-WIFI-BT, select Next, choose "Hello World", Next and Finish.

 

The USB cable should connect to the KitProg3 USB ports for programming which is the Left USB port.

 

image

 

Build and Run, the RED LED flashing.

image

 

The next step is try to connect the device to AWS cloud services.

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 6 years ago +3
    I am starting to experiment on the PSoC6 too. As I have not yet received the kit I will do it on a non-WiFi version, the CY8CKIT-062-BLE that is very similar and I plan to use it anyway. Until now, with…
  • saicheong
    saicheong over 6 years ago in reply to balearicdynamics +3
    I know Cypress with PSoC creator and ModusToolbox two IDE. I am no experiments of those two package and even any Cypress MPU. I prefer multi-platform IDE that can run under unix like environment (OSX/Linux…
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to saicheong +2
    Many thanks for the clarification. I work normally on Mac OSX so PSoC Creator has been always a pain in the past as I was obliged to work on Windows VM. No problem with the VM themselves, but it is a mess…
Parents
  • balearicdynamics
    balearicdynamics over 6 years ago

    I am starting to experiment on the PSoC6 too. As I have not yet received the kit I will do it on a non-WiFi version, the CY8CKIT-062-BLE that is very similar and I plan to use it anyway. Until now, with the Cypress PSoC I have used (PSoC4 and 5) I have always used the PSoC creator; it is great, IMHO, because of the creation of projects including the right libraries and designing the electronics by blocks (that, if I am not wrong, corresponds to the internal FPGA available blocks of the Cypress PSoCs). I saw in the documentation that there are two options now. The creator has this advantage but runs on Windows only while the example you show is based on the other development environment, multiplatform Eclipse-based. What is the best solution, in your opinion?

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 6 years ago

    I am starting to experiment on the PSoC6 too. As I have not yet received the kit I will do it on a non-WiFi version, the CY8CKIT-062-BLE that is very similar and I plan to use it anyway. Until now, with the Cypress PSoC I have used (PSoC4 and 5) I have always used the PSoC creator; it is great, IMHO, because of the creation of projects including the right libraries and designing the electronics by blocks (that, if I am not wrong, corresponds to the internal FPGA available blocks of the Cypress PSoCs). I saw in the documentation that there are two options now. The creator has this advantage but runs on Windows only while the example you show is based on the other development environment, multiplatform Eclipse-based. What is the best solution, in your opinion?

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to balearicdynamics

    No opinions or suggestions? image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saicheong
    saicheong over 6 years ago in reply to balearicdynamics

    I know Cypress with PSoC creator and ModusToolbox two IDE.

    I am no experiments of those two package and even any Cypress MPU. I prefer multi-platform IDE that can run under unix like environment  (OSX/Linux), but i am fine using Windows if necessary.

     

     

    Under https://www.cypress.com/products/psoc-creator-integrated-design-environment-ide  mention 

    To evaluate and design with all available PSoC 6 MCUs, please download the ModusToolbox SW environment

    so, some of PSoC MCUs is not support by PsOC creator.

     

    Second, the ModusToolbox official support Mbed/Amazon FreeRTOS which require for AWS connect and with well document/example, as connect AWS cloud is main requirement of this challenge. 

     

    So i prefer use ModusToolbox.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to saicheong

    Many thanks for the clarification.

     

    I work normally on Mac OSX so PSoC Creator has been always a pain in the past as I was obliged to work on Windows VM. No problem with the VM themselves, but it is a mess. I have read the two options and the documentation on the cypress site when I started a few days ago and also there it is suggested to use the Eclipse-based IDE to develop all the versions of Cypress PSoC, especially those with the WiFi support. I was already very attracted to the Modus and now I have a trustable answer. This saved me a lot of test to find the right software tool for development.

     

    Enrico