Connected Cloud Challenge
  • Challenges & Projects
  • Design Challenges
  • Connected Cloud Challenge
  • More
  • Cancel
Connected Cloud Challenge
Blog #11 Water sensor calibration
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
  • Author Author: wanfp97
  • Date Created: 25 May 2020 8:16 AM Date Created
  • Views 1567 views
  • Likes 3 likes
  • Comments 0 comments
  • psoc 6
Related
Recommended

#11 Water sensor calibration

wanfp97
wanfp97
25 May 2020

Few days ago, I have got some of the component that I have ordered online. With that, I'm going to make some improvements on my water dispenser that I have designed in my previous blogpost #8 Controlling water pump using PSoC6 .

 

I have replaced the 12 NPN transistor that I used in my previous blogpost with a N-channel MOSFET and also added a water sensor to the water dispenser to detect the water level.

 

BOM: PSoC6 WiFi-BT Prototyping Kit, a water pump, two 18650 battery, 18650 battery socket, 2 N-channel MOSFET, a push button, a buzzer, a red led, a green LED, 6x 10k ohm potentiometers, some jumper wires, a bread board, a water pump and hose, a 1.5L water bottle, a 500ml water bottle, bendable steel wire, a plastic tray, hot glue gun and glue sticks.

 

GitHub: https://github.com/wanfp97/PSoC6-water-sensor-calibration

https://github.com/wanfp97/PSoC6-water-sensor-calibration

Schematic Diagram:

image

Device Configurator setting:

image

red               : strong drive input buffer off, Initial Drive State Low    

buzzer         : strong drive input buffer off, Initial Drive State Low

wtr_sense   : strong drive input buffer on, Initial Drive State High

button         : strong drive input buffer on, Initial Drive State Low

water_pump: strong drive input buffer off, Initial Drive State Low

green          : strong drive input buffer off, Initial Drive State Low    

 

Coding:

#include "cy_pdl.h" // include Peripheral Driver Library
#include "cyhal.h" // include Hardware Abstraction Layer library
#include "cycfg.h" // include device configurator library
/*******************************************************************************
* Function Prototypes
********************************************************************************/
static void button_intr_handler(void *handler_arg, cyhal_gpio_event_t event);
/*******************************************************************************
* Global Variables
********************************************************************************/
volatile bool button_intr_flag = false; // Boolean type variable to store the interrupt flag
int main(void)
{
    init_cycfg_all(); // configure pins as done in Device Configurator
    __enable_irq(); // enable interrupt
    cyhal_gpio_register_callback(button_HAL_PORT_PIN,
                                 button_intr_handler, NULL); // assigning isr handler for button
    cyhal_gpio_enable_event(button_HAL_PORT_PIN, CYHAL_GPIO_IRQ_RISE,
                                 1u, true); // interrupt on rising edge (button pressed)
    for (;;)
    {
     if (true == button_intr_flag) // if interrupt happens (button pressed)
     {
         button_intr_flag = false; // clear interrupt flag for further interrupt
         if(Cy_GPIO_ReadOut(water_pump_PORT, water_pump_NUM)==0UL)
         {
          Cy_GPIO_Write(green_PORT, green_NUM, 1UL); // green LED on
          Cy_GPIO_Write(water_pump_PORT, water_pump_NUM, 1UL); // on water pump
         }
         else
         {
          Cy_GPIO_Write(green_PORT, green_NUM, 0UL); // green LED off
          Cy_GPIO_Write(water_pump_PORT, water_pump_NUM, 0UL); // off water pump
         }
     }
     else;
     if(0UL == Cy_GPIO_Read(wtr_sense_PORT, wtr_sense_NUM))
  {
         Cy_GPIO_Write(red_PORT, red_NUM, 1UL); // red LED on
         Cy_GPIO_Write(buzzer_PORT, buzzer_NUM, 1UL); // buzzer on
  }
     else
     {
         Cy_GPIO_Write(red_PORT, red_NUM, 0UL); // red LED off
         Cy_GPIO_Write(buzzer_PORT, buzzer_NUM, 0UL); // buzzer off
     }
    }
}
/*******************************************************************************
* Function Name: button_intr_handler
********************************************************************************
* Summary:
*   GPIO interrupt handler.
*
* Parameters:
*  void *handler_arg (unused)
*  cyhal_gpio_irq_event_t (unused)
*
*******************************************************************************/
static void button_intr_handler(void *handler_arg, cyhal_gpio_irq_event_t event)
{
    button_intr_flag = true;
}

 

Explanation of the circuit:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Water sensor calibration:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The high output for the red led and the buzzer can later on be modify to use to send the stopping signal to the water dispenser to stop it when the water level is high to prevent overflow.