Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021
Blog EnergySaverHighScore - Bernhard - Design for A Cause 2021  #3 - Setup Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bernhardmayer
  • Date Created: 4 Jun 2021 1:16 AM Date Created
  • Views 778 views
  • Likes 2 likes
  • Comments 0 comments
  • mqtt
  • raspberry_pi
  • mosquitto
  • arduino_design_challenge
Related
Recommended

EnergySaverHighScore - Bernhard - Design for A Cause 2021  #3 - Setup Raspberry Pi

bernhardmayer
bernhardmayer
4 Jun 2021

Installing mosquitto

 

Setting up the Raspberry Pi is quite simple and straight forward. I used the default Raspbian image. Then a MQTT broker is needed. Under Linux this usually is mosquitto and it can be installed using the package manager.

 

So type in:

sudo apt-get install mosquitto mosquitto-clients

 

This installs mosquitto and the command line tools to control it. and this is it. Mosquitto starts automatically at every start at the system.

 

Testing mosquitto

 

As written in my previous blog post I decided to transfer the data under the topic /power_priority

 

To view all data under this topic you just type in:

mosquitto_sub -h localhost -t /power_priority

 

To send data to this topic type in:

mosquitto_pub -h localhost -t /power_priority -m 23

 

 

Automatic testing

 

These command line commands can be used to setup a script which sends values from 0 to 100 to the topic in a loop.

 

#!/bin/bash
sleeptime=2

while true; do
    i=0
    while [ $i -lt 100 ]; do echo Prio: $i  
        mosquitto_pub -h localhost -t /power_priority -m $i 
        sleep $sleeptime 
        i=$[$i+10];
    done

    while [ $i -gt 0 ]; do echo Prio: $i  
        mosquitto_pub -h localhost -t /power_priority -m $i
        sleep $sleeptime 
        i=$[$i-10];
    done

done

 

Using data from aWATTar

 

The next step is to use the data from aWATTar. Their API is described here https://www.awattar.at/services/api/

 

The prices for the next 24 hours can be obtained with

curl "https://api.awattar.at/v1/marketdata"

 

I only need the price for the running hour. So the output can be stripped using bash tools.

curl -s "https://api.awattar.at/v1/marketdata" | grep -m1 marketprice | tr -dc '0-9.'

 

This is transformed into a bash script:

 

#!/bin/bash
marketprice=$(curl -s "https://api.awattar.at/v1/marketdata" | grep -m1 marketprice | tr -dc '0-9.')
mosquitto_pub -h localhost -t /power_priority -m $marketprice

 

And this script is called every hour using cron

2 * * * * /home/pi/mqtt/awattar.sh > /dev/null

 

At the moment I directly publish the prices to the topic. For the start and testing this should be OK.