Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021

Blog

  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Open Source EMDR Machine #0. The Whole Blog

    ilvyanyatka
    ilvyanyatka
    #1. Initial Plan #2. Installation of the necessary software and libraries #3. Electronic components #4. Breadboard layout and Schematics #5. Bluetooth trouble #6. Updated breadboard layout and design changes #7. Prototype functionality and a demo vid...
    • 19 Dec 2021
  • Thank you element14

    tbriceno
    tbriceno
    I received my runner-up prize recently and loved it. I made a blog post about over here --> Runner-up prize for the 2021 Design for a Cause Challenge  I look forward to competing in another challenge soon.
    • 11 Sep 2021
  • Open Source EMDR Machine #11. An update on Software Application

    ilvyanyatka
    ilvyanyatka
    Open Source EMDR Machine. The Whole Blog.   Where to get it The Workflow. A Short Tutorial The First Screen The Second Screen The Third Screen   An update on Software Application   Where to get it   Update: I finally ...
    • 21 Jun 2021
  • EnergySaverHighScore - Bernhard - Design for A Cause 2021  #5 - Power Outlet Software

    bernhardmayer
    bernhardmayer
    Update WiFiNINA firmware The first step for working with an Arduino board with the WiFiNINA module is to update its firmware. The boards usually come with firmware 1.2.3 and this is way outdated. With the Arduino IDE it can be updated to at leas...
    • 5 Jun 2021
  • Vital Care - 07 Final Summary

    sunnyiut
    sunnyiut
    Title: Vital Care By: Md. Kamrul Hussain Project Category: Design Challenge Project Name: Design For A Cause 2021 Blog post: 08   Previous Blogs: Blog No. Title 01 Introduction 02.a SPO2 basics [PPG] 02.b SPO2 [MAX30102] ...
    • 4 Jun 2021
  • EnergySaverHighScore - Bernhard - Design for A Cause 2021  #4 - Power Outlet Hardware

    bernhardmayer
    bernhardmayer
    As I have mentioned in my previous post (EnergySaverHighScore - Bernhard - Design for A Cause 2021  #3 - Setup Raspberry Pi ) I am going to control a power outlet to do some charging of batteries when plenty of energy is available. The main cont...
    • 4 Jun 2021
  • Garden Controller, 1 week of operation update

    tbriceno
    tbriceno
    This video shows the plants at 3 different times of a 5 day period. Based on the first three days, a change was made to the code and hardware because the soil dried out and the plants started to wilt. The very next day the plants had bounced back. Af...
    • 4 Jun 2021
  • Garden controller prototype update

    tbriceno
    tbriceno
    This video update shows the plants at 3 different times during a 5 day period. It has now been a full week and is still running great. After seven days, the water level has dropped approximately an inch. This is enough to make the water level sensor ...
    • 4 Jun 2021
  • Implementing BLE in MIT App Inventor for the Garden Controller

    tbriceno
    tbriceno
    This is a longer video and I still forgot to add stuff. I will have to make another video to cover the exporting of the app for permanent install on a device. I will also provide exports for people to experiment with in that post.www.youtube.com/watc...
    • 4 Jun 2021
  • Vital Care - 05 Respiration

    sunnyiut
    sunnyiut
    Title: Vital CareBy: Md. Kamrul HussainProject Category: Design ChallengeProject Name: Design For A Cause 2021Blog post: 06 Previous Blogs:Blog No.Title01Introduction02.aSpO2 basics [PPG]02.bSpO2 [MAX30102]03Temperature04ECG - AD8232 "...
    • 4 Jun 2021
  • Trakcore #8 Refining User Experience AKA Bugs Fix

    vlasov01
    vlasov01
    Design for A Cause 2021Trakcore #1 AI Assisted Posture Modification - Project Introduction#1 - Project Introduction#2 - Acquiring Data and Designing a Model#3 - Deploying and Testing Edge Impulse ML Model on Arduino Nano 33 IoT#4 - Enabling IMU and B...
    • 4 Jun 2021
  • EnergySaverHighScore - Bernhard - Design for A Cause 2021  #3 - Setup Raspberry Pi

    bernhardmayer
    bernhardmayer
    Installing mosquitto Setting up the Raspberry Pi is quite simple and straight forward. I used the default Raspbian image. Then a MQTT broker is needed. Under Linux this usually is mosquitto and it can be installed using the package manager.&nbsp...
    • 4 Jun 2021
  • Building an Android app for the Garden controller

    tbriceno
    tbriceno
    www.youtube.com/watch This is the beginning of the mobile app for the garden controller.
    • 4 Jun 2021
  • Temperature sensing for the Garden controller

    tbriceno
    tbriceno
    I added a simple temperature sensor to know local temperature for the garden controller. It wasn't the original plan, but it will work for the prototype.www.youtube.com/watch
    • 3 Jun 2021
  • Adding a water level sensor to the Garden Controller

    tbriceno
    tbriceno
    To avoid emptying the water reservoir for the garden controller, we need to monitor the water level. This video shows the hardware and coding to accomplish the task.www.youtube.com/watch
    • 3 Jun 2021
  • Adding the water pump to the Garden Controller

    tbriceno
    tbriceno
    A look at how I added and controlled the water pump for the Garden controller.www.youtube.com/watch
    • 3 Jun 2021
  • Beginning of the coding process - Garden controller

    tbriceno
    tbriceno
    The following video is the beginning of the coding process for my project. www.youtube.com/watch
    • 3 Jun 2021
  • EnergySaverHighScore - Bernhard - Design for A Cause 2021  #2 - Concept update

    bernhardmayer
    bernhardmayer
    "good" and "bad" energy consumptionAfter a few weeks of thinking on the concept I came to the conclusion that there is "bad" energy consumption and "good" energy consumption. With more and more households getting their own solar power system they hav...
    • 3 Jun 2021
  • EnergySaverHighScore - Bernhard - Design for A Cause 2021  #1 - Introduction

    bernhardmayer
    bernhardmayer
    EnergySaverHighScorePreface I know I am a little bit late in the competition but the conecpt needed a few more thoughts on it and now I give it a start. I hope I finish in time for the deadline but I will keep the project up until it is complete...
    • 3 Jun 2021
  • Design for a Cause 2021 - Robotic Hand (Blog #8) - Code update

    dwinhold
    dwinhold
    I wanted to post the updated code I am now using for the robotic hand. This code works 100% better, it calibrates the signal for each finger for more precise movement. #if defined(ARDUINO) && ARDUINO >= 100 #include "Arduino.h&qu...
    • 3 Jun 2021
  • Vital Care - 06 Arduino IOT Cloud Integration

    sunnyiut
    sunnyiut
    Title: Vital CareBy: Md. Kamrul HussainProject Category: Design ChallengeProject Name: Design For A Cause 2021Blog post: 07 Previous Blogs:Blog No.Title01Introduction02.aSpO2 basics [PPG]02.bSpO2 [MAX30102]03Temperature04ECG - AD823205Respiratio...
    • 28 May 2021
  • Smart agro probe-blog 6 deployment and testing

    vishwasn
    vishwasn
    We will now connect the system to the cloud and deploy the model to our microcontrollerI prefer Arduino IoT Cloud as it is easy to set up for the Arduino nano iot 33 board.You need to download the agent and then allow it to scan the connected board. ...
    • 28 May 2021
  • Garden Controller working prototype overview

    tbriceno
    tbriceno
    Below is a quick video I made to show an overview of the working prototype. I am still working on getting the build videos completed and up loaded. Although the video doesn't show the Bluetooth aspect, it is functioning with data being transferre...
    • 28 May 2021
  • Remote Agriculture Solution #09: Time to See the Work in Action

    aaryan2134
    aaryan2134
    Remote Agriculture SolutionBlog Links:#01: Introduction#02: Components and Design Structure#03: Setting up the AgroBot#04: Setting up Arduino Nano 33 IOT#05: Monitoring System#06: Irrigation System#07: Pest Control System#08: Linking Everything to Ar...
    • 28 May 2021
  • DIY soil moisture sensor for garden controller

    tbriceno
    tbriceno
    www.youtube.com/watch In this video, I build a soil moisture sensor from scratch and explain its operation. In another video I will cover the code for reading the sensor with the Nano 33 IoT.
    • 28 May 2021
>