Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021
Blog EnergySaverHighScore - Bernhard - Design for A Cause 2021  #5 - Power Outlet Software
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bernhardmayer
  • Date Created: 5 Jun 2021 8:34 AM Date Created
  • Views 732 views
  • Likes 3 likes
  • Comments 0 comments
  • mqtt
  • wifinina
  • incl
  • arduino_design_challenge
Related
Recommended

EnergySaverHighScore - Bernhard - Design for A Cause 2021  #5 - Power Outlet Software

bernhardmayer
bernhardmayer
5 Jun 2021

Update WiFiNINA firmware

 

The first step for working with an Arduino board with the WiFiNINA module is to update its firmware. The boards usually come with firmware 1.2.3 and this is way outdated. With the Arduino IDE it can be updated to at least 1.3.0 and this should be done. The process is described here: https://arduino-insights.com/board/mkr-wifi-1010/wifi-firmware-update-nina-w102/

 

MQTT client

 

The Software for my controllable power outlet is mainly built around the MQTT client. There exist several MQTT libraries for Arduino but some of them only support publish and not subscribe. For my application MQTT subscribe is the main function. So I decided to go with the PubSubClient (https://github.com/knolleary/pubsubclient ).

 

Source code

 

The sketch is based on the mqtt_basic example of the library. It only subscribes to the /power_priority topic, receives the messages and compares them to a local value. If the power priority is lower the output (and the builtin led) is enabled, otherwise disabled.

 

Here is the source code:

 

#include <SPI.h>
#include <WiFiNINA.h>
#include <PubSubClient.h>

#define SECRET_SSID ""
#define SECRET_PASS ""
char ssid[] = SECRET_SSID;        // your network SSID (name)
char pass[] = SECRET_PASS;    // your network password (use for WPA, or use as key for WEP)
int status = WL_IDLE_STATUS;     // the WiFi radio's status

#define LOCAL_POWER_PRIO 70 // set local power priority
#define POWERPIN 4

IPAddress server(192, 168, 1, 61);

void callback(char* topic, byte* payload, unsigned int length) {
  char buf[10];   // local buffer
  Serial.print("Message arrived [");
  Serial.print(topic);
  Serial.print("] ");
  for (int i=0;i<length;i++) {
    Serial.print((char)payload[i]);
    if(i<10) buf[i]=(char)payload[i]; // copy to buffer
  }
  buf[9]=0;
  if(length<10) buf[length]=0;  // limit length
  Serial.println();
  float power_priority=atof(buf); // convert to float
  Serial.println(power_priority);
  if(power_priority<LOCAL_POWER_PRIO) // local power priority is higher so set everything on
  {
    Serial.println("output on");    
    digitalWrite(LED_BUILTIN, HIGH);
    digitalWrite(POWERPIN, HIGH);
  }
  else    // local power priority is higher so set everything off
  {
    Serial.println("output off");    
    digitalWrite(LED_BUILTIN, LOW);
    digitalWrite(POWERPIN, LOW);
  }
}

WiFiClient ethClient;
PubSubClient client(ethClient);

void reconnect() {
  // Loop until we're reconnected
  while (!client.connected()) {
    Serial.print("Attempting MQTT connection...");
    // Attempt to connect
    if (client.connect("arduinoClient")) {
      Serial.println("connected");
      // ... and subscribe
      client.subscribe("/power_priority");
    } else {
      Serial.print("failed, rc=");
      Serial.print(client.state());
      Serial.println(" try again in 5 seconds");
      // Wait 5 seconds before retrying
      delay(5000);
    }
  }
}

void setup()
{
  Serial.begin(57600);

  digitalWrite(POWERPIN, LOW);
  pinMode(POWERPIN, OUTPUT);

  client.setServer(server, 1883);
  client.setCallback(callback);

  while (!Serial) {
    ; // wait for serial port to connect. Needed for native USB port only
  }

  // check for the WiFi module:
  if (WiFi.status() == WL_NO_MODULE) {
    Serial.println("Communication with WiFi module failed!");
    // don't continue
    while (true);
  }

  // attempt to connect to WiFi network:
  while (status != WL_CONNECTED) {
    Serial.print("Attempting to connect to WPA SSID: ");
    Serial.println(ssid);
    // Connect to WPA/WPA2 network:
    status = WiFi.begin(ssid, pass);

    // wait 10 seconds for connection:
    delay(10000);
  }

  // you're connected now, so print out the data:
  Serial.print("You're connected to the network");
}

void loop()
{
  if (!client.connected()) {
    reconnect();
  }
  client.loop();
}

 

Video

 

The following video shows how the whole system works with a battery charger connected. The power priority is simulated by the script ramping up and down from 0 to 100.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

In the video you can see the LED at the relay going on and off and thus see the battery charging (blinking LEDs at the battery). You may even hear the sound of the relay toggling.