Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021
Blog Open source EMDR Machine #9. Explanation and examples of the code.
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ilvyanyatka
  • Date Created: 25 May 2021 4:24 AM Date Created
  • Views 1280 views
  • Likes 5 likes
  • Comments 0 comments
  • design for a cause 2021
  • Smart Led
  • c#
  • open source emdr machine
  • ws2812b
  • c#.net
  • design for a cause - design challenge
  • arduino nano 33 iot
  • design_for_a_cause_2021
  • c++ coding
Related
Recommended

Open source EMDR Machine #9. Explanation and examples of the code.

ilvyanyatka
ilvyanyatka
25 May 2021

Open Source EMDR Machine. The Whole Blog.

 

  • The Arduino side code
    • Code for the Sound
    • Code for the Smart LED strip
    • Code for the motors
    • Code for the server
      • Initialization of the server
      • To create a server
      • To get a raw GET request and create a web page on the server
      • To get parameters from a GET request string
    • The timers
  • The desktop application side code
    • Code to send a request to start the machine
    • Code to send a request to stop the machine
    • Code to create parameters of the request from EMDR model
    • When “start” request is sent - example
    • When “stop” request is sent - example

 

The whole code for this EMDR machine can be found on GitHub https://github.com/ilvyanyatka/Emdr-App-With-WiFi-Arduino-Option

 

The main calculation on how far the light ball should move and when to start/stop motors/sound is basically just Math. It is done in the Step() function. You can see it’s code in this project GitHub repository.

Below is some code to explain the other most important parts of the machine.

 

 

The Arduino side code

 

Code for the Sound

 

In the initialization section:

 

#define LEFT_SOUND_PIN 9
#define RIGHT_SOUND_PIN 10

 

 

In the loop() code, if we are less than ⅓ away from the start or end point - start the sound

 

    

if(sound>0)
      {
        if(!sound_left_on){
          
          // send signal to start left sound
          tone(LEFT_SOUND_PIN,440);
          sound_left_on = true;
        }
      }

 

440 here means 440Hz. The right channel sound is started exactly the same way.

 

And the code to stop the sound:

 

if(sound_left_on){
      noTone(LEFT_SOUND_PIN);
      sound_left_on = false;
    }




Code for the Smart LED strip

 

I learned about the FastLED library from this github repository’s code and it’s creator https://github.com/sensboston/ .

First, I installed FastLED library in Arduino IDE (Tools -> Manage Libraries -> Search for “FastLED”)



In the initialization section:

 

#include <FastLED.h>
// number of leds in the strip. In my case 5 m * 60 per m
#define MAX_N_LEDS 300
#define LED_PIN    2
CRGB leds[MAX_N_LEDS];



Initialization of LED strip in setup()

 

FastLED.addLeds<WS2812, LED_PIN, GRB>(leds, MAX_N_LEDS);

 

 

In the loop(), code to change the light ball position:

 

if(light > 0)
 {
     // turn off previous led
      setLED(prev_ledNum, 0, 0, 0);
      // highlight current led
      setLED(ledNum, r, g, b);
 }

 

Where r(ed), g(reen), b(lue) are parameters that Arduino Server gets through GET requests. There are also to_led and from_led variables, so the light ball runs only inside its borders.

 

To turn off all LEDs during “stop” request I used

 

 

  FastLED.showColor(CRGB::Black);

 



Code for the motors

 

In the initialization section:

 

#define MOTOR1_LEFT_PIN    3
#define MOTOR1_RIGHT_PIN    4
#define MOTOR2_LEFT_PIN    5
#define MOTOR2_RIGHT_PIN    6
#define MOTOR_ON HIGH
#define MOTOR_OFF LOW

 

In the setup():

 

pinMode(MOTOR1_LEFT_PIN, OUTPUT);
 pinMode(MOTOR1_RIGHT_PIN, OUTPUT);
 pinMode(MOTOR2_LEFT_PIN, OUTPUT);
 pinMode(MOTOR2_LEFT_PIN, OUTPUT);



The same as for the sound,  I start the motor if I am less than ⅓ away from the start or end point. In the loop() (code is identical for all four motors)

 

      if(motor2>0)
      {
        if(!motor2_left_on){
          // send signal to start left motor2
          digitalWrite(MOTOR2_LEFT_PIN, MOTOR_ON);
          motor1_left_on = true;
        }
      }

 

And to stop the motors

 

     if(motor2_left_on){
      digitalWrite(MOTOR2_LEFT_PIN, MOTOR_OFF);
      motor1_left_on = false;
    }



 

Code for the server

 

To use WiFi and run the server I needed to install WiFiNINA library by Arduino first ( (Arduino IDE: Tools -> Manage Libraries -> Search for “WiFiNINA”)

 

Initialization of the server

 

In the initialization section I added:

#include <WiFiNINA.h>
#include "arduino_secrets.h" // this is where ssid and passkey are stored
 
char ssid[] = SECRET_SSID;        // your network SSID (name)
char pass[] = SECRET_PASS;    // your network password (use for WPA, or use as key for WEP)
 
IPAddress local_IP(192, 168, 1, 128);
#define USE_STATIC_IP
 
int status = WL_IDLE_STATUS;
 
WiFiServer server(80);



To create a server

 

I used one of the numerous examples that come with WiFiNINA library

 

#ifdef USE_STATIC_IP
  WiFi.config(local_IP);
#endif
  
  // attempt to connect to WiFi network:
  while (status != WL_CONNECTED) {
    Serial.print("Attempting to connect to SSID: ");
    Serial.println(ssid);
    // Connect to WPA/WPA2 network. Change this line if using open or WEP network:
    status = WiFi.begin(ssid, pass);

    // wait 10 seconds for connection:
    delay(10000);
  }
  server.begin();

 

 

To get a raw GET request and create a web page on the server

 

To get the body of raw data of request I also used slightly modified sample code. In addition this code creates a webpage on the Arduino server where the therapist can start/stop the machine with default parameters. It is done just in case the therapist doesn’t have software but only the Arduino part of the machine.

 

String GetRequestValue()
{
  String result = "";
  String currentLine = "";                // make a String to hold incoming data from the client
  WiFiClient client = server.available();   // listen for incoming clients
 
  if (client) {                             // if you get a client,
    Serial.println("new client");           // print a message out the serial port
    while (client.connected()) {            // loop while the client's connected
      delayMicroseconds(10);                // This is required for the Arduino Nano RP2040 Connect - otherwise it will loop so fast that SPI will never be served.
      if (client.available()) {             // if there's bytes to read from the client,
        char c = client.read();             // read a byte, then
        Serial.write(c);                    // print it out the serial monitor
        if (c == '\n') {                    // if the byte is a newline character
          if(currentLine.startsWith("GET")){
            result = currentLine;
          }
          
          // if the current line is blank, you got two newline characters in a row.
          // that's the end of the client HTTP request, so send a response:
          if (currentLine.length() == 0) {
            client.println("HTTP/1.1 200 OK");
            client.println("Content-type:text/html");
            client.println();
 
            // the content of the HTTP response follows the header:
            client.print("Click <a href=\"/stop\">here</a> to stop emdr machine<br>");
            client.print("Click <a href=\"/start\">here</a> to start emdr machine<br>");
 
            // The HTTP response ends with another blank line:
            client.println();
            // break out of the while loop:
            break;
          } else {    // if you got a newline, then clear currentLine:
            currentLine = "";
          }
        } else if (c != '\r') {  // if you got anything else but a carriage return character,
          currentLine += c;      // add it to the end of the currentLine
        }
     }
    }
    // close the connection:
    client.stop();
    Serial.println("client disconnected");
  }
  return result;
}

 

 

To get parameters from a GET request string

 

I used this code:

//////////
// get param from command string in format param1=Aaa&param2=Bbb...
//////////
String getParam(String data, String paramName)
{
  String result = "";
  int index = data.indexOf(paramName);
  if (index >= 0)
  {
    String param = data.substring(index + paramName.length());
    index = param.indexOf("=");
    if (index >= 0)
    {
      param = param.substring(index + 1);
      index = param.indexOf("&");
      if (index >= 0) param.remove(index);
      result = param;
    }
  }
  return result;
}



The timers

 

The timer for recalculation of light position, sound and motors is set to 20ms. The timer to get new data from WiFi is set to 120ms

 

In initialization section:

 

// ms, how often run the check and update
#define STEP_INTERVAL 20
#define PARAMS_UPDATE_STEP_INTERVAL 120

 

 

In the loop():

 

 

// if less then STEP_INTERVAL ms passed - do nothing
  if(millis() - last_step_time < STEP_INTERVAL)
  {
    delay(STEP_INTERVAL);
    return;
  }
  // set time for the next check
  last_step_time = millis();
 
  // if less then PARAMS_UPDATE_STEP_INTERVAL ms passed - do nothing
  if(millis() - last_params_update_step_time > PARAMS_UPDATE_STEP_INTERVAL)
  {
     last_params_update_step_time = millis();
     // get new data from wifi
  …
  }
  // do light/sound/motor update
…





The desktop application side code

 

I wrote desktop application in c#.NET, using Xamarin forms. The idea was to make it cross platform and to work on Universal Windows Platform (UWP), Android and iOS. I cannot test it on iOS because I don’t have any Apple devices, so I kept the iOS project just in case. For Android I tested it on VS.NET Android emulator, I haven't tested it on a real Android phone yet. I assume code that involve calls to HttpClient need to be changed, probably using dependency injection like described here Xamarin and the HttpClient For iOS, Android and Windows

I just didn’t have enough time to work on it because I decided to replace the communication between the application and Arduino from BLE to WiFi at the last moment.

All the communication related code is stored in ArduinoHTTPUtils.cs file

 

Code to send a request to start the machine

 

     

public static void SendStart(EmdrModel emdrModel)
        {
            string requestString = "http://" + IP + "/start?" + CreateParamsString(emdrModel);
            // Call asynchronous network methods in a try/catch block to handle exceptions.
            try
            {
                client.GetAsync(requestString);
            }
            catch (HttpRequestException e)
            {
                Debug.WriteLine("\nException Caught!");
                Debug.WriteLine("Message :{0} ", e.Message);
            }
        }

 

 

Code to send a request to stop the machine

public static void SendStop()
        {
            string requestString = "http://" + IP + "/stop";
            // Call asynchronous network methods in a try/catch block to handle exceptions.
            try
            {
                client.GetAsync(requestString);
            }
            catch (HttpRequestException e)
            {
                Debug.WriteLine("\nException Caught!");
                Debug.WriteLine("Message :{0} ", e.Message);
            }
        }



Code to create parameters of the request from EMDR model

 

public static string CreateParamsString(EmdrModel emdrModel)
        {
            string result = "";
            //Ex. result = "light=1&sound=1&motor1=1&brightness=45&speed=20&red=128&green=0&blue=128";
            result = string.Format("light={0}&sound={1}&motor1={2}&motor2={3}&speed={4}&red={5}&green={6}&blue={7}&brightness={8}",
                emdrModel.UseLight? 1 : -1,
                emdrModel.UseSound ? 1 : -1,
                emdrModel.UseSmallTappers ? 1 : -1,
                emdrModel.UseLargeTappers ? 1 : -1,
                emdrModel.Speed,
                emdrModel.Color.R,
                emdrModel.Color.G,
                emdrModel.Color.B,
                emdrModel.Brightness);
            return result;
 
        }

 

 

When “start” request is sent - example

 

In the Xamarin form, on each PropertyChanged event for each value I send a new GET request

Ex.

 

 

private void speedSlider_ValueChanged(object sender, ValueChangedEventArgs e)
        {
            emdrModel.Speed = (int)Math.Round(e.NewValue);
            // send data to Arduino
            if (emdrModel.Platform == TargetPlatform.Arduino)
                ArduinoHTTPUtils.SendStart(emdrModel);
        }



When “stop” request is sent - example

 

When Back button is pressed or application is closed I send a GET request to stop the machine

Ex.

 

       

protected override void OnSleep() 
        { 
              ArduinoHTTPUtils.SendStop();
        }



This is pretty much it. The rest of desktop application code is GUI and the part of the application that does light/sound on PC itself.