Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021
Blog STEPS - Blog #1
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: stocktoncycles
  • Date Created: 18 Mar 2021 8:16 PM Date Created
  • Views 466 views
  • Likes 4 likes
  • Comments 1 comment
Related
Recommended

STEPS - Blog #1

stocktoncycles
stocktoncycles
18 Mar 2021

To get our Arduino creative juices flowing, we decided to build some simple projects with the neighbor kids.  Like most people out there, we started with a couple Arduino Unos and made a few blinky LED projects.  After that, we upped our game with a MPU6050 Multi-Function shield and a HC-SR04 ultrasonic range finder in order to build a lanyard-mounted social distancing meter that would help us maintain safety regulations during COVID-19.  The seven segment display showed the distance in inches and the buzzer alarms if the distance reaches less than 36".  With a little hot glue and some cardboard, we were able to mock it up into a wearable lanyard and test it throughout the house.

image

 

After that we were ready to move on to the project at hand, STEPS (Skill Training Encouragement device for People on the Spectrum).  For the hardware, we made the decision to use all off-the-shelf plug and play type modules instead of procuring individual components and rolling our own boards.  This should help to speed up the design and build process, though it makes for a clunky assembly.  We started by mocking up the hardware on a breadboard.  It makes the device a little big for a wearable, but allows us to access probe points and makes for easy troubleshooting and repair.  We plan to use this breadboard platform for the majority of the process and will only worry about form-factor once we've got all the components working together well.

image

The first portion we planned to tackle was the OLED configuration.  We used a 0.96 inch, 128 x 64 bicolor OLED screen that communicates over I2C.  Using the Adafruit SSD1306 library, we were off and rolling pretty quick with their example code.  Then we began to develop a screen layout that would work for us.  Our screen has a yellow band of pixels at the top and the others are blue.  We'll use the yellow as one region and will divide the blue into two sections.  The screen doesn't have specific functionality to clear pixel regions but we can overwrite an area with 'black' instead of 'white', which could work.  The other option is to keep all the screen information in memory and completely rewrite the entire screen each time there is an update.

image

 

While I worked on the code for the OLED, my daughter, Clara developed graphics that we'll print on some cardstock and use with RFID tags to emulate the step locations (ie: toilet handle, faucet, towel).  She will also be creating similar, small graphics to be displayed on the OLED.

  • Sign in to reply
Parents
  • aspork42
    aspork42 over 5 years ago

    Looks like you’re off to a great start.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 5 years ago

    Looks like you’re off to a great start.