Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog 5" TFT Display and Module RA8875
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
  • Author Author: roborob1266
  • Date Created: 24 Jul 2018 1:58 PM Date Created
  • Views 7014 views
  • Likes 7 likes
  • Comments 12 comments
  • ra8875
  • tft screen
  • wiring
  • design for a cause - design challenge
  • uno
  • arduino coding
  • mkr2uno
  • mkr1000
Related
Recommended

5" TFT Display and Module RA8875

roborob1266
roborob1266
24 Jul 2018

I received the Adafruit 5.0" 40-pin TFT Display 800x480 with Touchscreen PRODUCT ID: 1596 and the RA8875 Driver Board for 40-pin TFT Touch Displays 800 x 480 Max PRODUCT ID: 1590.

I had a hard time getting the display to work with the MKR1000 device so I checked the Adafruit website but no luck on the wiring diagrams or instructions.

I tried the Arduino website and no one had any information on how to wire it up. I tried Google and YouTube for any wiring videos.

I connected my Uno to the RA8875 module and put the jumper wires to the ports listed in the Arduino ino file for the ts_calibration and the TFT display lit up and I was able to get the touch readings!

So with doing that, I tried the MKR2UNO module and wired it as I did with my Uno and it didn't work.

Not be defeated, I looked at the MKR2UNO schematics and compared Pin to Pin with how I had it connected to the Uno and tried some different pins, modified the ino code for the ts_calibration under the Adafruit RA8875 library that I added to Arduino and it worked!

Here are the RA8875 pins and the MKR1000 pins that need to be used for the calibration.

RA8875/ MKR1000

VIN/ PIN 14 = +5

GND/ PIN 11 = GND

SCK/ PIN 09 = SCK

MISO/ PIN 10 = MISO

MOSI/ PIN 08 = MOSI

CS/ PIN 06 = Defined as CS in code

RST/ PIN 02 = Defined as RST

INT/ PIN 03 = Defined as INT

 

I modified the code to look like these pins:

 

#include <SPI.h>

#include "Adafruit_GFX.h"

#include "Adafruit_RA8875.h"

 

 

#define RA8875_INT     3

#define RA8875_CS      6

#define RA8875_RESET   2

 

and finally, I changed the code to reflect the 800x400 rather than the 480x272 display:

 

void setup()

{

  Serial.begin(9600);

  Serial.println("Hello, RA8875!");

 

 

  /* Initialise the display using 'RA8875_480x272' or 'RA8875_800x480' */

    if (!tft.begin(RA8875_800x480))

  {

    Serial.println("RA8875 not found ... check your wires!");

    while (1);

  }

image

  • Sign in to reply

Top Comments

  • roborob1266
    roborob1266 over 8 years ago in reply to genebren +2
    Thank you Gene! The hardship was well worth it since it is working now! Never give up, never surrender!
  • Andrew J
    Andrew J over 6 years ago in reply to roborob1266 +2
    I'm not taking account, per-se, of touch down, move release. When I ask for status (line 05), the response will be -1 if no touch detected, or another value that equates to TOUCH_PRESSED, TOUCH_MOVED,…
  • genebren
    genebren over 8 years ago +1
    Nice update on your design challenge project. Good work on getting everything connected and running. That was some first class detective work there. Gene
Parents
  • aspork42
    aspork42 over 6 years ago

    There are some other simple ways to debounce. Just read the pin. If it is HIGH (aka pressed) then do a delay(100) and read the pin again to see if it is still HIGH. If so, then you react. Like the post above mentioned, break the issue down to its core. Make a new sketch that only reads the touchscreen and does something like write to serial port or flips an LED on or off. Writing to serial port is a little tricky since it is blocking code and could mask the issue; so be sure to use a fast baud rate and print as little as possible - like a single character.

     

    Simple debounce looks like this:

     

    if(digitalRead(pin){

         delay(50); // debounce

         if(digitalRead(pin){

              //react

         }

    }

     

    Check out this post for a more in-depth look:

    https://learn.adafruit.com/make-it-switch/debouncing

    This means the pin must be depressed for at least 50 ms before the program will react. That is fast enough not to be noticed by a human, but slow enough for the system to settle out any contact bounce.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 6 years ago

    There are some other simple ways to debounce. Just read the pin. If it is HIGH (aka pressed) then do a delay(100) and read the pin again to see if it is still HIGH. If so, then you react. Like the post above mentioned, break the issue down to its core. Make a new sketch that only reads the touchscreen and does something like write to serial port or flips an LED on or off. Writing to serial port is a little tricky since it is blocking code and could mask the issue; so be sure to use a fast baud rate and print as little as possible - like a single character.

     

    Simple debounce looks like this:

     

    if(digitalRead(pin){

         delay(50); // debounce

         if(digitalRead(pin){

              //react

         }

    }

     

    Check out this post for a more in-depth look:

    https://learn.adafruit.com/make-it-switch/debouncing

    This means the pin must be depressed for at least 50 ms before the program will react. That is fast enough not to be noticed by a human, but slow enough for the system to settle out any contact bounce.