Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog Audio4Vision #9 - Interfacing Amplifier and Speaker with MKR1000
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
  • Author Author: pranjalranjan299
  • Date Created: 13 Sep 2018 3:44 PM Date Created
  • Views 1847 views
  • Likes 2 likes
  • Comments 1 comment
Related
Recommended

Audio4Vision #9 - Interfacing Amplifier and Speaker with MKR1000

pranjalranjan299
pranjalranjan299
13 Sep 2018

Welcome to our 9th blog post! In this update we are going to guide you through the process to play .wav files on the MKR1000. The components we have used are -

 

  1. Arduino MKR1000
  2. PAM 8403 Amplifier (5V with Potentiometer)
  3. Speaker (4 Ohms, 3 Watts)
  4. Jumper cables

 

Speaker 3 diameter 4 ohm 3 watt 7961087309image

                                       Speaker (8 Ohms, 3 Watts)                                                                                                                                                                      PAM 8403 Amplifier

 

The library designed for SAMD boards is called AudioZero. This library enables an Arduino Zero or MKR1000 board to play back .wav files from a storage device like an SD card. More information can be found on https://github.com/arduino-libraries/AudioZero

 

Pin diagram -

 

image

After connection -

 

imageimage

image

image

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Code -

 

#include <SD.h>
#include <SPI.h>
#include <AudioZero.h>


void setup()
{
  // debug output at 115200 baud
  Serial.begin(9600);
  while (!Serial) {
    ; // wait for serial port to connect. Needed for native USB port only
  }


  Serial.print("Initializing SD card...");


  if (!SD.begin(4)) {
    Serial.println("initialization failed!");
    while (1);
  }
  Serial.println("initialization done.");
  delay(2000);


  // 44100kHz stereo => 88200 sample rate
  AudioZero.begin(2*44100);
}


void loop()
{
  int count = 0;


  // open wave file from sdcard
  File myFile = SD.open("a.wav");
  if (!myFile) {
    // if the file't opden, print an error and stop
    Serial.println("error opening test.wav");
    while (true);
  }


  Serial.print("Playing");
  
  // until the file is not finished  
  AudioZero.play(myFile);


  Serial.println("End of file. Thank you for listening!");
  //while (true) ;
}

 

Demonstration -

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Stay tuned for our next blog!

  • Sign in to reply
Parents
  • DAB
    DAB over 8 years ago

    Interesting project.

    I look forward to seeing this build progress.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 8 years ago

    Interesting project.

    I look forward to seeing this build progress.

     

    DAB