Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog Blowing-Whistle as Controller(BWaC) ----- Analyse the Spectrum with ArduinoFFT #4
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
  • Author Author: fyaocn
  • Date Created: 17 Aug 2018 6:03 AM Date Created
  • Views 1996 views
  • Likes 6 likes
  • Comments 4 comments
Related
Recommended

Blowing-Whistle as Controller(BWaC) ----- Analyse the Spectrum with ArduinoFFT #4

fyaocn
fyaocn
17 Aug 2018

Analyse the Spectrum with ArduinoFFT

1. The ISD1820 is microphone module, the analogue value shall be turned into digital value for processing purpose. 

Pin A0 is set as INPUT, fetching data form ISD1802.

int inputPin = A0;

The following codes do the job with adcTune function, the analogueRead(A0) pins is set for sound wave catching.

void adcTune(double *vReal,double *vImag ,int *readings)
{
  // read from the sensor AND advance to the next position in the array:
  //for (int  readIndex= 0; readIndex < numReadings; readIndex++) {    readings[readIndex] = analogRead(inputPin);  }
  for (int  readIndex= 0; readIndex < numReadings; readIndex++){
    delay(CYCLETIME); // delay fpr cycle
    readings[readIndex] = analogRead(inputPin); 
    }
   
      for (int i = 0; i < numReadings; i++) {
      vReal[i] = readings[i] ;/* Build data with positive and negative values*/
      vImag[i] = 0.0; 
        }
}

imageimage

 

2. The easiest solution to process the digital data is by FFT algorithm. There would be considerable amount of calculation for fast process, especially for low performance Cortex-M0 core. The arduinoFFT library can handle the calculation in short time. There have been many technique in fast calculation on Complex data, and the result is good.

image

In this test, only peak frequency is printed. In fact , the spectrum is available for further encryption. 

In function fftTune(), there are three sub-steps like FFT.windowing(), FFT.Compute(), FFT.ComplexToMagnitude(). After that, FFT.MajorPeak() can pick the peak frequency within the spectrum.

void fftTune(double *vReal,double *vImag, uint16_t samples)
{
         FFT.Windowing(vReal, samples, FFT_WIN_TYP_HAMMING, FFT_FORWARD);  /* Weigh data */
        FFT.Compute(vReal, vImag, samples, FFT_FORWARD); /* Compute FFT */
        FFT.ComplexToMagnitude(vReal, vImag, samples); /* Compute magnitudes */
        Serial.println("Computed magnitudes:");
        PrintVector(vReal, (samples >> 1), SCL_FREQUENCY);
        double x = FFT.MajorPeak(vReal, samples, SAMPLINGFREQUENCY);
}

  • Sign in to reply

Top Comments

  • prashanth.nagendrappa
    prashanth.nagendrappa over 8 years ago +1
    Nice Update
  • aspork42
    aspork42 over 8 years ago +1
    Nice update - I was wondering about the reading you got. Your previous post noted a frequency of ~2735 Hz. This shows around 241 Hz. I wonder what value you have for delay(CYCLETIME); Since that could…
  • fyaocn
    fyaocn over 8 years ago in reply to aspork42 +1
    Code in the sketch #define CYCLETIME 1 means only 1 ms is set. The 241Hz is test results when I tap the table. It varies around 200Hz~350Hz if you can try. As to frequency over 2kHz, that is a challenge…
Parents
  • genebren
    genebren over 8 years ago

    Nice update on your design challenge project.  The ArdunioFFT processing looks pretty powerful.  Do the results match with your other experiments?

    Keep up the good work.

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Nice update on your design challenge project.  The ArdunioFFT processing looks pretty powerful.  Do the results match with your other experiments?

    Keep up the good work.

    Gene