Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog Completed Project!
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
  • Author Author: roborob1266
  • Date Created: 31 Aug 2018 2:36 AM Date Created
  • Views 5311 views
  • Likes 17 likes
  • Comments 15 comments
  • adxl335eb
  • ra8875
  • hc-sr04
  • autism assistant
  • adafruit vs1053 mp3 player
  • design for a cause - design challenge
  • uno
  • mkr1000
  • adafruit ra8875
Related
Recommended

Completed Project!

roborob1266
roborob1266
31 Aug 2018

Hello all

I completed my project! Here are two photos of the devices used in this project.

1. MKR1000 (Arduino Board included in KIT

2. ADXL335EB (Tilt Sensor - included in KIT)

3. HC-SR04 (Ultrasonic Sensor - included in KIT)

4. RA8875 (Video Module - Adafruit Item 1590)

5. 5" Touch Screen display  (Adafruit Item 1596)

6. MP3 Player Music Shield (Adafruit Item 1788)

7. Arduino UNO

8. Jumper Wires (included in KIT)

9. USB cables for both the UNO and MKR1000 (USB cable included for MKR1000 in KIT)

imageimage

 

 

Also, if anyone knows where to submit this for the Competition, please let me know so I can make sure it is submitted on time!

Thanks!

 

As a side note, the SD Proto Shield never worked out of the box. I tried touching the solder points but it didn't help, I researched about it on different forums and found out that there were a batch of these that were defective and needed to be replaced.

That is why I purchased and used the VS1053 MP3 Player with SD shield attached and it worked just fine!

 

Video of my project!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +6
    Hi Rob, Congrats! It's a great project.. nice to see it finally in action, your perseverance paid off! I'm working on something slightly similar as a side project, but it's dragging for me : )
  • aspork42
    aspork42 over 8 years ago +5
    Great job! I like what you have done! I think you still have some time left in the official contest so if there are other things you want to work out you might be able to. It would be cool to see icons…
  • 14rhb
    14rhb over 8 years ago +5
    Hi Rob, Very impressive work, well done on completing it Rod
Parents
  • aspork42
    aspork42 over 8 years ago

    Great job! I like what you have done!

     

    I think you still have some time left in the official contest so if there are other things you want to work out you might be able to. It would be cool to see icons displayed on the screen - I know you wanted to add that in.

     

    What about the possibility of some sort of case for this to make it a little more robust and mobile that someone can bring it with them?

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • roborob1266
    roborob1266 over 6 years ago in reply to aspork42

    Hi James.

    I am resurrecting this project with a Mega 2560 and I am running into a bit of a problem.

    When I touch the screen, the section I press on the touch screen, plays the audio twice. I am figuring that it is counting when i touch the screen and when i let off of the screen.

    What I am reading is that this is probably a debounce problem. I am going to have to research on software debounce unless there is a hardware resolution like a capacitor in line with the input that goes into the RA8875 chip.
    I am not sure what to do at this point. Any suggestions would be appreciated.

    I am willing to send you my code to look at if you like. if you send me an email address, i can send it. I would rather not post the code on here till its all done.

     

    Regards,

    Rob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • roborob1266
    roborob1266 over 6 years ago in reply to aspork42

    Hi James.

    I am resurrecting this project with a Mega 2560 and I am running into a bit of a problem.

    When I touch the screen, the section I press on the touch screen, plays the audio twice. I am figuring that it is counting when i touch the screen and when i let off of the screen.

    What I am reading is that this is probably a debounce problem. I am going to have to research on software debounce unless there is a hardware resolution like a capacitor in line with the input that goes into the RA8875 chip.
    I am not sure what to do at this point. Any suggestions would be appreciated.

    I am willing to send you my code to look at if you like. if you send me an email address, i can send it. I would rather not post the code on here till its all done.

     

    Regards,

    Rob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • aspork42
    aspork42 over 6 years ago in reply to roborob1266

    I'll PM you. We should post the findings back here so the community can see. I re-watched the video and it looks like some of them are likely double-playing. The arduino code from the Uno should be enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aspork42
    aspork42 over 6 years ago in reply to aspork42

    Rob - so I can't seem to PM you with how the site is set up. You should be able to message me however. Can you have a try at that?