Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog 19 - MagicHat first words
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
  • Author Author: amgalbu
  • Date Created: 12 Jun 2015 11:08 AM Date Created
  • Views 2056 views
  • Likes 4 likes
  • Comments 8 comments
  • enchanted_objects
  • tts
  • magic_doctor_hat
  • arduino
  • speaker
Related
Recommended

19 - MagicHat first words

amgalbu
amgalbu
12 Jun 2015

I completed the mouth and the MagicHat now can speak.

I had to make some changes to the circuit for reading audio output. The new version includes two resistors and a capacitor to shift up voltage level by 2.5V

 

image

 

Using an headphone, I cut off one of the speakers and added a connector to be connected to the Arduino board

 

image

 

The video shows MagicHat saying its first word. "Hello". Unfortunately audio quality is not that good due to my smartphone limitations, but it gives the idea!

In the video, you can also see all the hardware ready to be installed

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 11 years ago +1
    I like it, nice idea using the headphone as a mini-speaker.
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    I like it, nice idea using the headphone as a mini-speaker.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    Nice.

    It's possible to let the Arduino generate the text-to-speech on its own without a sound card.

    It uses one of the PWM pins to generate the audio (bitbanging speech image ). Send it trough a low pass filter and amplify.

    The sound is horrid, but it's fun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to Jan Cumps

    Hi Jan

    I made some preliminary test with libraries like Cantarino, but the speech is unaudible!! Do you have a solution for that?

     

    Cheers

    Ambrogio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to amgalbu

    Just a silly idea. Why not a simple 1 transistor amplifier ? I think you can do it with minimal components and there are tons of projects around.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to amgalbu

    Just a silly idea. Why not a simple 1 transistor amplifier ? I think you can do it with minimal components and there are tons of projects around.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to balearicdynamics

    Here's an example where I did it with a one transistor amplifier:

     

    [Christmas Wreath of Things] Internet of Holiday Lights - Bonus kicker: the IoT talks (a spoken tribute to Science Fair kits)

     

    It's very difficult to understand - it's nothing more than a gimmick - but then again my low pass filter pas pathetic. But a fun project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to balearicdynamics

    Hi Enrico

    That's a good idea. Voice can be heard easily in a quiet enviroment but it's not loud enough to be heard in a noisy room. Definetely there are a lot of possible improvements, this is one of them... unfortunately it's a busy time for me so for the moment my hope is to complete the project!

     

    Cheers

    Ambrogio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to Jan Cumps

    Thanks Jan!