Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog A place in the cloud Post #1 - Overview and what I did over Easter.
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
  • Author Author: e14 Contributor
  • Date Created: 7 Apr 2015 3:55 AM Date Created
  • Views 543 views
  • Likes 3 likes
  • Comments 5 comments
  • atmel_sama5d4
  • place_cloud
  • enchanted_objects
Related
Recommended

A place in the cloud Post #1 - Overview and what I did over Easter.

e14 Contributor
e14 Contributor
7 Apr 2015

Hi All,

 

My project synopsis for those who didn't see my application is quite basic in its theory. What I intend to do is create an IoT message bus and transaction system.

I will either roll my own, or something off the shelf with RabbitMQ and then build an API so that devices can readily communicate their results across the network

into the message queueing system and have them displayed in a portal.  Of course there are solutions out there that do this already, but there is no harm in rolling

your own proof of concept.  I want to do this so I can continue to customise my solution down the track and be able to control how I interact both from the client side and the

server side.

 

Now onto what I did over the Easter weekend long weekend..

 

Well I received my kit of parts from Element 14 and after building my new desk on Friday night I was finally in a position to get setup and start work on this design challenge.

Warning.. picture may contain traces of easter eggs... :-)

image

My new corner L shaped desk. 2100mm x 2100mm x 750mm x 730mm (length x width x height)

image

 

I'd read a lot about the Atmel SADA5D4 and the trouble people were having, so I figured, let's give this a go. It can't be that hard, right?

Glad to see that people were not exaggerating. If you want a lesson in calm and patience, buy yourself one of these and try to figure out how to make

it work.  I managed to get the serial interface working so I could actually talk to the device and was able to build myself a new linux kernel based on Ubuntu.

Currently I am failing because my unix VM can't properly mount my SDCard, which means I can't easily write the OS to the card, but I'll overcome that in the next day or two, I hope.

 

The operating system installed on the SAMA5D4 is a huge disappointment. The implementation is severely lacking in those everyday tools which could have made

this SBC into a 5 star performer. Had they been able to bundle it with a more complete implementation of UNIX, or even standardised it a little more towards Debian and given us an install

where we could readily use a development toolchain it would have immediately changed how the board can be used. What they really need to do is re-evaluate the board

and enable the functionality that exists on the board via the various interfaces. A good example of this is the HDMI port.

If you are providing a HDMI port, at least include the necessary modules to allow the HDMI port to be used as a console.

 

I could see this card easily rivalling a Raspberry Pi 2 if a bit more forethought had been put into the software/operating system layer of the card.

 

Now there are a couple of useful tools installed, there is a http light server as well as python. I could probably use these to roll my own MQ, so even in its vanilla flavour, the SAMA5D4 may

prove to be useful yet. I just can't spend a lot of time working against the tools, I'd rather work with them.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago +1
    JokerZ , your project tags are missing in your post. There are two tags, 'enchanted_objects' and <a specific tag for your project> that mark that your blog is for Enchanted Objects. Your tag is documented…
  • nikil511
    nikil511 over 11 years ago +1
    Hi Rob, SAMA5D4 is using Intel's Yocto. Professionals think highly of it, and I can guess why, but for diy people it might not (yet) be a perfect match. Eitherway the features of the pre-installed distro…
Parents
  • Jan Cumps
    Jan Cumps over 11 years ago

    JokerZ , your project tags are missing in your post.

    There are two tags, 'enchanted_objects' and <a specific tag for your project> that mark that your blog is for Enchanted Objects.

    Your tag is documented here: http://www.element14.com/community/docs/DOC-75182/l/enchanted-objects-challenge-competitors

     

    Regards, Jan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 11 years ago

    JokerZ , your project tags are missing in your post.

    There are two tags, 'enchanted_objects' and <a specific tag for your project> that mark that your blog is for Enchanted Objects.

    Your tag is documented here: http://www.element14.com/community/docs/DOC-75182/l/enchanted-objects-challenge-competitors

     

    Regards, Jan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Jan Cumps

    Thanks Jan,

    appreciate the help. It should now all be sorted.


    Regards

    Rob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to e14 Contributor

    Yep image