Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects - Enchanted Clock (#3)
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
  • Author Author: dwinhold
  • Date Created: 4 Apr 2015 11:11 PM Date Created
  • Views 927 views
  • Likes 6 likes
  • Comments 4 comments
  • enchanted_objects
  • enchanted_clock
Related
Recommended

Enchanted Objects - Enchanted Clock (#3)

dwinhold
dwinhold
4 Apr 2015

Hello everyone,

 

So I have been programming the Arduino for enchanted clock I'm building (Work in progress). I am still having issues with the SAMA5D4 Xplained, I may have to change to an RPi if time starts to get tight. I really don't want to do this as our sponsors have been very generous and I don't want to let them down.

 

So to update where I am at. I have decided that for the clock to stay in time due to the inconsistency in a wood clock, I have made a binary clock. This clock will be integrated with my wood clock and through servos it will re-set it to the correct time. Below is a picture of the Binary Clock on the breadboard working. I will make a PCB board cape for final product. The time on the Binary Clock will be seen as well as the wood clock time.

 

image

 

 

Schematic:

image

Clock Code:

 

#include <Wire.h>
#include <RTClib.h>
#include <TimerOne.h>

byte numPins = 5;
byte ledPins[] = {2, 5, 8, 10, 12};

byte hourLeds[][2] = {{1, 3}, {3, 1}, {0, 3}, {3, 0}};
byte minLeds[][2] = {{4, 2}, {3, 4}, {2, 3}, {1, 2}, {0, 1}, {2, 0}};
byte secLeds[][2] = {{2, 4}, {4, 3}, {3, 2}, {2, 1}, {1, 0}, {0, 2}};

RTC_DS1307 RTC;

int hour, min, sec;

void setup()
{
  Wire.begin();
  if (! RTC.isrunning())
  {
    RTC.adjust(DateTime(__DATE__, __TIME__));
  }
  Timer1.initialize(20000); // uS
  Timer1.attachInterrupt( refresh );
}

void loop()
{
  static long lastTick;
  long thisTick = millis();
  if (thisTick > lastTick + 500l) // every 0.5 seconds
  {
    DateTime now = RTC.now();
    hour = now.hour();
    min = now.minute();
    sec = now.second();
    lastTick = thisTick;
  }
  refresh();
}

void refresh()
{
  int s = sec;
  int m = min;
  int h = hour;
  for (int bit = 0; bit < 6; bit++)
  {
    if (s & 1)
    {
      setLed(secLeds[bit]);
     // delay(10);
    }
    s = s >> 1;
    if (m & 1)
    {
      setLed(minLeds[bit]);
    }
    m = m >> 1;
    if (h & 1 && bit < 4)
    {
      setLed(hourLeds[bit]);
    }
    h = h >> 1;
   }
   allOff(); // so last led not brighter
}

void setLed(byte pins[])
{
  byte plusPin = ledPins[pins[0]];
  byte minusPin = ledPins[pins[1]];
  allOff();
  pinMode(plusPin, OUTPUT);
  digitalWrite(plusPin, HIGH);
  pinMode(minusPin, OUTPUT);
  digitalWrite(plusPin, LOW);
}

void allOff()
{ 
  for (byte pin = 0; pin < numPins; pin++)
  {
    pinMode(ledPins[pin], INPUT);
  }
}

 

Servo controller and timing sensor to be programmed into the script, this is for the clock only (so far).

 

My big focus is on the wooden clock, this is a huge part in the whole project. I will update mid week with photos of the progress.

 

Dale & Chrystal Winhold

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 11 years ago +2
    Good job. Like the idea of a binary clock.
  • Workshopshed
    Workshopshed over 11 years ago +2
    It took me a while to work out the LED wiring but I got it eventually, very cunning.
  • mcb1
    mcb1 over 11 years ago +2
    How long did it take you to work out that wiring. I had a headache just trying to follow it ... full marks. Mark
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    It took me a while to work out the LED wiring but I got it eventually, very cunning.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago

    It took me a while to work out the LED wiring but I got it eventually, very cunning.