Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects - Enchanted Clock #7 - Voice recognition
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
  • Author Author: dwinhold
  • Date Created: 8 Jun 2015 2:49 AM Date Created
  • Views 1161 views
  • Likes 6 likes
  • Comments 2 comments
  • design_challenge
  • enchanted_objects
  • enchanted_clock
Related
Recommended

Enchanted Objects - Enchanted Clock #7 - Voice recognition

dwinhold
dwinhold
8 Jun 2015

Sorry for the delay in this posting, between working 7 days a week for the past 3 weeks and family I got a bit behind on blogging.

 

Chrystal has been working on the thermostat regulator with the servo for  a bit now. She is wanting to do it on her own so I am letting her learn about the motor and connecting it to the Arduino. She is starting to program it to turn on and off, this has been frustrating at times but she hasn't backed off. I have pictures of her getting mad with frustration but can't post them (She threatened me with pictures she has taken). She is getting it, wait until I tell her it will be integrated into the voice recognition. image

 

For the voice recognition update:

 

I am using the Voice Recognition Module V3 "Speak to Control".

 

It is a speaker-dependent voice recognition module. It supports up to 80 voice commands in all. Max 7 voice commands could work at the same time. Any sound could be trained as command. This board has 2 ways to control: Serial Port (full function), General Input Pins (part of function). General Output Pins on the board could generate several kinds of waves while corresponding voice command was recognized.

 

 

Controllers information:

 

 

 

 

 

Parameter

 

 

 

● Voltage: 4.5-5.5V

 

● Current: <40mA

 

● Digital Interface: 5V TTL level for UART interface and GPIO

 

● Analog Interface: 3.5mm mono-channel microphone connector + microphone pin interface

 

● Size: 31mm x 50mm

 

● Recognition accuracy: 99% (under ideal environment)

 

 

 

 

Feature

 

 

 

 

 

● Support maximum 80 voice commands, with each voice 1500ms (one or two words speaking)

 

● Maximum 7 voice commands effective at same time

 

● Arduino library is supplied

 

● Easy Control: UART/GPIO

 

 

● User-control General Pin Output

 

 

 

Here is a link to the Voice Recognition V3 Arduino library (Download zip file)

 

 

Below are pictures of the module, programming the module and a video of it in operation:

 

image

 

image

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The wooden clock is coming along very well, I want to save displaying any pictures of it until I'm complete. This project is the best Chrystal and I have ever done, we continue to learn more about electronics and programming every day.

 

 

Thank you for reading and watching,

 

Dale and Chrystal Winhold

  • Sign in to reply

Top Comments

  • dwinhold
    dwinhold over 11 years ago in reply to Workshopshed +1
    The nice thing about this module is you don't require a usb-ttl adaptor to program it. It can all be done through the Arduion.
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    Hi Dale, Chrystal,

    that's an interesting module, they are obviously keen for people not to reverse engineer the board as they've gone to the effort of potting it. I see on the website that even the previous version has the manufacturer details removed from the chip  http://www.elechouse.com/elechouse/index.php?main_page=product_info&cPath=168_170&products_id=2151

    I look forward to seeing the wooden clock.

    Cheers,

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago

    Hi Dale, Chrystal,

    that's an interesting module, they are obviously keen for people not to reverse engineer the board as they've gone to the effort of potting it. I see on the website that even the previous version has the manufacturer details removed from the chip  http://www.elechouse.com/elechouse/index.php?main_page=product_info&cPath=168_170&products_id=2151

    I look forward to seeing the wooden clock.

    Cheers,

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dwinhold
    dwinhold over 11 years ago in reply to Workshopshed

    The nice thing about this module is you don't require a usb-ttl adaptor to program it. It can all be done through the Arduion.