Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects Design Challenge - Planning and Building
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
  • Author Author: Workshopshed
  • Date Created: 24 Jun 2015 12:32 PM Date Created
  • Views 1986 views
  • Likes 3 likes
  • Comments 7 comments
  • enchanted_cottage
  • enchanted_objects
Related
Recommended

Enchanted Objects Design Challenge - Planning and Building

Workshopshed
Workshopshed
24 Jun 2015

Planning and Research

The project was planned by creating a calendar of the 15 weeks in a spread sheet then mapping the high level tasks to the weeks. Two weeks were left empty to allow for issues and overruns. Critical path items such as the house were ordered early on and potentially long lead time items such as the battery were ordered as soon as possible.

image

I knew that I would be out of town for a couple of weeks during the project so I effectively did twice the work in the preceding weeks so that I could have something to show. Many of the posts were drafted well ahead of time and photos or videos were added when they became available, the topics were re-ordered as necessary and some topics dropped or added. The story lines were often written on the way to work in the mornings.

 

I was not familiar with the Arduino Yún and some of the electronics so lots of research was done into these during my commute from work or during lunch times.

 

Nearing the end of the project, roughly around the start of June the remaining tasks were drawn up into a "snagging list" each being a single low level item such as "paint frame", "C++ code for blinking LED" etc. This meant that the list of things to do grew quite rapidly but because each was smaller and more focused they also got completed quickly. It also allowed "non-critical" items to be discarded.

 

The last week was reserved for commissioning but unfortunately some software items over ran and had to be completed that week too.

 

The Build Process

 

The process of building was to strip down the old weather house to analyse how the new mechanism could be added. After removing the old mechanism the house was fixed back together. The roof was made so that it could be lifted on and off. The new framework was intentionally made to be stand-alone, this allowed changes to be made without risking filling the house full of holes. It also allowed testing to be done without risking damaging the house. Where possible the new parts added were from the kits provided. The electronics and coding was done in a modular fashion with each component being constructed and fine tuned before incorporating into the over all design.

 

Next: Enchanted Objects Design Challenge - Testing

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 11 years ago +1
    You should have been a project manager! Great job. Clem
  • mcb1
    mcb1 over 11 years ago +1
    Seems to have come together nicely. Unfortunately we have seen many other challengers fail because they either don't plan early enough or try to wait rather than juggle things. The story lines were often…
  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed +1
    I only have 15km to go ...well if it was a straight line. Unfortunately someone stuck a river in the way so its a 35km road trip. The bottleneck is that since the earthquakes, everyone moved out to the…
Parents
  • mcb1
    mcb1 over 11 years ago

    Seems to have come together nicely.

     

    Unfortunately we have seen many other challengers fail because they either don't plan early enough or try to wait rather than juggle things.

     

    The story lines were often written on the way to work in the mornings.

    Hopefully you don't drive image ...I'd have trouble with this ..... despite the slow traffic flow.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1

    No, I get a bus and either a tube + train or two tubes to get to the office. The best time was 1hr 20minutes, the worst was 3hrs but that did involve quite a lot of walking.

     

    If look at a map of London, I have to get from the top right to the bottom left each time I visit the office.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed

    I only have 15km to go ...well if it was a straight line.

    image

     

    Unfortunately someone stuck a river in the way so its a 35km road trip.

    The bottleneck is that since the earthquakes, everyone moved out to the North and hence everyone converges on the one bridge to cross it .....

     

    If there is no traffic its 25mins, but from 7am it's more like an 1 -1.5hrs ...and that is using the shortcuts.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to mcb1

    LOL. Mark I have no river in the way, just a silly airport to get around with much traffic at rush hour. The names on your map are interesting. Is this Belfast as in Northern Ireland?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 11 years ago in reply to mcb1

    LOL. Mark I have no river in the way, just a silly airport to get around with much traffic at rush hour. The names on your map are interesting. Is this Belfast as in Northern Ireland?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 11 years ago in reply to clem57

    No ..... Christchurch, New Zealand.