Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects Design Challenge - Sleeping Golem
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
  • Author Author: Workshopshed
  • Date Created: 21 May 2015 8:19 AM Date Created
  • Views 3012 views
  • Likes 5 likes
  • Comments 13 comments
  • enchanted_cottage
  • sleep
  • enchanted_object
  • winners
  • arduino_yun
Related
Recommended

Enchanted Objects Design Challenge - Sleeping Golem

Workshopshed
Workshopshed
21 May 2015

Putting the Arduino Yun to sleep

 

Hans and Matilda thought back to the Golem and how he slept between each activity, that could also work for their Yún.

  

The key things were:

 

  • Turning the Linino power off
  • Turning the Linino power back on
  • Low power on the ATMega side
  • Waking back up.
  • Timers and servo.

 

Poweroff is not enough

 

The Linino O/S uses BusyBox for a lot of the tasks of it's shell. One of these is the "poweroff" command. http://www.busybox.net/BusyBox.html#poweroff

Running this with the multimeter in the loop to check the current we see that running poweroff makes no difference to the current draw, the Yún still takes 200mA.

 

/*
  Running shell commands using Process class.
  based on http://arduino.cc/en/Tutorial/ShellCommands
*/

#include <Process.h>

int ledPin = 13;                 // LED connected to pin 13

void setup() {
  pinMode(ledPin, OUTPUT);      // sets the digital pin as output

  pinMode(A5, OUTPUT);
  digitalWrite(A5, HIGH);    // sets the Linino on

  Bridge.begin();    // Initialize the Bridge

  Process p;
  p.runShellCommandAsynchronously("poweroff"); // Run in background so process returns

  digitalWrite(ledPin, HIGH);   // sets the LED on
}

void loop() {
}

 

Test points and wired control

 

A discussion on the Arduino forum lead to a part of the schematic that controlled the 3.3v regulator. The RT8010 regulator has a two test points TP51 and TP52 (bridged by a 0ohm resistor). The author kindly points out where those test points are located as there's no silk screen indicating which are which. As per the example the corner I/O pin was used, A5.

image

image

Retrospectively they remembered that the A5 pin is shared with the I2C bus on the Uno, luckily this is not the case for the Yún.

The software control for this is pretty straight forward too, it can be controlled as a digital pin. You'd want to wait until any writing to disk was complete before powering off so that will need to be factored into the software. Using that control the consumption drops to 30mA.

 

int ledPin = 13;                 // LED connected to pin 13

void setup()
{
  pinMode(ledPin, OUTPUT);      // sets the digital pin as output
  pinMode(A5, OUTPUT);
}

void loop()
{
  digitalWrite(A5, LOW);   // sets the Linino off
  digitalWrite(ledPin, HIGH);   // sets the LED on
  delay(8000);                  // waits for a 8 seconds
  digitalWrite(A5, HIGH);    // sets the Linino on
  digitalWrite(ledPin, LOW);    // sets the LED off
  delay(8000);                  // waits for 8 seconds
}

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

You are getting sleepy, very sleepy

But it's possible to even better than that. The commands to put the Arduino to sleep are pretty straightforward even so Hans took the approach of using a library. RocketScream had produced one that made life pretty simple so the code example was extended to incorporate that.

 

//Library from http://www.rocketscream.com/blog/2011/07/04/lightweight-low-power-arduino-library/#sthash.PhJ0PF9f.dpuf
#include "LowPower.h"

int ledPin = 13;                 // LED connected to pin 13

void setup()
{
  pinMode(ledPin, OUTPUT);      // sets the digital pin as output
  pinMode(A5, OUTPUT);
  delay(25000);                 // Nice long delay to help with reprogramming    
}

void loop()
{
  digitalWrite(A5, HIGH);    // sets the Linino on
  digitalWrite(ledPin, LOW);    // sets the LED off
  delay(8000);

  digitalWrite(A5, LOW);   // sets the Linino off
  digitalWrite(ledPin, HIGH);   // sets the LED on

  delay(8000);                  // waits for a second
  digitalWrite(ledPin, LOW);   // both lights off, power and P13

  //Sleep
  LowPower.powerDown(SLEEP_8S, ADC_OFF, BOD_OFF);
}

 

The multimeter uses a different socket for currents over 200mA so a cable swap and photo was taken to get a more accurate reading of the lowest current. For the powerDown the Watchdog timer is used and hence Timer0 which is used for Millis() is turned off and Timer1, used by the Servo() library is also off. This will affect the flashing/colour cycling of the LED and servo so that needs to be factored in the the code.

 

This brings the power down to 2.5mA, approx 80th of the original power required or 33 days of runtime from the battery. Obviously the bursts of activity will bring this down but a week's run time seems achievable.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

image

It may also be possible to reduce even more power by permanently turning off those peripherals such as the ADC which are not used although because of the devices used in the project most of the peripherals are used and there may be more effective ways to save power such as minimising the time that the Linino part is powered up.

 

Next: Enchanted Objects Design Challenge - The townsfolk get Rickrolled

 

Reference

 

BusyBox - The Swiss Army Knife of Embedded Linux

Arduino Yun - put linux environment to sleep or halt

Arduino, Zigbee and Embedded Development: Sleeping Arduino - Part 1

http://www.rocketscream.com/blog/2011/07/04/lightweight-low-power-arduino-library/

Advanced Arduino: direct use of ATmega counter/timers

<avr/power.h>: Power Reduction Management

Sparkfun Adventures in Low Power Land

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 11 years ago +2
    Caution: If you've copied the original code I recommend swapping it with this updated version as the sleep makes it challenging to re-programme the device. I'll do something with the final version of the…
  • Workshopshed
    Workshopshed over 11 years ago +2
    Looking at Gammon Forum : Electronics : Microprocessors : Power saving techniques for microprocessors it would appear that I can turn off the ADC for a bit of power consumption improvements. Jan Cumps…
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps +1
    You can see it in the lower picture, all the lights are off on the Yún. I'm measuring the current after the power board so that super bright blue LED isn't included in the measurement, so that would be…
Parents
  • Jan Cumps
    Jan Cumps over 11 years ago

    You could also desolder the leds from the Arduino to eek that last mAH out of the battery.

     

    The 3.3V power led (3.3V - LED voltage drop) / 560R.

     

    (this may not be worth it, because they aren't on permanently)

    Wireless led when on (VPIN - LED voltage drop / 270R

    USB and WAN led when on : (3.3V - LED voltage drop / 330R,

     

    Even if you manage to loose 1mA (3.3V - 2.5V)/560R = 1.4mA, that's still a significant part of your 2.5mA sleep consumption.

    Yeah, I know, for the battery this 1mA doesn't really matter, but you can brag that you powered the Yún down by more than that that factor 80. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps

    Once the RT8010 is disabled then all of the 3.3v LEDs go off. In the second video you can see all the lights going off, green power comes back on a the orange tx flashes. I'm using the red pin13 LED to show when it's just running the ATMega at 30mA.

    There's quite a lot of other things on the board, perhaps the level shifters or the AU6350 SDCard/USB Bus chip add up as the ATMega should be using a lot less than 2.5mA when it's asleep.

    It might be interesting to see if pulling out the SDCard makes a difference?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    I couldn't watch the video yet because I'm uploading one myself to youtube. Upload just eats away all my bandwidth .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps

    You can see it in the lower picture, all the lights are off on the Yún. I'm measuring the current after the power board so that super bright blue LED isn't included in the measurement, so that would be a candidate for removal...

    On a related note you can control some of those LEDs in software Arduino Yun LEDs

     

    There's also some stuff here about running at a lower voltage and/or frequency.  Gammon Forum : Electronics : Microprocessors : Power saving techniques for microprocessors

    I suspect my biggest power savings are going to be minimising the time that the Linino section is running. I believe the boot time is 60s but I've not actually measured that or worked out what I can do to reduce it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps

    You can see it in the lower picture, all the lights are off on the Yún. I'm measuring the current after the power board so that super bright blue LED isn't included in the measurement, so that would be a candidate for removal...

    On a related note you can control some of those LEDs in software Arduino Yun LEDs

     

    There's also some stuff here about running at a lower voltage and/or frequency.  Gammon Forum : Electronics : Microprocessors : Power saving techniques for microprocessors

    I suspect my biggest power savings are going to be minimising the time that the Linino section is running. I believe the boot time is 60s but I've not actually measured that or worked out what I can do to reduce it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    I saw it now (my movie just finished uploading, so my network is back to the land of the living).

    You are right. When you put the puppy to sleep, the leds switch off.