Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects Design Challenge - Turn on and offable
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
  • Author Author: Workshopshed
  • Date Created: 10 Jun 2015 8:47 AM Date Created
  • Views 3291 views
  • Likes 5 likes
  • Comments 16 comments
  • mosfet
  • enchanted_cottage
  • enchanted_object
  • arduino
Related
Recommended

Enchanted Objects Design Challenge - Turn on and offable

Workshopshed
Workshopshed
10 Jun 2015

Whilst Matilda worked on the LEDs and top panel, Hans finished off the circuits for the MOSFET power switch and connectors.

 

Circuit Explanation

 

A MOSFET is used as a low side switch to turn the power to the servo, RGB LED controller board and humidity sensor. This is connected to the Arduino output with a few extra components from the Arduino Workshop KitArduino Workshop Kit.

 

The gate of the MOSFET effectively acts like a big capacitor and for a short period before the transistor turns on it can draw a sizeable current. So series resistor R1 is used to limit the current drawn from the pin. A second resistor R2 sinks that charge to ground when the switch is turned off and ensures that the MOSFET remains off when the Arduino is asleep. The ratio of these two resistors needs to be high so that there's not a big voltage drop over R1, as the MOSFET will only switch on when the threshold voltage of 4v is reached. The final component is a protection diode, this dissipates the charge from any inductive loads such as the servo's motor when the MOSTFET is turned off.

 

imageimage

Protoshield

 

By this point the protoshield had been through a few revisions. This was clear by the spaghetti layout of the resulting wires. The headers for the cables were also a problem and had to be bent over to allow the connectors to fit. Some of these also had to be repositioned so that they could fit around the support struts. Given that the MOSFET will mostly be off and switching infrequently, it should not be necessary to attach a heatsink.

imageimage

 

The cable for the new knock knock sensor was also created and Hans realised that the strip board had +V, SIGNAL, GND with the protoshield had SIGNAL, +V, GND as intended so that means the cable will need to be carefully fitted in the correct orientation.  Not an ideal situation but also not a complete disaster.

 

Next: Enchanted Objects Design Challenge - Windows 10

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 11 years ago in reply to balearicdynamics +1
    Using a bipolar transistor you'd not need to include R2 as the transistor only turns on when current flows, the mosfet turns on when there is a voltage that charges up the gate so if the Arduino is disconnected…
  • shabaz
    shabaz over 11 years ago +1
    Hi Andy, Like you, I too use non-polarized (i.e. cheap!) connectors for prototypes, one trick (well, an obvious one, I'm sure you know it) to help with connector orientation is to put a blob of marker…
  • mcb1
    mcb1 over 11 years ago +1
    The gate capacitance is pF. It's really only a problem when you're trying to switch it fast. You could easily drop the series resistor to a few ohms and be totally safe. Also the spec says the gate voltage…
Parents
  • mcb1
    mcb1 over 11 years ago

    The gate capacitance is pF.

    It's really only a problem when you're trying to switch it fast.

     

    You could easily drop the series resistor to a few ohms and be totally safe.

    Also the spec says the gate voltage ranges from 2v to 4v, and the load current is quite low.

     

    The IRF540 includes a flyback diode so the extra one is not needed ...however it is good design practice.

     

    I'd be tending to use a spot of hot glue on one end of that crossover type lead ...I can see magic smoke ..

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1

    Thanks Mark, I'm new to power mosfets so the explanation was mostly for my benefit understanding other people's example circuits. The 220R resistor was the lowest I had, it was provided in the workshop kit so saved me buying something else.

     

    I did notice the diode in the schematic symbol but had not appreciated that it would work in that way, cheers.

     

    For other leads I've made them polarised by cutting one of the pins and gluing up the matching hole. I really hope that I don't short out my knock knock sensor or Arduino power supply. There's 5 different connectors on that board and they all really need to be plugged in the right way around. If I was to convert this into a product rather than a prototype I'd put everything on one board and eliminate all of the connectors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1

    Thanks Mark, I'm new to power mosfets so the explanation was mostly for my benefit understanding other people's example circuits. The 220R resistor was the lowest I had, it was provided in the workshop kit so saved me buying something else.

     

    I did notice the diode in the schematic symbol but had not appreciated that it would work in that way, cheers.

     

    For other leads I've made them polarised by cutting one of the pins and gluing up the matching hole. I really hope that I don't short out my knock knock sensor or Arduino power supply. There's 5 different connectors on that board and they all really need to be plugged in the right way around. If I was to convert this into a product rather than a prototype I'd put everything on one board and eliminate all of the connectors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed

    Andy

    We're all learning something with this challenge...

    I really hope that I don't short out my knock knock sensor or Arduino power supply

    Can you change the header on your prototype.?

    Its fairly common to have Ground, Power then signal, as the standard for servos, etc.

    If they get reversed all that swaps is signal and ground, so no magic smoke ...

     

    I did notice the diode in the schematic symbol but had not appreciated that it would work in that way, cheers.

    There is a very guide around saying you should not do it that way for a relay.

    The diode tends to encourge the relay coil to remain on longer, and tends to result in reduced contact life due to increased arcing. (the pull apart forces are delayed, therefore more time to arc)

     

    The diode across the FET is simply to protect it from reverse voltages that exceed the Drain to Source breakdown voltage (100v in this case)

    BUT it will ensure any voltage generated by an inductive load (motor, relay) has a path to the supply ...  where those nice fat 470 -1000uF (or greater) caps are located ......

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1

    Its fairly common to have Ground, Power then signal, as the standard for servos, etc.

    yes, I spotted that the servos were wired like that so I standardised all the connectors the same way. The protoshield is correct it's the strip board circuit that's different , looking at the photo I took there's just enough room to do a crossover so I'll do that and swap the cable back.

    Thanks

     

    For relays would you recommend a capacitor across the contacts?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed

    For relays would you recommend a capacitor across the contacts?

    Not really required.

     

    They are sometimes used to stop spark suppression (and therefore reduce EMI), but they need to be matched to the load.

    You'd really need to dealing with some pretty heavy currents or voltages before you'd be entering into that territory. image

     

    Mark