Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Wardrobe: Progressive Approach
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
  • Author Author: iayanpahwa
  • Date Created: 12 Jun 2015 8:55 PM Date Created
  • Views 2271 views
  • Likes 6 likes
  • Comments 11 comments
  • enchanted_wardrobe
  • enchanted_iot_devices
Related
Recommended

Enchanted Wardrobe: Progressive Approach

iayanpahwa
iayanpahwa
12 Jun 2015

Here's a flowchart explaining the complete working on Enchanted Wardrobe:image

 

I am bit conscious about the suggest clothes feature, Based on temperature and weather conditions outside the wardrobe needed to be suggest clothing for the day to the user and now if user wants to go by the suggestion he can press the button and accordingly the cloth section will come ahead.! say if its a bright sunny day and wardrobe suggests to wear cotton clothes put shades and uv protection cream and if user agrees then the cotton clothes sections should come ahead if user agrees to the suggestion and presses the button, for this the sections should be divided properly in the wardrobe and a motorized mechanism needs to be made. GOOD IDEA to use motor shield but how is the question, SUGGESTIONS ARE WELCOMED image.

For Enchanting the suggestions in sound I'll save pre-made MP3 files in root of OPEN-WRT yun os and can envoke them to play within arduino code. I am gonna buy a usb based sound card tomorrow and i wish ALSA(Advanced Linux Sound Architecture) drivers works for me.

Header 1

opkg update

opkg install kmod-usb-audio

opkg install madplay

Commands to bring USB sound functionality to yun.

 

FINGERS CROSSED image

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed +2
    You're among friends ...you can tell us that you have one at home ...
  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed +1
    How do you know these things ....
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to iayanpahwa +1
    If I don't remember wrong, there is one of these systems to the laundry near home. If it maybe helpful I'll check if they leave me make some details photos. Enrico
Parents
  • iayanpahwa
    iayanpahwa over 11 years ago

    GReat! Bdw have anyone checked my small video demo?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • iayanpahwa
    iayanpahwa over 11 years ago

    GReat! Bdw have anyone checked my small video demo?