Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog [ExM] #3 First attempt on Arduino Yun
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
  • Author Author: nikil511
  • Date Created: 8 Apr 2015 11:53 AM Date Created
  • Views 2053 views
  • Likes 2 likes
  • Comments 2 comments
  • enchanted_objects
  • espresso_ex_machina
  • espresso
  • Coffee
  • coffee_maker
Related
Recommended

[ExM] #3 First attempt on Arduino Yun

nikil511
nikil511
8 Apr 2015

I Just received Arduino Yun.

There was some delay due to Greek customs,  as it was send from the US,  but element14 took care of it, along with the expenses

Thanks! :-)

image

 

So I power up YUN with a micro usb cable, and search for wifi. Found one named "Arduino YUN blahblahxxxxx", connected and tried surfing it on IP 192.168.240.1

And this is the welcome screen. (password is arduino)

imageimage

 

I configured my Wifi SSID and pass, (would be usefull to have a tick-box for displaying pasword)

rebooted and I can see Yun on my accesspoint, getting an IP, great!

 

imageimage

 

Did an ssh connection via putty, using root and arduino as pass, and here is the linino.

Downloaded arduino 1.6.3

Arduino - Software

Specified board as Yun, selected correct port, and uploaded the "blink" example... waiting...it works! :-)

All was straight forward and as expected, nice.

YunResetIllustrations.png

Note, if something goes wrong with your Wifi settings, you can:

  • hold the WiFi button for more than 5 seconds but less than 30, it will reset the WiFi networking settings.
  • or hold down the Arduino’s WiFi reset button for more than 30 seconds, and Yun will reset to factory conditions.

 

 

 

 

 

 

 

 

 

next >> [ExM] #4 First attempt with infineon RGB LED Lighting Shield XMC1202

 

 

  • Sign in to reply
Parents
  • clem57
    clem57 over 11 years ago

    Very easy to setup and program even on wifi. nikil511 what plans do you have for this?

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 11 years ago

    Very easy to setup and program even on wifi. nikil511 what plans do you have for this?

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • nikil511
    nikil511 over 11 years ago in reply to clem57

    well, initial plan is to use SAMA5D4 as the core of the coffee machine, and later Yun might make it in to the grinder. Backup plan is to use Yun in the coffee machine in case I have problems with SAMA5D4.

    We will see :-)

     

    Manolis