Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Generating a Mysterious Signal
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
  • Author Author: crjeder
  • Date Created: 7 Jun 2015 10:23 PM Date Created
  • Views 4869 views
  • Likes 4 likes
  • Comments 46 comments
  • smart_key_hooks
  • enchanted_objects
  • bit_banging
Related
Recommended

Generating a Mysterious Signal

crjeder
crjeder
7 Jun 2015

Let us assume that I want to create a signal like this:

 

image

Where:

 

Signal

Name

Duration in

μs ± 150 ns

T0H0.4
T1H0.8
T0L0.85
T1L0.45
Treset> 50

 

The usual way to generate arbitrary signals is called "Bit banging". It requires software to set the output in the "HIGH" and "LOW" state in the exact timing given by the protocol. The timing requirements for this signal look pretty strict that I do not believe that this would be possible or at least not very reliable. So I am looking for some hardware support.

After a lot of head ache and reading datasheets the idea of using the PWM came into my mind.

Bit Banging with PWM

 

Let's look at the signal again:

  • it starts always with "HIGH" and ends with "LOW" (except for reset which is always "LOW")
  • length of signal is 1.25 μs (reset again an exception)
  • 0.05 μs resolution (0.05 is the greatest common divisor of 1.25, 0.4, 0.85 and 0.45)

 

Exact Solution

The signal can be generated with PWM of 1/0.05 μs = 20 MHz frequency. Therefore the "alphabet" above translates to:

 

SymbolDuty %
"0"32
"1"64

 

The PWM frequency of 20 MHz is quite high, can the signal be done approximated with lower frequency?

 

Reasonable Approximation

The odd thing about the spec for this signal is that it is not symmetric, i. E. the high time for "0" is not equal to the low time for "1" as I had expected. Since the rising edge of the signal is every 1.25 μs this allows the receiver to synchronize. The sampling presumably takes place at exactly the half of the time which explains the asymmetry: It gives a safety margin for the timing or rather does not require steep edges.

The tolerance for the falling edge is quite high. I did not recognize it at first sight, but when I converted the whole timing into nano seconds (ns) It's pretty clear:

 

Signal Name

Time of Falling Edge

Nominal [ns]

Time of Falling Edge

Minimal [ns]

Time of Falling Edge

Maximal [ns]

T0H400350550
T1H800650950

 

This allows a much more reasonable approach:

Divide the 125 ns in three sections ad vary the duty cycle between 1/3 and 2/3 or in decimal:

 

SymbolDuty %
"0"33
"1"66

 

The frequency in this case is only 2.4 MHz. That's much better!

 

Reset

 

The reset symbol is an exception - it does not fit in the above timing. It can be generated by 40 periods with a duty cycle of 0%.

Since we are able to generate the signal there is only one question left: What is this for?

 

Usage of the Signal

 

Did you recognize / guess the signal? What do you think it is for? image

 

(solution in the next blog post)

  • Sign in to reply

Top Comments

  • crjeder
    crjeder over 11 years ago in reply to balearicdynamics +3
    Yes, the quiz with you guys balearicdynamics , mcb1 , clem57 and Workshopshed was a lot of fun! Thank you for participating!
  • Workshopshed
    Workshopshed over 11 years ago +2
    Will there be a small flower dancing along to the music?
  • mcb1
    mcb1 over 11 years ago in reply to crjeder +2
    It's been a very interesting trip back down memory lane... Looking at this sheet for WS2812B it says single NRZ protocol http://www.seeedstudio.com/document/pdf/WS2812B%20Datasheet.pdf There is some interesting…
Parents
  • crjeder
    crjeder over 11 years ago

    And we have a winner to this "Guess the Mysterious Signal" mini-callenge:

     

    Congratulations to clem57!

     

    He mailed me the correct answer 5 hours ago!

    It is a WS2812B RGB LED with integrated controller.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to crjeder

    I had not understood that you was asking for the exact component name ... Then, I am sorry I have delayed (maybe I find a way to kill clem57 with some strange frequency in attach to a mail) but I spent half of the day outside under the sun. Today we decided to posticipate the daily work some hours image So, my compliments to the winner !

     

    Enrico

     

    P.S. By the way crjeder, as mentioned in the datasheet of the WS2812B RGB LED:

    The data transfer protocol use single NZR communication mode. After the pixel power-on reset, the DIN

    port receive data from controller, the first pixel collect initial 24bit data then sent to the internal data latch,

     

    The NZR communication mode (that means Non Zero Return code) is one of the applications of the mentioned Manchester code are you can read on Wikipedia.

     

    Cheers, Enrico.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to crjeder

    Sure, nothing to say about your solution, that I think it is the more elegant and simple. But ... Just to know thanks to your quiz more about this protocol, recovered from the memory lane image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 11 years ago in reply to balearicdynamics

    Yes, the quiz with you guys balearicdynamics, mcb1, clem57 and Workshopshed was a lot of fun! Thank you for participating!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to crjeder

    As far as I'm aware, NRZ is not about the voltage levels, its about data.

     

    I know from playing with these leds that you do require to have the right frequency for data, so here's what I believe is happening.

    Inside is an intelligent chip, that samples incoming data stream.

     

    They could either compare the data level against a counter to see if it is One or Zero, or just check the level at 1/2 way (ie 62.5uS)

     

    After counting 24 bits of data, it shapes any incoming and passes anything on the Data_In to the Data_Out pin.

    I'm presuming it also sends the reset to the next pixel ...

     

    Whatever you set these to will remain when you pull the data line, so you can just run once and then stop the processor if you want.

     

     

    Using PWM and setting the ratio is a very clever way to simulate what you need, so well done.

    You've also exercised many grey matters ....

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 11 years ago in reply to mcb1

    mcb1 wrote:

     

    After counting 24 bits of data, it shapes any incoming and passes anything on the Data_In to the Data_Out pin.

    I'm presuming it also sends the reset to the next pixel ...

    The reset signal is used to set the LED from "pass the data" into "put next 24 bits into latch" mode. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to crjeder

    Not to be picky, but I think your scaling for the mystery signal is incorrect.

    For a 1 on your raw signal the 'mystery signal' does a high and low which together = 125uS (which could be the clock cycle).

     

    If you excuse the poor cut and pasting, it should look more like this.

    image

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago in reply to crjeder

    Not to be picky, but I think your scaling for the mystery signal is incorrect.

    For a 1 on your raw signal the 'mystery signal' does a high and low which together = 125uS (which could be the clock cycle).

     

    If you excuse the poor cut and pasting, it should look more like this.

    image

     

    Mark