Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog MagicHat - 22 - Securing everything up
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
  • Author Author: amgalbu
  • Date Created: 22 Jun 2015 10:00 AM Date Created
  • Views 2439 views
  • Likes 4 likes
  • Comments 12 comments
  • https
  • security
  • enchanted_object
  • magic_doctor_hat
  • enchanted-objects
Related
Recommended

MagicHat - 22 - Securing everything up

amgalbu
amgalbu
22 Jun 2015

Even if the MagicHat is not sending any sensitive data out on the Internet, it's always important to make communication as secure as possible.

For this reason, I will implement HTTPS communication between the web browser and NodeJS running on Arduino Yun. Since the communication is now encrypted, we can use basic authentication (were password is just Base64 coded, but not encrypted)

To add HTTPS support, we need to:

 

Install OpenSSL

OpenSSL setup can be downloaded from here. Installation is plain vanilla

 

Create a self-signed certificate

To create a self-signed certificate, open a command prompt window and type the following commands

set OPENSSL_CONF=C:\Program Files (x86)\GnuWin32\share\openssl.cnf

This commands set the path for the OpenSSL configuration file

 

openssl req -x509 -newkey rsa:2048 -keyout c:\temp\key.pem -out c:\temp\cert.pem -days 365 -nodes



req: PKCS#10 certificate request and certificate generating utility.

-x509: this option outputs a self signed certificate instead of a certificate request. This is typically used to generate a test certificate or a self signed root CA.

-newkey arg this option creates a new certificate request and a new private key. The argument takes one of several forms. rsa:nbits, where nbits is the number of bits, generates an RSA key nbits in size.

-keyout filenamethis gives the filename to write the newly created private key to.

-out filename This specifies the output filename to write to or standard output by default.

-days nwhen the -x509 option is being used this specifies the number of days to certify the certificate for. The default is 30 days.

-nodesif this option is specified then if a private key is created it will not be encrypted. When this option is not added, NodeJS will ask for the private key's passphrase when the private key is used

 

Create a server that support HTTPS

The following code creates a server with HTTPS support

 

var options = {
  key: fs.readFileSync('key.pem'),
  cert: fs.readFileSync('cert.pem')
};

var server = https.createServer(options, app);
server.listen(3000, function(){
  console.log('We have started our server on port 3000');
});

 

Install NodeJS's basic authentication module

Since a  lot of the middleware was pulled out of the Express core in v4 and put into separate modules, the basic auth module needs to be explicitely installed

 

npm install basic-auth-connect

 

Implement basic authentication in node

 

var basicAuth = require('basic-auth-connect');

// NEW CODE BEGINS HERE

// replace 'user' and 'pass' with your username and password

app.use(basicAuth('user', 'pass'));
//NEWCODE ENDS HERE

app.use(express.static(__dirname));
app.use(express.static('.'));



Client side changes

The only change required on the client side Javascript is to changes the websocket URL from ws://<ipaddress> to wss://<ip address> to use Secure web sockets. if standard web sockets are used, web browsers will raise a security error because you are trying to use an unsafe connection

 


With  all these changes in place, we can now connect to the MagicHat web interface using HTTPS. Since the certificate is self-signed and not by a trusted certification authority, web browser will complain about that and will warn you about potential risks


image


By clicking on the"Continue to this website" link, you will be asked for username and password

 

image

  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 11 years ago in reply to Workshopshed +2
    Hi Andy I agree with you, but it's a bit too expensive to request certificate to a certification authority like verisign. The cost of "trusted certificate" is in the order of a couple thousand dollars…
  • crjeder
    crjeder over 11 years ago in reply to crjeder +2
    Yes, self signed certificates are for testing. Full Stop! They should never ever be on public sites!
  • Workshopshed
    Workshopshed over 11 years ago +1
    Self signed certificates are great for prototyping secure systems, the only concern is that people get blind towards accepting the warnings if they are used too much. There's probably a good way to distribute…
  • clem57
    clem57 over 11 years ago in reply to crjeder

    I worked on encryption at a bank and self signed certs were a no no for production. Only testing allowed for internal use.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 11 years ago in reply to crjeder

    Yes, self signed certificates are for testing. Full Stop! They should never ever be on public sites!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 11 years ago in reply to balearicdynamics

    Don't mix up OpenSSL with self signed certificates. Many sites which have trusted certificates use OpenSSL.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 11 years ago in reply to clem57

    Modern Browsers clearly warn you if this site presents self signed certificates.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 11 years ago in reply to Workshopshed

    Andy is right! If you have no trusted 3rd party, a certificate is worthles. You can never know if the site you visit is from the organisation it claims to be. We, for exampe all trust element14. But who knows which public key the web site has? So Mr. Evil can set up a site, call it www.element14-community.com or www.element14.org and sign the certificate and claim that is Premier Farnell's community. If you smell the fishy odor then you can check the certificate and see, that it is self signed. What do you gain form this?

    On the othe hand if by presenting a verified certificate we know that a company called "Premier Farnell plc" owns the site and that Cybertrust has verified this.

    The later is harder to fake, don't you agree?

    Essentially you still have to trust Cybertrust and Premier Farnell but you cant get any better as long as you dont go to the Head Office and ask for the public key in order to manually verify it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>