Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Review 4: Digital Continuous Rotation (360°) Servo Part 2
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
  • Author Author: Jan Cumps
  • Date Created: 4 Apr 2015 1:12 PM Date Created
  • Views 2006 views
  • Likes 3 likes
  • Comments 6 comments
  • enchanted_player
  • enchanted_objects
  • servo
  • continuous_servo
  • servo_motor
  • arduino
  • servo_360
Related
Recommended

Review 4: Digital Continuous Rotation (360°) Servo Part 2

Jan Cumps
Jan Cumps
4 Apr 2015

In Part 1 I reviewed the servo and made a test bed for prototyping. I'll continue with some stats and measurements.


You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


Dead Band

 

The continuous servo has a range of angles, around 90, where it doesn't rotate. Calling Servo.write() with a value in that dead band makes the motor stop.

On mine that band is between 89 and 94. The few values below and above that range cause some noise in the motor, but it doesn't start to spin yet.

It spins under 87 and above 96.


Servo Signal


Servos are controlled with a PWM signal. The duty cycle defines how the motor reacts.

The Arduino Servo library generates the PWM signal that drives the servo. The frequency is 50 Hz.


image


I'm using the test bed from the previous post to check the PWM across the range.


image

I've entered full speed counterclockwise, half speed, stop, half speed clockwise and full speed.

The table below gives a capture of the high part of the PWM.


 

0: full speed counterclockwiseimage
45: half speed counterclockwiseimage
90: stand stillimage
135: half speed clockwiseimage
180: full speed clockwise *image



* the scale of the 180 signal is different because the PWM is too wide to fit on the scope screen in the range used for the other measurements.



  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 11 years ago +1
    One of these days, I will invest in an oscilloscope!
  • clem57
    clem57 over 11 years ago +1
    Thank you for showing what the range is/does!
  • Workshopshed
    Workshopshed over 11 years ago +1
    Because I was not planning to use this servo I thought there was no harm in opening it up. There's a plastic spacer next to the motor which I'm guessing is where the potentiometer goes when it's not a…
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    Because I was not planning to use this servo I thought there was no harm in opening it up. There's a plastic spacer next to the motor which I'm guessing is where the potentiometer goes when it's not a continuous device. A small circuit board connects the inputs to the motor and the other end has a multistage gearbox, a bearing on the last stage to support the loads on the horn. Not a lot on the board, just a big IC, some transistors and a few discrete components.

     

    At the end of the day it was quite straightforward to get it back together.

    image

    image

    image

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago

    Because I was not planning to use this servo I thought there was no harm in opening it up. There's a plastic spacer next to the motor which I'm guessing is where the potentiometer goes when it's not a continuous device. A small circuit board connects the inputs to the motor and the other end has a multistage gearbox, a bearing on the last stage to support the loads on the horn. Not a lot on the board, just a big IC, some transistors and a few discrete components.

     

    At the end of the day it was quite straightforward to get it back together.

    image

    image

    image

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    Cool.

     

    I've made this teaser for my Enchanted Light Organ - also with a smaller 180° servo: