Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Review 7: Atmel SMART SAMA5D4 Xplained Ultra - C++ ADC Example on Linux
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
  • Author Author: Jan Cumps
  • Date Created: 16 May 2015 2:53 PM Date Created
  • Views 2515 views
  • Likes 3 likes
  • Comments 11 comments
  • enchanted_player
  • enchanted_objects
  • c++
  • xplained_ultra
  • atmel
Related
Recommended

Review 7: Atmel SMART SAMA5D4 Xplained Ultra - C++ ADC Example on Linux

Jan Cumps
Jan Cumps
16 May 2015

I'm making steady progress on this drizzly day.

I have my first C++ linux program running that samples the an ADC pin on the SAMA4D4 Xplained Ultra Board.

 

In the mid 90's, I was a C++ software developer. Around that same time, the standard template library (STL) came into fashion.

It's great to use it once again.

 

image

 

Getting the ADC values

 

Once again, this is inspired by Robert Peter Oakes's work on this board, SAMA5D4 Xplained Ultra - Tips and Tricks #2 - Using the built in IO and external devices.

I'm using a very similar setup as Peter, but instead of using the Linux command line to read the sample results, I've written a C++ program.

But we're both triggering a sample and reading results by accessing /sys/bus/iio/devices/iio:device0/in_voltage0_raw.

 

The schematic is very simple: a potentiometer with both ends connected to ground and 3.3V of the Xplained board. The wiper goes to A1.

To make things funny, A1 is analog port 0 in the linux mapping. (I don't know yet what A0 is, but it has a digital signal on it when I sample it with my scope.)

 

The program is cross-compiled using the GNU toolchain on a windows machine, loaded to the linux root user's home folder, and executed.

It shows a sample result in the terminal window every second.

I haven't used any of the Atmel libraries. All is done via standard file access.

 

#include <iostream>
#include <fstream>

using namespace std;

const char fileName[] = "/sys/bus/iio/devices/iio:device0/in_voltage0_raw";

int main() {
  string line;
  while(1) {
    ifstream myfile(fileName, ios::in);

    if (myfile.is_open()) {
      while (getline (myfile,line)) {
        cout << line << '\n';
      }
      myfile.close();
    } else {
      cout << "Unable to open file " << fileName << "\n";
    }
  }

  return 0;
}

 

That's the whole program. After compilation, linking, uploading and setting the executable flag, here's what it looks like in the terminal:

 

image

 

The value changes when moving the potentiometer wiper.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago +1
    ... and with this post I'm claiming dibs on being the first among all roadtest and designchallenge contenders who cross-compiled and ran a c program that accesses I/O on this very board . If we find prior…
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to michaelkellett

    michaelkellett, I don't know. The ADC is configured as a character device. I haven't figured out yet how to reconfigure it to change rates, etc..

    Buffering is documented here: http://www.at91.com/linux4sam/bin/view/Linux4SAM/IioAdcDriver

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago

    How do you actually control the ADC, it isn't actually a file so there must be some kind of driver thing somewhere which is setting sample rates and doing buffering etc (I hope) .

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago

    I've now ported my light organ design from Arduino to SAMA5D4 (including the fft library)

     

    7 second video capture:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Good reuse and demonstration.

     

    It is always good to get back to basics when evaluating new boards.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>