Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog The Genie's Day Brightens
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
  • Author Author: RParkerE
  • Date Created: 22 May 2015 9:12 PM Date Created
  • Views 2736 views
  • Likes 4 likes
  • Comments 14 comments
  • enchanted_objects
  • mini_automator
Related
Recommended

The Genie's Day Brightens

RParkerE
RParkerE
22 May 2015

The week was full of rain and clouds for the poor genie all week. Unable to leave his house and make any progress on the things that needed to get done, due to the unfortunate consequences of doing your electrical work in the rain, but today the sun peeked out from behind the clouds and shone with the brightness of 2000-2500 lumen. It was magnificent! However, shortly after its arrival, the clouds took over again . But while the sun was out the genie made headway on his electrical wiring of his sweet new crib. He set the power supply to roughly thirty volts and tested out his lights to see if they worked.

                                                                       imageimage

And it worked! How excited the genie was! This was a huge step in the right direction with the build of his new pad. Now all that was needed to be done was wire it all up to his sweet new dimmer and you could call him Xzibit Jr.

                                                                                                      image

WAIT! There is no light!!!! What in the world is going on? No explosions, check. No fire or smoke, check. Then what? The genie checked the voltage coming out and the light intensity and found:

                                                                  imageimage

But that doesn’t make sense! 30 Volts in and only a 100th of that out? How could this be? The genie has yet to figure this out, but he will be working diligently over the weekend to figure out a solution!

                                                                                   

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to Jan Cumps +3
    Jan Cumps You wouldn't be the first or last to miss something in a post ... You raised a very good pint about the meter though. I wonder if someone who has a working LED can do some checking using a simple…
  • RParkerE
    RParkerE over 11 years ago in reply to mcb1 +3
    I found the culprit and it was much simpler than assumed. I had a poor connection, after I soldered the pins it worked perfectly fine. I am working on my next update now
  • Jan Cumps
    Jan Cumps over 11 years ago +2
    The week was full of rain and clouds for the poor genie all week. Unable to leave his house and make any progress on the things that needed to get done, We seem to have the opposite way of working . I…
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to mcb1

    mcb1 wrote:

     

    ...

    Yes but no light as well ...

    ...

     

     

    You are right. I had missed that the Infineon board isn't connected in the bright light photo. [/must check if eyes are fully open before posting]

     

    The pointer you give to the Internet of Holiday Lights work will be a good one. There are a number of good working sketches uploaded in that design contest.

    I started with (read: blatantly stole) the one from peteroakes BYOB Party #3, Infineon Library Available.

    But any of the contenders sketches and libraries would work to get you going.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago

    Don't forget the heatsink ....

    The frequency and shape of the output signal of the Infineon board may be too hectic for your meter.

    Yes but no light as well ...

     

    You may wish to try experimenting with a few standard leds and 10v ...rather than destroy your high power one.

     

     

    This looks like similar to my 30W RGB version, which even with a single led string at 1/3 power was enough to make you see spots for a while afterward.

    Internet of Holiday Lights RoadTest Plus (suppliment) Part 2

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    That's one bright LED

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago
    The week was full of rain and clouds for the poor genie all week. Unable to leave his house and make any progress on the things that needed to get done,

     

    We seem to have the opposite way of working image.

    I only work on the project when the weather is bad or when it's dark.

     

    On the measurement: The frequency and shape of the output signal of the Infineon board may be too hectic for your meter.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<