Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog The kits are here, Its Time to start
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
  • Author Author: iayanpahwa
  • Date Created: 3 Apr 2015 6:28 AM Date Created
  • Views 1213 views
  • Likes 5 likes
  • Comments 10 comments
  • enchanted_objects
  • enchanted_iot_devices
Related
Recommended

The kits are here, Its Time to start

iayanpahwa
iayanpahwa
3 Apr 2015

I received my kits today, Finally I can start with my first module of Enchanted Wardrobe. It would be around the Yun.

P.S the servo is quiet big, I got an idea to use it wisely image ,@STAY TUNED! for more.image

Thanks Element14 once again...

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed +1
    Here's the review and a test bed: Review 3: Digital Continuous Rotation (360°) Servo . My next challenge is to find a nifty way to use this type of motor. I wasn't expecting a continuous servo. It's surprises…
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    The servo has got a bit of power to it, in my test yesterday it seemed to rotate about 380° when I ran the 0 to 180° sweep code into it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    It's indeed a 360° motor. I've tested it, and it's capable of doing a little more than full circle, just like you experienced.

    The motor has a model number SM-S4303R on it. Datasheets tell that this is a  'Continuous Rotation Servo'.

    These continuous motors are a bit tricky to program and calibrate.

    Here's a slow runner I just bodged together:

     

    #include <Servo.h> 
    
    Servo myservo;  // create servo object to control a servo 
                    // twelve servo objects can be created on most boards
    
    int pos = 90;    // variable to store the servo position 
    
    void setup() 
    { 
      myservo.attach(9);  // attaches the servo on pin 9 to the servo object 
      myservo.write(90);
    } 
    
    void loop() 
    { 
      myservo.write(100);
      delay(15);
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    It's indeed a 360° motor. I've tested it, and it's capable of doing a little more than full circle, just like you experienced.

    The motor has a model number SM-S4303R on it. Datasheets tell that this is a  'Continuous Rotation Servo'.

    These continuous motors are a bit tricky to program and calibrate.

    Here's a slow runner I just bodged together:

     

    #include <Servo.h> 
    
    Servo myservo;  // create servo object to control a servo 
                    // twelve servo objects can be created on most boards
    
    int pos = 90;    // variable to store the servo position 
    
    void setup() 
    { 
      myservo.attach(9);  // attaches the servo on pin 9 to the servo object 
      myservo.write(90);
    } 
    
    void loop() 
    { 
      myservo.write(100);
      delay(15);
    }