Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog The kits are here, Its Time to start
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
  • Author Author: iayanpahwa
  • Date Created: 3 Apr 2015 6:28 AM Date Created
  • Views 1203 views
  • Likes 5 likes
  • Comments 10 comments
  • enchanted_objects
  • enchanted_iot_devices
Related
Recommended

The kits are here, Its Time to start

iayanpahwa
iayanpahwa
3 Apr 2015

I received my kits today, Finally I can start with my first module of Enchanted Wardrobe. It would be around the Yun.

P.S the servo is quiet big, I got an idea to use it wisely image ,@STAY TUNED! for more.image

Thanks Element14 once again...

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed +1
    Here's the review and a test bed: Review 3: Digital Continuous Rotation (360°) Servo . My next challenge is to find a nifty way to use this type of motor. I wasn't expecting a continuous servo. It's surprises…
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    Here's the review and a test bed: Review 3: Digital Continuous Rotation (360°) Servo.

    My next challenge is to find a nifty way to use this type of motor. I wasn't expecting a continuous servo.

    It's surprises like this that may steer us into unknown directions image.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps

    Sounds good, I've tried your code and can confirm that it's a continuous rotation servo. That's no good for what I need but I'd already bought myself a smaller servo that is a standard positional model.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago

    I'm going to write a review here on element14 today.

    It's going to include a test bed where you can enter the speed in the Serial Monitor of Arduino IDE,  between 0 (fast counter clock) and 180 (fast clowkwise). It will run at that speed for 5 seconds then stop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago

    I've been digging a bit further in the howabouts of this type of servo,

    and my code above is more complex than it should be.

    There's no need to keep telling it the speed in the loop.

     

    #include <Servo.h> 
    
    Servo myservo;  // create servo object to control a servo 
    
    void setup() 
    { 
      myservo.attach(9);  // attaches the servo on pin 9 to the servo object 
      myservo.write(100);
    } 
    
    void loop() 
    { 
      // this space intentionally left blank
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    I'm still learning about this, but these servos work differently.

     

    If you write 90 to them, they stop, in the current position, not in a fixed 0 point.

    A value lower than 90: turn left. The lower the value, the faster the speed.

    A value higher than 90: turn right The higer the value, the faster the speed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>