Energy Harvesting Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Energy Harvesting Design Challenge
  • More
  • Cancel
Energy Harvesting Design Challenge
Blog A Very Compact Guide to Energy Harvesting - Part 001
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 7 Apr 2013 9:06 PM Date Created
  • Views 714 views
  • Likes 2 likes
  • Comments 5 comments
  • energy_harvesting_challenge
Related
Recommended

A Very Compact Guide to Energy Harvesting - Part 001

COMPACT
COMPACT
7 Apr 2013

Preface

My thanks to Element14 and Würth Electronik for inviting me to participate in this Energy Harvesting  RoadTest Challenge.

I've already completed a large battery of tests and experiments and over the coming weeks publish my findings and progress.

image

Introduction

Energy Harvesting is best defined as the recovery and application of otherwise spent or wasted energy.

This energy is usually found in varying quantities in some obvious and not so obvious places.

 

An obvious example is Solar Energy - It's found virtually everywhere on planet Earth on bright sunny days.

A less obvious example is Thermal Energy from the difference between the ambient temperature and ground temperature.

Both are valid sources of energy that can be transformed into Electrical Energy by appropriate conversion techniques.

In my articles I will include details of odd locations and devices where I have harvested energy.

 

Where possible I will be using existing items and technologies in the quest for environmental sustainability and minimal impact.

And like usual I will retain the original functionality of the items.

 

imageimage

imageimage

 

Can anyone pick the odd picture out?

 

My first goal is to create a TV remote control that requires no disposable batteries. Its power will be derived from a choice harvested energies.

A TV remote control is a fairly basic device. All that happens is when you press a button a set of Infrared LEDs commence blinking in a sequence that is recognized to a TV set as a command.

It spends the remainder of its time sleeping and turns on only when a button is pressed.

A low energy microcontroller is perfect for this task.

 

If time permits, I will create other more capable items that operate from harvested energy and effort.

 

No Batteries Required.

As per usual I followed my standard strategy of Crawl, Walk then Run by familiarising myself with the Energy Harvesting Kit and conducting a large range of experiments and tests.

 

This kit is an absolute beauty!

It is specifically designed to expedite the development of Energy Harvesting Solutions. All of the fiddly preparation such as minute surface mount soldering has been completed allowing immediate commence Energy Harvesting research.

It comes very neatly packaged in a translucent plastic parts case that contains;

     An Energy Harvesting board

     And Target Load board

 

The boards showcase many Würth Electronik Components that are perfectly suited their intended tasks.

The components used include Inductors, Connectors, Switches, Ferrite Beads, LED and Battery Holder.

The boards also showcase Energy harvesting semiconductors from Linear Technology and EFM32 microcontroller from EnergyMicro.

 

The main idea is that the Target Load board can be operated from energies harvested by the Energy Harvesting board.

The boards are neatly connected together adjacent to each other making components easily accessible from the top.

 

The lid of the case has two apertures;

     One to show the LCD display on the Target Load board

     And one for the Solar Cell on the Harvesting Board.

 

It enables operation with the lid closed. To get it working all you have to do is take the kit into the sunlight and Hey presto - Instant Temperature Sensor Readings on the LCD Display.

(Just as you would with a Solar powered Calculator.)

 

The Energy Harvesting board contains four different Energy Harvesting Power supplies, a Solar Cell and Peltier Device mounted on a Heatsink.

Other energy sources can be connected via its test pins or its PiezoElectric source connector.

 

Unlike traditional power supplies the Energy Harvesting Power Supplies;

     a. are designed to accumulate small amounts of power and then use them when enough is available.

     b. be very efficient as not to waste the precious energy they have captured.

     c. generate a power good signal to indicate that power is at acceptable and available.

 

Here is a picture of the energy storage bank.

image

 

The Target Load Board is an EnergyMicro Giant Gecko STK3700.

It an evaluation board for the highly efficient EFM32 32 bit ARM microcontroller - a microcontroller designed to operate from miniscule amounts of power.

It is perfectly suited to operate from accumulated harvested energies and periodic operation.

 

.... To be continued...

 

Please feel free to leave comments. It'll help me know what to do improve my articles.

  • Sign in to reply
Parents
  • vsluiter
    vsluiter over 13 years ago

    Hi COMPACT,

    Nice to see you back again. I guess crawl, walk run is a very good strategy... I always start with running, but that gets very tiring in the end image

    To pick the odd one out: I guess it's the drum pad because it doesn't have a red and black lead

     

    I like your idea for the remote. It's low power, and a lot of batteries are wasted in these things. Good candidate for energy harvesting!

    Looking at the pictures you made, I realized that energy harvesting is also something based on local conditions; your toys-with-energy-kit picture is sunny (and it's 23.7 degrees outside! whoaa....), so sun is apparently an abundant energy source at your place. When you'd be designing something to use above the polar circle, solar power would not be the source of choice. Local solutions for global impact.... I'm getting carried away image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vsluiter
    vsluiter over 13 years ago

    Hi COMPACT,

    Nice to see you back again. I guess crawl, walk run is a very good strategy... I always start with running, but that gets very tiring in the end image

    To pick the odd one out: I guess it's the drum pad because it doesn't have a red and black lead

     

    I like your idea for the remote. It's low power, and a lot of batteries are wasted in these things. Good candidate for energy harvesting!

    Looking at the pictures you made, I realized that energy harvesting is also something based on local conditions; your toys-with-energy-kit picture is sunny (and it's 23.7 degrees outside! whoaa....), so sun is apparently an abundant energy source at your place. When you'd be designing something to use above the polar circle, solar power would not be the source of choice. Local solutions for global impact.... I'm getting carried away image