Experimenting with Current Sense Amplifiers
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Current Sense Amplifiers
  • More
  • Cancel
Experimenting with Current Sense Amplifiers
Challenge Blog Blog #3: Converting measured value to Amperes
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: misaz
  • Date Created: 19 Apr 2022 1:43 PM Date Created
  • Views 4425 views
  • Likes 7 likes
  • Comments 11 comments
  • MikroE Click Board
  • raspberry pi
  • csa
  • current sense amplifier
  • MAX40080
  • Experimenting with Current Sense Amplifiers
Related
Recommended

Blog #3: Converting measured value to Amperes

misaz
misaz
19 Apr 2022
Blog #3: Converting measured value to Amperes

I welcome you to my next blog post as part of Experimenting with Current Sense Amplifiers Design Challenge. In my first blog I described my experiments plan and in my second blog post I shown basics of using MAX40080 sensor as part of MikroE Current 6 Click Board. In this third blog I will continue with fundamentals of MAX40080 sensor. In this blog post I will describe approaches how to find formula for converting measured digital value in range between -4095 and 4095 to real value in Ampere unit. I will show two approaches how to do this. The first I will show experimental approach of determining formula from measured values at known currents and then I will show accurate approach providing exact formula for converting value.

Experimental approach

The first approach which I will describe is experimental. If we do not know how to convert measured value exactly, we can suppose some things and then estimate function (for example linear function) that we can use for converting value. In case of current sensing, we luckily can suppose linearity of value because we measure voltage drop on shunt resistor which is linear with current according to ohm law and ADC inside MAX40080 is also almost linear. Se we can set up two experiments with two different static known currents flowing through circuit, read values measured by sensor and compute coefficients of linear function using linear interpolation. So, lets experiment.

For the first measurement we can reuse values measured from previous blog. In this blog I used 100ohm resistor powered by 3.3V rail of Raspberry Pi and sensor returned values between around 20 to 30 and we computed average of 100 samples as a 24.1. So, for first measurement of theoretical current 0.033 A (value 0.0333 is computed using ohm law as a U / R where U is voltage on resistor 3.3V and R is value of the resistor) we know that sensor returns 24.1.

For second measurement I upgraded my setup. Because I have no regulable high power bench power supply, I was limited to standard power adapters. Instead of 3.3V from Raspberry Pi which is limited to source 50mA I decided to use 12V from barrel jack. I bought barrel jack connector and solder wires to it:

image

For powering I used old router power supply which can source 5A/12V. The next material issue which I faced was resistor. At this point I realised that is easy to make some high current flow like 1A, but do I have resistor which can handle this current without overheating? I don’t. All my resistors which I have can handle 0.25 or 0.6W, but for handling so “high” current (about 1 Amp) on “high” voltage (about 12 V) requires 12 Wats (P = U * I = 12 * 1 = 12). After some calculations and estimation, I decided to make setup of 16 × 100-ohm resistors connected using 8 paralell branches and each branch having 2 resistors connected in series. This result to final resistance of 25 ohms (100 * 2 / 8), allowing to flow 0.48 A at 12 V and reducing load on each resistor to 0.36 W (limit is 0.25 but this I did not considered as significant violation at room temperature). Final connection looks schematically as follows:

image

And in reality:

image

After connecting I run the same program as in previous blog post with following output:

image

Now we get higher numbers than in previous case and it is expected behaviour because we measure higher current. So, we have two measurements of two different currents 0.033A and 0.48A and two different values 24.1 and 355.42 calculated based on data from sensor.

Experimentally determining conversion formula using linear interpolation

Now we know two inputs and corresponding outputs of some linear function. I will refer value returned by sensor as VAL and real current as I. Linear function and our known points looks on the plot as follows:

image

Generic formula of linear function looks as follows:

image

And if we replace X and Y by our variables:

image

So, it is function which expects VAL as parameter and outputs real current as a value. Our task is to find parameters A and B which are used within formula. The purpose of linear interpolation is to build two equations (with two unknown variables A and B) and solve it. We replace VAL by known values returned by sensor and I by theoretically known corresponding currents. The equations look as follows:

image

And now we can solve them. You can use online solver like WolframAlpha, but I did it manually using multiplication of first equation by constant and then summing with second equation. After it one unknown variable disappear (it is multiplicated by zero) and after that we can get value of one coefficient by solving simple single equation containing single unknown variable:

image

And now we can place newly discovered value of B param to one of original equation and simply solve it:

image

Now we know A and B params. I used WolframAlpha for checking my results. Computed parameters look correct and rounding errors which I did does not look significant:

image

So, now we can place parameters A and B to original formula and get resulting linear function for converting measured value to real current in Amperes:

image

Testing Formula

For testing formula, I used another third configuration with resistor. I used 12V as in previous case and 220ohm resistor (in fact it was 2 × 2 series-parallel configuration). Expected current from ohm law is 12 / 220 which is approximately 55mA. So, lets check. I used the same program with following output:

image

So now we can “call” our function F with value 42.38 and see what we get:

image

We got 0.0577 A which is after converting from A to mA 57.7mA and this is very near our known theoretical result 55mA. It looks that our experimentally determined formula is correct. Minor error is caused by noise, accuracy of voltage and resistor values used and so on. Our formula is not totally correct because we computed it from similarly inaccurate values.

Only single sample suffice

One possible upgrade of our formula reduces need of parameter B with another small assumption. We can assume that sensor returns 0 when measuring 0A current and then we need only one point. This assumption is quite trivial. Efficiently we reduce equations by B parameter which would be zero. Note that we calculated B parameter near zero. The non-zero B parameter introduce some offset to our calculations, and it is problematic especially when measuring negative values.

Accurate Approach

In previous section you have seen experimental approach of estimating coefficients for converting measured value to current. But MAX40080 is not a black magic, and all its structures are documented. We can make exact formula using parameters from datasheet. I will describe process in a reverse way: from 12-bit digital value to real current. The important image for this section is block diagram of MAX40080 sensor from datasheet:

image

The first step of making formula is realize what does the senser measure. The digital value which we receive comes from ADC. ADC in MAX40080 is 12-bit, so it converts voltage in range 0V to reference voltage and convers it to value between 0 to 4095 (2^12 – 1). MAX40080 is bidirectional so it adds 13th bit and returns value in range -4095 to 4095. The first question is what the reference voltage is? The answer is in datasheet: It is 1.25V:

image

So MAX40080’s ADC converts value in range -1.25V to 1.25V (I personally thing that it internally measures voltage in range 0 to 1.25V and sign bit is provided by some comparator externally. It is internal detail, and I did not find accurate answer to this question in datasheet but it is not important for us).

From this knowledge we can convert digital value to voltage (still not a current) by simple cross multiplication (or linear interpolation with single point as used in previous sections):

image

Now we received voltage on input of ADC. Input of ADC is connected across some multiplexer and filtering circuit from amplifier. This amplifier has fixed gain 25 or 125 depending on configuration. Note that datasheet has wrong label which I crossed out for making it less confusing.

image

So, if we want to get voltage on input rather the amplified one, we just need to do reverse operation of amplification which is division. Formula will look as follows:

image

So now we have computed real voltage on the input of MAX40080 chip but we do not need a voltage. We rather need the current. So now we must understand what we are really measuring. The answer is also visualized on block diagram from MAX40080 datasheet:

image

So, we are measuring voltage drop on resistor which is outside the MAX40080. In our case it is resistor on MikroE Click Board. It is this resistor:

image

It is large because it can handle large current. In opposition its value is very small because it should be transparent for measured circuit. Its value is only 10mOhms (mili-ohms) according to datasheet:

image

So now we know formula for getting measured voltage, we know value of resistor having measured voltage drop so now we can use simple ohm law to get final formula for getting value of current from measured value:

image

We can simplify nested fractions:

image

And this is final formula which we can use for converting measured value (VAL) to current I in Amperes.

Testing Formula

Our script used standard 50mV range, so G value is 25. We can try evaluating our formula for measured values from my previous experiments. We know that sensor returned values around 355.42 (which was average for 100 samples) for theoretically computed current of 0.48A. So, let’s check formula:

image

We are near expected result. In this case error is not caused by an experimentally determined coefficients, but rather by noise, and also improper calculation of theoretical currents resulting from assumed voltage exactly 12V and resistor value exactly 25ohm which both was inaccurate with some tolerance in real world.

Comparing Experimental and Theoretical Results

Finally, we can compare our theoretical formula with experimentally deduced one. Theoretical formula matches our assumption that B param should be zero. When you measure value of 0, you get 0A of current. Now think about A param. A param is coefficient which corresponds to value in Amperes for one measured unit. So, if we evaluate our exact formula with VAL=1, then we should get A param of our experimentally deduced formula. Let’s do this:

image

Our experimentally estimated coefficient was 0.00135. 0.00122 and 0.00135 are very similar numbers which confirms that both methods resulted into very similar formula. Lastly, we can compare with results coming from somebody else. If you download official library from MikroE and opens current6.h file, you can see that this library use coefficient of value 0.00125 which is also very similar to coefficients computed by me:

image

Summary

In this blog post you have seen two ways how to get or compute formula for converting measured value from MAX40080 CSA sensor to value in real Ampere unit. I shown experimental way gathering formula from measurements using linear interpolation and also you have seen accurate method providing formula from datasheet parameters. From practical point of view, these information are useless because we can just use formula and coefficients computed by someone else. But I still like it. I learn a lot. This process allowed me to deeply understand operation of MAX40080 CSA and CSAs in general. In fact, this process is very similar for other CSA no matter of vendor. Only parameters like G, and Vref differs. Sometimes internal structure differs slightly.

Experiments Status and Future Plans

At the time of writing this blog post I started experimenting with using MAX40080 from MAX32625 microcontroller. After first MCU experiments I faced some issues that cost me a lot of time and I also found some mistakes in datasheet which I will report to Maxim. I am currently testing my own library and I plan to post some first thoughts soon. I also plan to prepare some simple Python library because I feel some interest from other challengers due to lack of any official library for Raspberry Pi. I also have some idea how to utilize my library for MCUs on Raspberry Pi and I am considering creating CLI utility for interacting MAX40080 without any programming needed. I am still waiting for PCBs for my more advanced experiments. OSHPark panelised them and send them to fab but still did not ship them to me. In the meantime, I ordered and received required components.

Last Words

For this blog it is totally all. Thank you for reading it and stay tuned. If you find any inconvenience or other issue in my formulas, computation or somewhere else, feel free to write a comment. I also like to hear any feedback in comments.

Next blog: Blog #4: Using MAX40080 CSA with MAX32625 MCU – First thoughts

  • Sign in to reply
Parents
  • guillengap
    guillengap over 4 years ago

    I have not analyzed this tutorial in detail but I have the knowledge to do it and I promise to do it. And to be honest, in this contest I didn't expect to find someone who likes to make sensor libraries. In fact I have no interest in winning this contest, I want to develop an idea that I have in mind and its very different from the one I am competing here, but I need a library.
    My explanation is that hardware developers need library creators. If I start to make a library, maybe I'll invest two or three months to make it work well, but as soon as I have the library, I'll do my project in two or four weeks. I think I lose my goal if I start from the beginning, that is to say making a library, in fact the manufacturers continually change them due to hardware or programming errors (bug logs).

    Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 4 years ago in reply to guillengap

    Thank you for replay and feedback. Due to multiple requests I decided to do 3 projects/libraries which may help you (and other members):

    1. My own Library for MCUs which I already created, and I am testing it in these days. It will be available within about 6 days.
    2. Simple python library allowing to use basic features of sensor. Other features will be included upon requests. It will be available within about 10 days.
    3. Command Line utility based on my first library allowing to use sensor without any programming needed. At starting it will allow you to use basic features of sensor. Other features will be included upon requests. It will be available in about 6 to 15 days.

    So most probably in about 10 days you get library which will allow you to do your experiments.

    You are correct about HW, SW and documentation bugs. MAX40080 is new chip so at least documentation is not fully polished yet. In opposition analog perofmrance, accurancy and noise are very good. I found at least 6 minor mistakes in MAX40080 datasheet and some descriptions which are not clear. I will post description about first two regarding FIFO soon (in about 4 days). Today I created 4 tickets at Maxim support, and I plan to create other tickets after some further experiments and investigations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • guillengap
    guillengap over 4 years ago in reply to misaz

    I have a doubt, in a rechargeable battery there is a current that goes in one direction when it is discharged, and the current flows in the opposite direction when it is charged.
    Question: Is it possible to measure both currents simultaneously with this sensor? If this is true, how would be the electrical connection of this sensor with this battery?

    Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 4 years ago in reply to guillengap

    I have very few experiences with battery charging circuits but I think it should work. MAX40080 can sense currents in both direction without any issue. Direction of currents can freely change at runtime. Both sensing RS+ and RS- voltages have to be higher than GND but in this is ok in this case. I think you just need to discconnect circuit at some point and connect RS+ to one end of disconnected wire and RS- to the second end of diconnected wire like connecting standard ampermeter. I recommend to measure voltages before connecting and if all conditions from Absolute Maximum Ratings from Dataheet are met (and preferably also coresponding recommended parameters from Electrical Characteristic), it should work well. Note that Maxim/ADI mention battery operation devices as a candidates for using MAX40080 at main page of Datasheet:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to misaz

    Excellent work misaz.

    The E14 community is very fortunate in your offer to share the intellectual property. I have neither the skill nor knowledge to develop the library needed to continue this challenge. I have followed your blog posts in anticipation of your success.

    I have been using the crumbs of knowledge that have fallen from your table to further my challenge project along. My hope was I might come up garner a method to get a measurement. Your offer to share a library is what I look forward to.

    My challenge is to measure motor current in a 12VDC system. I look forward to using your code. If it can help your efforts, I would welcome the opportunity to be a beta tester.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • colporteur
    colporteur over 4 years ago in reply to misaz

    Excellent work misaz.

    The E14 community is very fortunate in your offer to share the intellectual property. I have neither the skill nor knowledge to develop the library needed to continue this challenge. I have followed your blog posts in anticipation of your success.

    I have been using the crumbs of knowledge that have fallen from your table to further my challenge project along. My hope was I might come up garner a method to get a measurement. Your offer to share a library is what I look forward to.

    My challenge is to measure motor current in a 12VDC system. I look forward to using your code. If it can help your efforts, I would welcome the opportunity to be a beta tester.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • misaz
    misaz over 4 years ago in reply to colporteur

    Thank you for feedback. I do not plan any private alfa testing because time is going and this only postpones release date. I will rather publish library and then fix possible bugs after reportings.