Experimenting with Current Sense Amplifiers
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Current Sense Amplifiers
  • More
  • Cancel
Experimenting with Current Sense Amplifiers
Challenge Blog Blog 6: Now for some initial data
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: colporteur
  • Date Created: 26 Apr 2022 9:42 PM Date Created
  • Views 2932 views
  • Likes 8 likes
  • Comments 13 comments
  • Current 6 Click
  • raspberry pi
  • MAX40080
Related
Recommended

Blog 6: Now for some initial data

colporteur
colporteur
26 Apr 2022

With the python library, misaz shared in his blog post, I can continue with my challenge testing.  My initial tests of the sensor are using the locomotive on the bench. I have been using 3VDC, 5VDC and 12VDC to set some expectations before moving to the rail tests.

I still try and follow the process my electronics lab college instructor tried to instill in us 40 years ago. Have some idea of what the measurement should be, before you go poking around with testing equipment making measurements. I had no success getting current measurements using my Fluke VOM so I only have what the sensor is providing.

The python script generates a current & voltage reading every five seconds. The initial voltage applied to the locomotive motor is 5VDC, then changes (highlite) to 3VDC and then to 12VDC.

image

My question to the sharper electronic knives in the drawer than me is, do the current values look reasonable?

The current reading moves between.05 to .09, the average, throwing out the negative values in the calculation, is .06. I was expecting higher current values at the higher voltages. What I interpret from the current reading is a motor that is an active load where the resistance changes to ensure a steady current. That doesn't seem correct?

The motor speed does change with a change in the voltage.

I confess there is a lot of rust and dust accumulated on my electronic theory. Part of my motivation for doing these challenges is to refresh my knowledge. I would appreciate any feedback members have to offer before proceeding with further testing. What do you see in the values so far?

  • Sign in to reply

Top Comments

  • misaz
    misaz over 4 years ago in reply to michaelkellett +1
    Both Python anb C Library suppoort configuring digital filter. Maximum value of digital filter (128) eliminated almost whole noise in my case of sensing current flowing simple resistor on breadboard. …
  • dang74
    dang74 over 4 years ago in reply to colporteur

    LOL.  So in my case I guess I have another 18 of experiencing similar feelings.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to dang74

    Thanks for the kind words D74. My 40 years employed struggled under the same doubting perspective.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dang74
    dang74 over 4 years ago

    Earlier today I was reading blog#2.  Back then you were concerned that you were in over your head.  I am so glad pushed ahead.  I had some frustration and self doubt during my road tests so I can totally relate.  Things seem to be progressing now, and hey, you have the ability to read data, but best of all, you are learning new things and solving problems as they emerge, and there in lies the real reward.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 4 years ago in reply to colporteur

    Just a quicky today, the sun is shining and it won't tomorrow so I'm going out on the bike !

    Easy bit first, I suspect the current drawn is really spikey so that the meters are choking on the spikes and only on the 10A range are they happy.

    Next a quick thought about DC motors, I'm assuming your loco has a traditional permanent magnet DC motor with brushes.

    The armature DC resistance will be very low.

    When the motor spins in a magnetic field a voltage is generated in the windings. It doesn't matter why it spins, it still makes that voltage.

    If you apply volts to the motor it will start to spin due to the current in the armature interacting with the mag netic filed from the magnets. As it spins it will make that voltage which tries to stop the current flowing, thats why it's called a "back emf".

    The voltage increases the faster the motor turns.

    The mechnical power in the motor = back emf x current

    The heat going into the motor = current squared x armature resistance

    The force exerted by the armature is proportional to the current.

    The motor will spin faster and faster and the back emf will increase, reducing the force the armature can exert. When this force is equal to the force of friction and load slowing it down the armature spin speed will stabilise.

    If you increase the voltage the motor will spin faster so the current will increase less than you expect.

    With your motor at 5V the input power was about 0.225W and at 12V it's 0.72W.

    With a pure resistive load the increase would have been to  1.296W and the current would have gone up to 0.108A.

    Your measurements are showing just what we should expect for a motor.

    Hope that helps.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to dougw

    I would like to better understand your explanation.

    With much help from the sharper knives, I have scripts that contain reading that are more stable.

    image

    I pulled the following readings and did some ohms law calculations. Well, truth be known I let some website do it for me so that it was presentable.

    There is a power difference between each load voltage as you suggested. What confuses me is the change in resistance. In my mind, the copper wire windings should have a constant resistance. Varying the voltage across that resistance would produce different currents. I'm wondering if I am mixing impedance and resistance. Yes, there is a constant resistance but that is not the only variable in play. There is inductance and capacitance along with the resistance.

    I have tried measuring the resistance of the motor with little success. The value reads 1 ohm and I know I'm not putting 12amps through this little motor.

    I have a disconnect in my theory at some point. I went digital in my career and motor theory took a back stage. The only time I got involved with them was by replacing them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>