Products
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
Experimenting with Flyback Transformers
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Flyback Transformers
  • More
  • Cancel
Experimenting with Flyback Transformers
Blog DC to DC Demystified - Blog 1 - Does it fly back?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Flyback Transformers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Anthocyanina
  • Date Created: 10 Jan 2024 11:02 PM Date Created
  • Views 3865 views
  • Likes 11 likes
  • Comments 21 comments
  • flyback converter
  • smps
  • EXPERIMENTING WITH FLYBACK TRANSFORMERS
  • SMPS Flyback Transformers
  • bourns
  • dc to dc
Related
Recommended

DC to DC Demystified - Blog 1 - Does it fly back?

Anthocyanina
Anthocyanina
10 Jan 2024
Group photo!

This being my first blog, i'll begin with a short introduction:

My name is Sara, I'm an electronics engineering student and electronics is also my hobby, I came across the element14 community when looking for help with a function generator, and have continued to visit it occasionally as it has proved to be a valuable source of knowledge and fun content.

When I started in electronics, adventuring into power electronics felt a bit scary, and when it came to switched-mode power supplies, I just wanted to avoid them, even at the cost of efficiency and space.

It seems many newcomers to the world of electronics also find them at least a bit confusing, so I'll try my best to remove the mystery around designing your own switched-mode supply, in this case, around the flyback topology.

This series of blogs will assume you have some basic understanding of how inductors work, and what a transformer is.

With that out of the way, let's get to it, first,

Meet the family!

Thanks to element14 and Bourns for providing a fairly comprehensive transformer kit. This kit contains all the magnetic components you'll need to build a proper power supply: Gate driver transformers(in green), Flyback transformers, and common mode chokes(in red).

Bourns's design challenge kit

And that's it? Won't you tell us more about them? Well, rather than going into detail about each transformer in this blog, I'm just going to jump right into building a circuit and see what happens!

I thought it would be easiest to start with the lowest input voltage transformer:

The BA60951CS

today's subject of focus

This is a really tiny transformer

 they really are tiny!

Bourns has made this really compact transformer to work with an input voltage between 7 and 24V and rated the secondary to 15V. Perfect to work with at the bench. They specified the working frequency of this transformer to be 120KHz, but the electrical specifications were, well, specified at 250KHz. Because of this, I'll be using a switching frequency of 250KHz, especially since it's also here that its Q factor approaches its maximum of around 70 when measuring it with an impedance analyzer. This tells me that the 120KHz working frequency is likely a mistake in the datasheet.

 primary inductances and Q factor measurements

With the impedance analyzer we can of course also measure the leakage inductance, which is the inductance that isn't magnetically coupled to the other windings of the transformer, but instead acts as if we added an inductor in series to an ideal transformer.

To measure the leakage inductance, we short all the windings, except the one we want to measure:

This is only correct if we're using all the windings. To properly measure the leakage inductance, connect the winding to measure, and short the other windings you will use. If you are only going to use two windings from a transformer with 3 or more, leave the rest unshorted. At the end of the post, there will be a link to a video by Biricha showing how to properly measure a transformer. Thanks to javagoza for pointing this error out.

 test setup for measuring leakage inductance

Knowing what this leakage inductance is will be useful later when it's time to design the snubber circuit, because this inductance, together with the parasitic capacitance of our switch will determine the ringing frequency during the off portion of the flyback cycle, and knowing this frequency wll inform the component selection for our snubber. If you have no idea what a snubber is, or why a flyback cycle has an off portion, don't worry, we'll get to that in the next blog.

Inductance and leakage inductance masurement results

Bourns says in the datasheet that this transformer has a nominal primary inductance of 25 µH, a nominal leakage inductance of 0.6 µH, and a primary DC resistance of at most 0.55 ohms, and this is confirmed by the measurements with values of 24.75 µH, 450nH, and 553 milliohms, respectively. They also provide us with the turns ratio between primary and secondary of 0.77, and from the equation that connects turns ratio with inductance:

 image

we input the inductances:

image

and get a turns ratio of 0.7696, almost exactly what the datasheet claims. Perfect!

now let's take a look at

The Flyback converter topology

flyback converter schematic with mostly ideal components

This is the simplest flyback converter schematic representation, and in this case, the components used are all ideal, except for the MOSFET, as I couldn't get LTspice to run a proper simulation with an ideal voltage controlled switch. The selection of the MOSFET and that of the other components is such just because those were the components I had lying around, it was random, and after all, this was just meant to be a proof of concept, to see if the circuit would work.

Using this almost ideal schematic, we can see how the voltage output equation for a flyback converter (in DCM mode) gives us a close match to what we see in the simulation, where R is the load resistor, T is the period of our switching frequency, D is the duty cycle, and Lp is the primary inductance (primary inductance for the ideal case only):

image

 a look at the input and output voltages

Lp should technically be the magnetizing inductance, but for now, as the modeled transformer is ideal, the entire primary inductance is assumed to be magnetizing.

After seeing the simulation results, I went to build the circuit:

flyback converter on a breadboard, 10 ohm sense resistors are paralleled with jumpers, to use either of them depending on what's being measured

 a look at the MOSFET and output stage of the converter

I also added 10 ohm resistors in series with both the input and the output to take a look at the currents, which according to the (close to) ideal simulation should look like this: 

 a simulation of the almost ideal circuit, showing the primary current and output diode current

(that ringing on the primary side current has to do with parasitic components in the mosfet, which we'll see later)

but since my real life components are far from ideal, I went ahead and measured everything using the impedance analyzer, and then modeled the circuit in LTspice as well as my measurements allowed me to, and now the current waveforms became spicier: 

 primary and diode currents with more realistic components

you might also notice that the transformer coupling is no longer 1. This is because with real components we have less than perfect coupling, and the uncoupled part is what becomes the leakage inductance. 

We can calculate the coupling factor like this:

image

This equation also assumes no losses, but if we model the transformer as measured, ideally coupling the magnetizing inductance and adding the leakage inductance in series, uncoupled, as well as taking into account the series resistance of the windings, we get a very similar result, just with larger amplitude ringing as you can see here:

image

now let's take a look at the MOSFET and diode currents in the real circuit:

 a real measurement of the circuit, with the jumpers across the 10 ohm resistors removed

we can see that they are an almost exact match to what we see in the simulation. From this we can now safely assume that the circuit will behave just as in the simulation once i bridge the 10 ohm resistors. We won't be able to see the currents anymore, but knowing that the circuit behaves just as expected from the simulation, we can use the results of the resistorless simulation, together with the voltage measurements of the real life circuit to get the complete picture of what's going on with our circuit.

So, does it fly back?

Well, from this experiment we can see that this simple converter cobbled together from an assortment of randomly selected components does behave exactly as seen in the diagrams found all over the internet which show the waveforms of a DCM flyback converter. It does fly back!

But what exactly is it that *flies back*?

While the circuit's behaviour is almost textbook, and that's great! it is still not entirely clear to me what flies back, having found different answers in different places, with some saying that "flyback" refers to the beam in CRT TVs flying back to where it would begin drawing the next line, others saying it is about the energy "flying back" from one winding to the other on the off portion of the cycle, and others saying it is about the magnetic field collapse in the transformer.

Another explanation which seemed pretty reasonable is that when it came to the CRT high voltage transformers, they got their name because if you touched one live, it would make you fly back! Wink

Anyway, seeing how easy it is to get a flyback converter going was very encouraging, and since this cobbled together circuit worked perfectly, I'm going to continue exploring the flyback topology on it. 

In this image from TI's "Power Tips #98: Designing a DCM flyback converter" PDF, we see all the waveforms we should expect to see, as well as the ones we actually saw.

image

but there is one important waveform left we have yet to look at, the voltage at the MOSFET (Voltage between Drain and Source). Let's take a look:

 in green: Vds of our almost ideal circuit

On this almost ideal circuit, we see it is just as expected, with the maximum Vds of around 20.5V, which would be what we get from the equation described in TI's guide:

image

and from our closer to real life simulation:

 in green: Vds of our more realistic circuit

well, that is *not ideal* for sure! we're getting spikes of over 25V at Vds!

and our real life circuit, again, agrees with the simulation: 

 Vds of our real life circuit

so, what is going on here? That's what I'll explore in the next blog, what that ringing is, where does it come from, why do we not want it, and how to get it under control. Here's a sneak peek at how that looks like when it's under control:

 voltage spikes under control, but how? hmmm!

Again, this is my first blog, and I'm far from being a writer, so I'm also taking this as an opportunity to ask for feedback, let me know what you think I can improve about my writing, so the next blogs are nicer to read.

Any questions, I'll be happy to answer in the comment section.

Thank you! Slight smile

How to properly measure transformers: Transformer Measurements

  • Sign in to reply

Top Comments

  • Anthocyanina
    Anthocyanina over 2 years ago in reply to Anthocyanina +1
    I couldn't wait to post this in another blog, so the simulations here will also serve as sneak peeks: This is how the currents look like with the unshorted aux leakage measurement, this looks the furthest…
Parents
  • javagoza
    javagoza over 2 years ago

    Congratulations Anthocyanina  on publishing your first blog! This is a great start and will make it easier for you to continue writing. Setting achievable goals for yourself is important, and you've done just that by planning your next blog. Keep up the good work!

    A question: when measuring the leakage inductance I see that you are doing it on the secondary winding and shorting primary and AUX, shouldn't you do it by measuring on the primary and shorting the other two windings? 

    And if you are not going to use the AUX winding, I think there is no point in short-circuiting it either, that winding would only be affected by the Eddy currents unconnected, no mutual inductance, at least that is what my intuition tells me, I am not an expert in this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to javagoza

    Thank you! 

    I took that picture when i was measuring the secondary leakage, and used it just to show a visual of how you would go about measuring the leakage inductance. I also measured the primary leakage. Leakage indutance is not something only present on the primary, I don't know why in most literature about flybacks they only consider the primary leakage, it might be that the secondary leakage is negligible when it comes to designing the specifications of the converter, but just as part of the primary inductance is not coupled to the secondaries, the secondares' inductances also aren't perfectly coupled to the primary, or to each other.

    I ran the simulation again, considering only the primary inductance, and curiously, the ringing damping looks closer to what i see with the AD2, but the amplitude of the ringing was closer to the simulation with both leakage inductances.

    image

    Curiously, the ringing frequency measured on the AD2 lies in the middle of the ringing frequency of this simulation and the one i included in the blog.

    About shorting the AUX winding, I'm going to re-measure that. Really interesting point! I had briefly thought about this and measured it with all the other windings shorted bcause my thinking process was that if the purpose of measuring this leakage inductance is to determine what portion of the total winding inductance isn't coupled to the rest of the system, even if a winding is not used, that leakage inductance still isn't part of the "transformer" portion of the entire magnetic system. This is what i think makes the most sense from what i've learned about transformers and coupled inductors, but i am not certain that this is the case, so as i've said, I will re-measure, and the findings will be posted in another blog this week.

    Thanks again! your comment has made me consider new things! Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to Anthocyanina

    I couldn't wait to post this in another blog, so the simulations here will also serve as sneak peeks:

    This is how the currents look like with the unshorted aux leakage measurement, this looks the furthest away from reality when compared to the other simulations

    image

    and what it looks like not considering leakage of the secondary:

    image

    this makes me think shorting the aux is still important when it comes to measuring leakage inductance, but using only the primary leakage still looks a bit closer to reality.

    I'm going to keep looking into this, thanks! javagoza 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to Anthocyanina

    For me all this is very complex.

    I made the previous comment to you from the perspective of measuring the leakage inductances of a transformer operating linearly.

    If we start to analyze the case of working in a flyback regime, I think it is more complex. 

    Probably the most worrying thing is the resonance that occurs between the leakage inductance and the parasitic output capacitor of the MOSFET when it is turned off.

    While the MOSFET is on, the secondary is disconnected due to the action of the secondary diode, t this moment we only have one inductor completely decoupled from the secondary, that is open circuit.

    This causes problems for me when it comes to understanding how to measure/calculate that leakage inductance, I think it will be mainly due to the air gap in the core. If we add to all this the AUX winding, I think we would have to analyze what type of rectification is done on that side. Maybe I am overthinking ha ha.

    Looking forward to reading your next blog with your conclusions, you are doing an excellent job.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to Anthocyanina

    Another thing that is on my mind is that since the leakage inductance depends on the frequency

    image

     you may be more interested in calculating the leakage impedance during the ringing period due to the oscillation produced by the parasitic capacitances and the leakage inductance.

    It seems to be a few tens of megahertz if I understand correctly.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to javagoza

    I was now able to simulate a much closer to ideal circuit, and thse are the idealized waveforms. when it comes to currents, it is as you say, one winding is not conducing at all while the other is: 

    image

    But there is still a voltage induced in the secondary, just blocked by the ideal diode, which has no capacitance, breakdown voltage, or recovery time, so it acts as a perfect barrier:

    image

    you can see in the orange waveform, the secondary voltage is highest while there is current flowing through the diode, but when the current stops, the voltage rapidly drops to 0. The red waveform is the PWM, and you can see that when the switch is on, there's of course 0V across what would be Vds if it was a perfect MOSFET, but there is voltage being induced in the secondary winding, and this voltage also is reflected back to the primary, inverted (so we measure from Vds to V1) and reduced by a factor of the turns ratio:

    Here's how it looks like reflected:

    image

    and here's how it looks like when scaled by the turns ratio:

    image

    So you can see, the voltage induced in the secondary, across the entire period does actually make itself present in the primary. This is actually a very useful characteristic of these converters as it allows the use of primary side regulation, by having the controller measure the reflected voltage to monitor the output of the secondary, meaning there would be no need for an opto-isolated feedback coming from the secondary.

    When it comes to real life circuits, wtih non-ideal components, we see that there is a bit of leakage current flowing through the windings(as seen in the screenshots in the blog when i'm taking measurements and the realistic simulations. This current keeps flowing because of the properties of inductors, but it is clearer to see why if we look at a more comprehensive model of the transformer:

    image

    In this model, we take the magnetizing inductance out, and replace it with an ideal transformer. The ideal transformer supposedly has infinite inductance, but that's impossible to simulate, so an arbitrarily high inducance of 1 kilohenry was used for both windings of the ideal transformer, and you see, while there is a measurable change in the behaviour of the circuit in the simulation, it is still significantly close to what it was before, especially considering the transformer part of the circuit is now a 1:1 transformer with ridiculously high inductance. This reflects the behaviour of what we call a coupled inductor, a more accurate term for our flyback transformers.

    Now it should be clearer why the current doesn't abruptly stop like it does in the ideal simulation, it has a path to flow through in the form of the ideal transformer windings, but i think Sam Ben-Yaakov explains it much better than I do:

    https://www.youtube.com/watch?v=laHN4Xn59lI

    About the leakage inductance, I'm still not entirely certain which value i should use when simulating, but now I'm leaning more toward just using the leakage measured between the windings i will actually use. I think this does make more sense now, considering the unused winding could be removed, and I will be testing that by taking a transformer apart, but it seems likely that it is the case.

    (with how long this was, i wonder if i should have turned this reply into its own blog post! hahaha)

    Thanks again for your comments! Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to javagoza

    I was now able to simulate a much closer to ideal circuit, and thse are the idealized waveforms. when it comes to currents, it is as you say, one winding is not conducing at all while the other is: 

    image

    But there is still a voltage induced in the secondary, just blocked by the ideal diode, which has no capacitance, breakdown voltage, or recovery time, so it acts as a perfect barrier:

    image

    you can see in the orange waveform, the secondary voltage is highest while there is current flowing through the diode, but when the current stops, the voltage rapidly drops to 0. The red waveform is the PWM, and you can see that when the switch is on, there's of course 0V across what would be Vds if it was a perfect MOSFET, but there is voltage being induced in the secondary winding, and this voltage also is reflected back to the primary, inverted (so we measure from Vds to V1) and reduced by a factor of the turns ratio:

    Here's how it looks like reflected:

    image

    and here's how it looks like when scaled by the turns ratio:

    image

    So you can see, the voltage induced in the secondary, across the entire period does actually make itself present in the primary. This is actually a very useful characteristic of these converters as it allows the use of primary side regulation, by having the controller measure the reflected voltage to monitor the output of the secondary, meaning there would be no need for an opto-isolated feedback coming from the secondary.

    When it comes to real life circuits, wtih non-ideal components, we see that there is a bit of leakage current flowing through the windings(as seen in the screenshots in the blog when i'm taking measurements and the realistic simulations. This current keeps flowing because of the properties of inductors, but it is clearer to see why if we look at a more comprehensive model of the transformer:

    image

    In this model, we take the magnetizing inductance out, and replace it with an ideal transformer. The ideal transformer supposedly has infinite inductance, but that's impossible to simulate, so an arbitrarily high inducance of 1 kilohenry was used for both windings of the ideal transformer, and you see, while there is a measurable change in the behaviour of the circuit in the simulation, it is still significantly close to what it was before, especially considering the transformer part of the circuit is now a 1:1 transformer with ridiculously high inductance. This reflects the behaviour of what we call a coupled inductor, a more accurate term for our flyback transformers.

    Now it should be clearer why the current doesn't abruptly stop like it does in the ideal simulation, it has a path to flow through in the form of the ideal transformer windings, but i think Sam Ben-Yaakov explains it much better than I do:

    https://www.youtube.com/watch?v=laHN4Xn59lI

    About the leakage inductance, I'm still not entirely certain which value i should use when simulating, but now I'm leaning more toward just using the leakage measured between the windings i will actually use. I think this does make more sense now, considering the unused winding could be removed, and I will be testing that by taking a transformer apart, but it seems likely that it is the case.

    (with how long this was, i wonder if i should have turned this reply into its own blog post! hahaha)

    Thanks again for your comments! Slight smile