Experimenting with Flyback Transformers
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Flyback Transformers
  • More
  • Cancel
Experimenting with Flyback Transformers
Forum What does "SP-E", "16/5" and "20/6" mean in the flyback transformer product titles
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Flyback Transformers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 44 subscribers
  • Views 2274 views
  • Users 0 members are here
  • flyback transformers
  • bourns
Related

What does "SP-E", "16/5" and "20/6" mean in the flyback transformer product titles

BigG
BigG over 2 years ago

This has me perplexed.

Each product datasheet would have a title as follows: Model 063929 SP-E 16/5 Flyback Transformer, or Model 094929 SP-E 20/6 Flyback Transformer

So what is "SP-E" as it is also included in the EMC Filter Choke datasheets but not in the BA60951CS datasheet. In fact here the Filer Choke product 071923 also has "13/4" in the title.

Furthermore, the BA60951CS does not include any of these numbers either.

Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 2 years ago in reply to BigG +4
    The voltage range isn't for the transformer, it's for the SMPS that it is intended to be designed into. Manufacturers of such supplies seem to have come to a consensus that a universal input power supply…
  • javagoza
    javagoza over 2 years ago in reply to javagoza +3
    From digikey site: SmartPower Safety 3 W to 22 W Flyback Transformers Bourns' transformers feature an E16/5 or E20/6 power-ferrite core shape with a high clearance and creepage distance Safety 3…
  • javagoza
    javagoza over 2 years ago +2
    SP refers to Bourns Smart Power Transformers Series https://www.bourns.com/docs/rohs-cofc/sp_transformer_coc.pdf?sfvrsn=1b4e58f6_3
Parents
  • shabaz
    0 shabaz over 2 years ago

    I can help with a bit of it. There are traditional E shaped ferrite core sizes, known as (say) EF 16 and EF 20. The ferrite itself (not the entire transformer) has approximate dimensions of 16 mm width, and 5 mm thick for the EF 16. For the EF 20 cores, those two dimensions are approx 20mm and 6mm. So I think they are referring to that the transformers are using ferrites of those dimensions.

    I've no idea what SP-E means though. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 2 years ago in reply to shabaz

    Aha. Thanks Shabaz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • BigG
    0 BigG over 2 years ago in reply to shabaz

    Aha. Thanks Shabaz.