Experimenting with Flyback Transformers
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Flyback Transformers
  • More
  • Cancel
Experimenting with Flyback Transformers
Forum Poll - Did You Increase Your Knowledge of Flyback Transformers?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Flyback Transformers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 43 subscribers
  • Views 2857 views
  • Users 0 members are here
  • EXPERIMENTING WITH FLYBACK TRANSFORMERS
Related

Poll - Did You Increase Your Knowledge of Flyback Transformers?

rscasny
rscasny over 2 years ago

As I stated last week, I sent the final blogs to my judges. One judge has scored the final blogs. I'm just waiting on the other judge. The announcement should be made later this week. 

I want to thank the participants of Experimenting with Flyback Transformers. It turned into a challenging program and an intense learning experience. I want to thank you for your time and some incredible blogs.

While I am waiting for the last judge to score the final blogs, I'd like to post a poll regarding how this program helped you increase your knowledge or even awareness of flyback transformers. 

Both participants and community members can vote in the poll.

Thanks.

Randall

--element14 Community Team

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +5
    It was very useful! I really enjoyed seeing the content from this challenge. Although it certainly lived up to its name and was challenging, it was great to see that all the contestants that stuck with…
  • misaz
    misaz over 2 years ago +4
    I did not join competition but even research when considering joining learnt me a lot.
  • Anthocyanina
    Anthocyanina over 2 years ago +4
    I did learn a lot. This challenge also helped me clear quite a few misconceptions and showed me there's still a lot to learn about flybacks
Parents
  • BigG
    BigG over 2 years ago

    If I can make an observation for other similar type of design challenges in the future... I felt it would have helped me immensely if some core components (e.g. diodes, mosfets, resistors, capacitors etc.) were included in the pack to get you started with a basic reference design. Having a BoM together with a reference design helps too.

    The purpose of this is to help you first and foremost validate that everything is working and then it helps you compare/contrast a working design with any other design ideas you may have built. Without this reference design built it is quite difficult to get started if you have not done this before as you have no baseline reference components to work from. Otherwise you spend a very long time seeking out basic components and having to test them before moving on (quite of few of my first choices proved to be poor ones and then I had to spend more time searching again and then waiting a week of so for another order to arrive etc). Basically poor search parameters lead to poor component choice etc. which then leads to delay.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to BigG

    You're right. I think the kit should have been expanded. I should have thought deeper and longer about what might be needed. This one was kind of new for me, too. I learned from the participants. I think for the next one, I'll ask everybody a month into the challenge what do they feel they could use. If it is board level components, we usually have good inventory and could get them out to everyone quickly. A reference design would have been helpful as well. I have to address that. Good point.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to rscasny

    I remember you made a generous offer to complete the kits with additional components. I think none of us take advantage of it, perhaps due to lack of confidence in our applications:

    How Can You Experiment with Flyback Transformers - Some Thoughts and Ideas 

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 2 years ago in reply to rscasny

    Hi Randall, I was suggesting something slightly different where reference components are provided as default (i.e. part of the pack) rather than where the user has an option to select, which you have often used in the past.

    What I am trying to get around is basically the poor choice scenario at the beginning and also to allow all competitors to validate (as in all competitors have the same baseline so if one of them cannot get it to work, it is easier to work out why).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 2 years ago in reply to rscasny

    Hi Randall, I was suggesting something slightly different where reference components are provided as default (i.e. part of the pack) rather than where the user has an option to select, which you have often used in the past.

    What I am trying to get around is basically the poor choice scenario at the beginning and also to allow all competitors to validate (as in all competitors have the same baseline so if one of them cannot get it to work, it is easier to work out why).