Experimenting with Gesture Sensors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Gesture Sensors
  • More
  • Cancel
Experimenting with Gesture Sensors
Challenge Blog Blog #14: Gesture Controlled Pacman
  • Challenge Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Gesture Sensors to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: misaz
  • Date Created: 3 Jan 2023 10:25 AM Date Created
  • Views 1711 views
  • Likes 9 likes
  • Comments 2 comments
  • max78000
  • MAX25405
  • pacman
  • experimenting with gesture sensors
  • game
  • MAX25405EVKIT
  • microcontroller
  • max78000fthr
  • MAX16935
Related
Recommended

Blog #14: Gesture Controlled Pacman

misaz
misaz
3 Jan 2023

Hello everyone. I welcome you to my blog post as part of Experimenting with Gesture Sensors competition. This is one of the most important blog posts because today I will show my fully completed Gesture Controlled Pacman console! It is this device:

image

Stand

As you can see, I developed new stand for it is built from Merkur building set which is Czech building set comparable to Meccano. Main difference between Merkur and Meccano is dots pitch. Merkur use metric pitch of exactly 1 cm (10 mm).

From side it looks as follows:

image

And from back we can see additional hardware used for controlling device:

image

On photo you can see bridgetek ME817EV evaluation board which drives RGB interface to the display and generate screen. This board is connected using colorful cable to the MAX78000FTHR board with MAX78000 microcontroller. MAX78000FTHR is directly connected to the shield board as part of MAX25405 Evaluation Kit. MAX25405 Sensor Board which is in the front of device below display is to the shield connected using ribbon cable. The last part is my own voltage regulator board which converts 12V from power adapter to the 3.3V used by Gesture Sensor shield. It uses MAX16935 Step-Down regulator for doing its task.

Startup

After startup device show splash screen indicating for what competition I created this device and which community hosted it Blush

image

After few second splash screen disappear and gesture sensor start working.

Control

This game is controlled by your hand, and you do not need to touch the device when playing! You only need swipe your hand in the front of device. Range is about 30 cm. Swiping hand from left to right set pacman direction to right. Swiping from top to down change direction to down and so on.

See it in the action!

On following video, you can see my play:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Block diagram

image

Pinouts

Most parts are connected intuitively. For example, MAX25405 Shield exactly matches pinout of MAX78000FTHR board. Similarly ribbon cable has lock which prevents issues with connection of sensor board with the shield. The only thing needs to be interconnected manually is connection between BT817 board and MAX78000FTHR. Connect it as follows:

  • GND on BT817 Board (CN8) to GND on MAX78000FTHR
  • MISO on BT817 Board (CN8) to P0.6 on MAX78000FTHR
  • MOSI on BT817 Board (CN8) to P0.5 on MAX78000FTHR
  • SCK on BT817 board (CN8) to P0.7 on MAX78000FTHR
  • CS on BR817 board (CN8) to P2.3 on MAX78000FTHR
  • PD on BT817 board (CN8) to P1.0 on MAX78000FTHR

For searching pins on MAX78000FTHR you can use following diagram from its datasheet:

image

BOM

For making project on your own you need following parts:

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
MAX25405EVKIT#, Evaluation Board, MAX25405, Optical IR Sensor MAXIM INTEGRATED (ADI) 1 Buy Now
MAX78000FTHR#, Development Board, MAX78000EXG+, 32 Bit, ARM Cortex-M4F MAXIM INTEGRATED (ADI) 1 Buy Now
MAX16935RAUE/V+, DC/DC CONV, BUCK, 2.2MHZ, 125DEG C MAXIM INTEGRATED (ADI) 1 Buy Now
ME817EV, Evaluation Board, BT817, Embedded Video Engine (EVE) BRIDGETEK 1 Buy Now
Display, 1024x600, TFT, LCD, RGB Interface RIVERDI 1 Buy Now
MP006289, Jumper Wire Kit, Male to Female, Multi-Coloured, 200 mm, 0.1" Dupont Connector, 0.2 mm² MULTICOMP PRO 1 Buy Now
 

Additional Parts

Product Name Manufacturer Quantity
Merkur building set Merkurtoys s.r.o. 1

Powering sequence

Recommended ordering of powering parts is following:

  • Plug 5, 9 or 12V jack from adapter to the MAX16935 regulator module or other 3.3V regulator Module. If you are in America, you can use adapter bundled with MAX25405 Evaluation Kit and power it directly without need of doing this step.
  • Plug jack from MAX16935 regulator to the MAX25405 Gesture Sensor Shield.
  • Check that Jumper JP1 on BT817 board is set to positions 1-2. Then connect USB cable to USBC2 connector of BT817 board.
  • Connect USB cable to MAX78000FTHR.

Flashing firmware

For flashing firmware to MAX78000 firmware download firmware from the end of this blog post and drag and drop firmware to the DAPLINK drive which appeared in your PC after you connected MAX78000FTHR.

image

Copy paste take some time and after completion drive disconnects and firmware start running.

Firmware

Firmware is written in C. It consists of:

  • My own MAX25405 Gesture Sensor library for configuring sensor and retrieving data from sensor. Implementation is in files: MAX25405.c, MAX25405.h, MAX25405_PlatformSpecific.c and MAX25405_PlatformSpecific.h
  • My own BT817 Library for initializing display and generating screens. Implementation is in files BT817.c and BT817.h
  • My own Gesture Detection algorithm implementation. Implementation is in files: GestureDetect.h and GestureDetect2.c
  • My own implementation of Pacman logic and objects. Implementation is in files: FieldState.h, Figure.h, Game.c, Game.h, GameRenderer.c, GameRenderer.h, GameStruct.h, Ghost.c, Ghost.h, GhostStruct.h, Pacman.c, Pacman.h, PacmanStruct.h, Vector.c and Vector.h
  • Logic for rendering splashscreen and its images. Implemented in files: SplashScreen.c, SplashScreen.h and Images.c
  • c for bundling all things together.

For controlling MAX78000 peripherals I use PeriphDriver library from Maxim SDK. I do not use any other library. Most of the code is my own.

Gesture Sensor Performance

Because this series of article and this project are all about gesture sensor. It is good time to review gesture sensor performance. On video above you have seen that it is possible to play (and win) pacman with the sensor, but you have also seen that gesture detection sometime do not go as I want. As part of this project, I implemented my own gesture detection. It is difference from my previous project: Gesture Controlled Tetris. In previous project I used EVKIT firmware which have implemented better and more advanced algorithm. My algorithm has slightly worse results, but I think it is still acceptable outcome from only two months of work and no previous experiences in this area. There were only few errors and in most cases my algorithm worked well and pacman went the correct direction. Also note that algorithm worked even I have additional thing (my hand with phone used as camera) in the scene. It is because my algorithm uses digital filters which filters static objects from the scene. More details about this and other features of my algorithm was described in previous two blogs.

Conclusion

This is my final project as part of this competition. Next time I will show one of my experiments which I did and later I will close my application by posting final blog in which I will summary all my effort as part of Experimenting with Gesture Sensors competition. For now, I thank you for reading this blog post and if you are interested in making your own Pacman console feel free to download source codes and firmware below.

Resources

  • My MAX25405 Gesture Sensor Library (Github)
  • Pacman firmware source codes and Eclipse Project (Github)
  • Pacman firmware binary (Hex)

Next blog:  Blog #15: Experimenting with Two MAX25405 Kits

  • Sign in to reply

Top Comments

  • obones
    obones over 3 years ago +1
    Very nice use of both the BT817 and the MAX25405, this really shows what a real world use of those chips could look like.
Parents
  • misaz
    misaz over 3 years ago

    EDIT 2023-01-04: I reuploaded all images which failed to upload yesterday. I also changed emthod of uploading images. Now page should load faster. Text is exactly the same as yesterday.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • misaz
    misaz over 3 years ago

    EDIT 2023-01-04: I reuploaded all images which failed to upload yesterday. I also changed emthod of uploading images. Now page should load faster. Text is exactly the same as yesterday.